Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Solving fan whine
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 337 subscribers
  • Views 7463 views
  • Users 0 members are here
  • fan noise
  • fan whine
  • electronics
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Solving fan whine

cstanton
cstanton over 4 years ago

I've recently received a device and it has a fan built into it for cooling, but I've noticed a particular whine with it:

image

A very high volume 3.7khz pitch whine/noise from it.

What could cause such a noise? and more importantly, what should be the solution?

This is what the fan looks like physically:

image

  • Sign in to reply
  • Cancel

Top Replies

  • BigG
    BigG over 4 years ago +1
    I can sympathise. I recently purchased one of those Ikea Air Quality sensors. At first, I wondered why others had noted online about the fan noise, especially as the fan is tiny, but then sure enough…
Parents
  • dougw
    dougw over 4 years ago

    Noise could come from electrical fluctuations, bearing vibration or airflow modulation.

    Electrical fluctuations get translated into acoustical noise by magnetostriction or electrostatic forces. You can test if this might be the cause by determining if the frequency of electrical fluctuations matches the frequency of the noise. The fixes to prevent these motions include firmer mounting or damping out the motions with rubber. It may be possible to filter the electrical signal a bit to minimize its effect.

    Bearing vibration can sometimes be deduced by seeing if the fan rattles at all when shaken, or if there is any play in the impeller when it is wiggled.. The easiest fix is just to lubricate the bearings or bushings.

    You can calculate potential airflow modulation frequencies by measuring the fan RPM and multiplying by the number of blades and obstructions. You can also get a little whistle effect if some flexible vane is flopping around in the airflow.

    Any fixed noise frequency can be "amplified" by a resonant acoustic cavity. These can be altered or eliminated by stuffing something into them.

    Does the pitch change with applied voltage or flow rate or orientation?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 4 years ago in reply to dougw

    The frequency changes with the rpm of the fan, faster = higher, slower = lower, orientation and voltage aren't something I have access to measure at present.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 4 years ago in reply to cstanton

    I would try lubricating the bushing simply because it is simpler than trying to guess what might cause an airflow whistle without being there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 4 years ago in reply to cstanton

    I would try lubricating the bushing simply because it is simpler than trying to guess what might cause an airflow whistle without being there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • cstanton
    cstanton over 4 years ago in reply to dougw
    dougw said:
    I would try lubricating the bushing

    I think this's going to be a factor. I appreciate the help, thank you :)

    Here's a reveal of where the fan is situated:
    image

    It's inside of Valve's Steam Deck.

    you can disregard the blue tape, that was there to check the noise while I moved the fan, here's what it covers:

    image

    The community behind the steam deck have discovered there's two brands of fan in the steam deck, this Delta, and one by Huaying, and the Huaying typically doesn't suffer from the high whine.

    Securing the enclosure, and the nearby aluminium shielding has reduced the noise somewhat, but it is still there.

    Before:
    image

    After: