Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Driving e-Paper display with Adafruit Feather nRF52 Bluefruit LE, but not getting sharp Image
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 15 replies
  • Subscribers 303 subscribers
  • Views 2733 views
  • Users 0 members are here
  • epaper
  • nrf52
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Driving e-Paper display with Adafruit Feather nRF52 Bluefruit LE, but not getting sharp Image

KKaushik
KKaushik over 3 years ago

I am driving e-Paper display with nRF52 Module named mentioned above, but not getting sharp image

#include <GxEPD.h>

#include <GxGDEH0213B73/GxGDEH0213B73.h> // 2.13" b/w newer panel

#include GxEPD_BitmapExamples

// FreeFonts from Adafruit_GFX
#include <Fonts/FreeMonoBold9pt7b.h>
#include <Fonts/FreeMonoBold12pt7b.h>
#include <Fonts/FreeMonoBold18pt7b.h>
#include <Fonts/FreeMonoBold24pt7b.h>


#include <GxIO/GxIO_SPI/GxIO_SPI.h>
#include <GxIO/GxIO.h>

#include "IMG_0001.h"

GxIO_Class io(SPI, /*CS=*/ 4, /*DC=*/ 3, /*RST=*/ 2); // arbitrary selection of 8, 9 selected for default of GxEPD_Class

GxEPD_Class display(io, /*RST=*/ 2, /*BUSY=*/ 5); // default selection of (9), 7

void setup()
{
Serial.begin(115200);
Serial.println();
Serial.println("setup");

display.init(115200); // enable diagnostic output on Serial

Serial.println("setup done");
//showpic();
}

void loop()
{
//showpic();
display.drawPaged(showFontCallback);
delay(5000);
}
void showFontCallback()
{
const char* name = "FreeMonoBold9pt7b";
const GFXfont* f = &FreeMonoBold9pt7b;
display.fillScreen(GxEPD_WHITE);
display.setTextColor(GxEPD_BLACK);
display.setFont(f);
display.setCursor(0, 0);
display.println();
display.println(name);
display.println(" !\"#$%&'()*+,-./");
display.println("0123456789:;<=>?");
display.println("@ABCDEFGHIJKLMNO");
display.println("PQRSTUVWXYZ[\\]^_");
#if defined(HAS_RED_COLOR)
display.setTextColor(GxEPD_RED);
#endif
display.println("`abcdefghijklmno");
display.println("pqrstuvwxyz{|}~ ");
}

void showpic()
{
//uint16_t x = (display.width() - 128) / 2;
uint16_t x = 0;
uint16_t y = 0;
display.fillScreen(GxEPD_BLACK);
display.drawExampleBitmap(gImage_IMG_0001, x, y, 128, 250, GxEPD_WHITE);
display.update();

}

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 3 years ago +3
    The black and white particles get separated based on voltage and duration of the applied signal. You can check the high voltage supply to ensure it is high enough (it could also need extra capacitance…
  • shabaz
    shabaz over 3 years ago in reply to KKaushik +2
    Where did you buy the display from? Did you buy it from the some source that the driver code came from, or not? You can see in the datasheet that you provided: The special parameters are not part…
  • feiticeir0
    feiticeir0 over 3 years ago in reply to KKaushik +1
    Hi ! I'm guessing, by the pictures, that's a display problem... Did it, in any time, give a sharper image ? Even the first time you thinker with it ?
Parents
  • rsjawale24
    0 rsjawale24 over 3 years ago

    Could you attach a picture of the display?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • KKaushik
    0 KKaushik over 3 years ago in reply to rsjawale24

    imageDark at Power Onimage

    When it gets updated it gives a darker image but is still not as clear as it is supposed to be. Immediately after the update, it goes dull and can't see anything. (This is when repeating update)
    If I update once only it will go dull and stops there.

    A similar thing happens when I quickly remove the display from the driver circuit. It stays dark for a longer time but starts to get dull again. Ans also previously updated images starts to show up in the background.
    Since I haven't worked with e-paper displays before, So I'm not sure about their behavior. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • feiticeir0
    0 feiticeir0 over 3 years ago in reply to KKaushik

    Hi !

    I'm guessing, by the pictures, that's a display problem...

    Did it, in any time, give a sharper image ? Even the first time you thinker with it ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • feiticeir0
    0 feiticeir0 over 3 years ago in reply to KKaushik

    Hi !

    I'm guessing, by the pictures, that's a display problem...

    Did it, in any time, give a sharper image ? Even the first time you thinker with it ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • KKaushik
    0 KKaushik over 3 years ago in reply to feiticeir0

    Hello,

    No these displays never gave any sharper images not even with ESP32. But I was in doubt because it's not just this one, there were other two. 

    1st FPC connector got damaged and 2nd one stopped working suddenly. Both of them didn't give any sharper images using the same library, so I thought there is some issue with the driver /library for EPD.

    Also when I checked the manufacturer for these, Its branded so I wasn't sure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rsjawale24
    0 rsjawale24 over 3 years ago in reply to KKaushik

    Did the display come along with the HAT that you're using?