Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Virtual Machines on Windows with Hyper-V Manager
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 326 subscribers
  • Views 1199 views
  • Users 0 members are here
  • vm
  • windows
  • virtual machine
  • hyper-v
  • linux
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Virtual Machines on Windows with Hyper-V Manager

shabaz
shabaz over 3 years ago

I do not know if this is common knowledge or not, but I just discovered that Windows 11 (and perhaps Windows 10) has VM capability that is easy to use, and free.

I used VMWare Workstation in the past, but that is pricey (and needs upgrading every couple of years because it inevitably stops working as Windows evolves). I never liked Oracle's VirtualBox.

If you need to spin up (say) Linux quickly, then it is just 5-10 minutes away from scratch. The information is here:

https://docs.microsoft.com/en-us/virtualization/hyper-v-on-windows/quick-start/quick-create-virtual-machine

I probably will not use it regularly, since I already have Linux on a separate Intel box, (and several Raspberry Pi's that can be brought up within seconds) but it could come in handy from time to time, for instance, for testing code.

A minor annoyance is that it will not run VMWare Workstation-created VMs (there may be conversion utilities, but they are third-party, and I couldn't find one that looked usable and free), but I can live with that.

image

It puts the virtual hard disks here by default:

image

The checkpoint feature is neat; I don't recall if VMWare Workstation ever had that. Here you can see I went back to an earlier checkpoint (it retains them all, in a tree):

image

Disk after creating those checkpoints:

image

  • Sign in to reply
  • Cancel

Top Replies

  • misaz
    misaz over 3 years ago +2
    I use it regularly. It is Type 1 hypervisor which is more performant than type 2 hypervisors like VirtualBox. It is much faster because very few virtual hardware is emulated. The only disadvatange is that…
  • Jan Cumps
    Jan Cumps over 3 years ago +1
    Ow, that's straightforward. I have a similar Linux farm as you. PIs, BBs and an Intel laptop all running some Linux. On my Windows laptop, I run Ubuntu under WSL - good enough to run build/make scripts…
Parents
  • misaz
    misaz over 3 years ago

    I use it regularly. It is Type 1 hypervisor which is more performant than type 2 hypervisors like VirtualBox. It is much faster because very few virtual hardware is emulated. The only disadvatange is that virtual GPU with virtual display is slow and laggy. I recommend using SSH and VNC for accessing Linux machines and RDP for windows machines instead of using virtual screen.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to misaz

    I rarely use the Linux desktop too. Mostly SSH using the excellent SecureCRT, and coding using Visual Code on Windows, remotely connected to the source code using the built-in VS Code Server that it automatically installs to the Linux box. I'm super-happy with this combination, I feel really productive with it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago in reply to misaz

    I rarely use the Linux desktop too. Mostly SSH using the excellent SecureCRT, and coding using Visual Code on Windows, remotely connected to the source code using the built-in VS Code Server that it automatically installs to the Linux box. I'm super-happy with this combination, I feel really productive with it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
No Data