Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Stereo Phono Cartridge to both Stereo and Mono Amps
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 21 replies
  • Subscribers 338 subscribers
  • Views 6668 views
  • Users 0 members are here
  • phono
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Stereo Phono Cartridge to both Stereo and Mono Amps

TC_Walker
TC_Walker over 3 years ago

Hello,

I am interested in a project to take a stereo signal from a record needle cartridge and split the signal into a stereo amp and also a mono amp to be used at the same time (and independently with some switching). I have tried a couple of simple methods that negatively effected the stereo signal. I am thinking op amps might be a way to do this but I am unable to design this. Regardless of what method is used sharing your knowledge would be so greatly appreciated.

- Tom

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +2
    Shabaz explains the principle in his message. (Although I think 1k resistors may be too low for some pre-amps) The problem is that a good mono mix is not made by adding the two channels of a stereo mix…
  • shabaz
    shabaz over 3 years ago in reply to michaelkellett +2
    Hi Michael, I found a reference to ceramic pickups on http://www.douglas-self.com/ampins/library/ampartew.htm which directed to a Wireless World article. In the August 1971 PDF issue of Wireless World…
  • michaelkellett
    michaelkellett over 3 years ago in reply to TC_Walker +2
    It looks as if you are going to try building a pre-amp based on the WW design. Meanwhile I have a little charge amplifier from Jan Cumps to test. He designed the board based on some suggestions from…
Parents
  • shabaz
    0 shabaz over 3 years ago

    It took a bit longer than expected, there's a lot of BC109's! 

    The image below shows just the left channel, I will copy-paste it to make the right channel once this one is reviewed. There is a PDF version of the circuit which may be easier to see.

    I wanted to highlight/ask these things:

    1. I've only used through-hole parts, so the board might end up being perhaps eurocard-sized, but as I understand there is room for that. 

    2. I've added a Line input too, since it's low-hanging fruit. If it's not needed, then the footprint for the relay contacts can be easily jumpered with wire, since then the relays (one for each channel since they are inexpensive and will simplify the layout) are not required.

    3. The mono output is perhaps a few hundred mVp-p when the main output is say 2V p-p, since the mono input will be expecting a low amplitude, but I don't know the precise value, so there are trimmers for that, labelled VR6 on the left channel.

    3. It needs an approx 24V supply, I'm thinking I could add a bridge rectifier if desired so that it can connect to a transformer. What's the opinion on that? 

    4. Considering adding a couple of small solder-in fuses on the mono output connections (both signal and ground) in case some problem occurs with the vintage equipment; is this a good idea, or not necessary?

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 3 years ago in reply to shabaz

    I have to say that I really don't "rate" the luxury version of the circuit - its way to complicated and very 5 decades ago.

    It also uses a very supsect and noisy technique of running the ceramic pickup into a low impedance with two pots and attenuation on the input signal for maximum noise. The 50k pot is an impedance matching effort. But the net effect of all this is to introduce a first order high pass filter with a -3dB point at about 1kHz and then recover the response with the frequency compensation in the first stage amplifier. That is pretty yucky.

    I would go for a high input impedance op amp buffer or possibly a charge amplifier with a first order high and low pass filters set to approx 50Hz and 15kHz. Equalization can be added once the signal is buffered and at a reasonable impedance level.

    I'd expect the cartridge to have about 100mV ouput (won't know untill I test) so even a fairly rough op amp with 10nV/rtHz noise will give a signal to noise ratio of 98dB - which is way better than the vinyl.

    Fine tuning the equalization means using a frequency response test record (if you are willing to sacrifice one to a ceramic pickup) and measuring the arm cartridge resonance frequency and Q - or else do it by ear !

    I don't quite understand Q6 and Q7 in your circuit.

    The 220nF across the emitter load resitance will just introduce a lot of distortion at higher frequencies.

    Why not mix the two channels at the mix ballance pot (feed once channel into each end via 22k) and have just one buffer amplifier.

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 3 years ago in reply to shabaz

    I have to say that I really don't "rate" the luxury version of the circuit - its way to complicated and very 5 decades ago.

    It also uses a very supsect and noisy technique of running the ceramic pickup into a low impedance with two pots and attenuation on the input signal for maximum noise. The 50k pot is an impedance matching effort. But the net effect of all this is to introduce a first order high pass filter with a -3dB point at about 1kHz and then recover the response with the frequency compensation in the first stage amplifier. That is pretty yucky.

    I would go for a high input impedance op amp buffer or possibly a charge amplifier with a first order high and low pass filters set to approx 50Hz and 15kHz. Equalization can be added once the signal is buffered and at a reasonable impedance level.

    I'd expect the cartridge to have about 100mV ouput (won't know untill I test) so even a fairly rough op amp with 10nV/rtHz noise will give a signal to noise ratio of 98dB - which is way better than the vinyl.

    Fine tuning the equalization means using a frequency response test record (if you are willing to sacrifice one to a ceramic pickup) and measuring the arm cartridge resonance frequency and Q - or else do it by ear !

    I don't quite understand Q6 and Q7 in your circuit.

    The 220nF across the emitter load resitance will just introduce a lot of distortion at higher frequencies.

    Why not mix the two channels at the mix ballance pot (feed once channel into each end via 22k) and have just one buffer amplifier.

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 3 years ago in reply to michaelkellett

    Hi Michael,

    I see what you mean. The charts below show the response measurement of the first stage (I can't simulate the entire circuit end-to-end due to a license limit).

    Due to the low input impedance they are setting the gain to more than 20 dB higher to compensate at the low end. With the 1nF model, the response then becomes levelled out with the input trimmer set to approx 40kohm. It doesn't seem an ideal way to interface to such a cartridge : ( I'll put this design on hold since it has these shortcomings, and it won't perform like a modern circuit. I guess magnetic cartridges superseded the ceramic ones and no-one improved these circuits much, since there doesn't seem to be many designs on the web.

    image

    Regarding Q6 and Q7, they were there to reduce load on the main stereo output, because the simulation showed a bit more distortion with a lower resistance for the load. I could increase the mixing resistances and replace with a single amplifier, but since it was just a single extra BJT I left it there since I'd already simulated with that topology. I didn't see much distortion for that section with the simulation, it was pretty negligible at that low output amplitude for the mono output, but perhaps I should have simulated with a higher input. I was just guessing what the cartridge level would be at that time.