Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Latch ciruit Design Problem/Sugguestions
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 338 subscribers
  • Views 1283 views
  • Users 0 members are here
  • esp32
  • help
  • suggestion
  • circuit
  • Design
  • latch
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Latch ciruit Design Problem/Sugguestions

Chuitoto
Chuitoto over 3 years ago

Hi! I'm working on a project which needs latch circuit in my design, which use for Power on/off by hardware and software...

VBAT is 12V. so I put it through a LDR to logic 3V3.

First I have a latch switch, when logic 3V3(pin2) connect to pin1. The top Pmons ON then power up the device.

When the  logic 3V3(pin2) connect to pin3, off_requ gose high(1) then go in some MCU input. The MCU will do some proccess., then set output off_pwr to hight (1) to disable the top Pmos. 

Will the below diagram works as I discribe above ? Feel free to give me some suggestion for improve design ! 

thank you so much if you do so! 

Latch circuit

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 3 years ago +1
    This should work fine. You can reduce the power in the on state by using N channel FETs instead of bipolar transistors. Something like BSS138. or 2N7000.
Parents
  • dougw
    dougw over 3 years ago

    This should work fine. You can reduce the power in the on state by using N channel FETs instead of bipolar transistors. Something like BSS138. or 2N7000.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 3 years ago

    This should work fine. You can reduce the power in the on state by using N channel FETs instead of bipolar transistors. Something like BSS138. or 2N7000.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Chuitoto
    Chuitoto over 3 years ago in reply to dougw

    Thank you for your reply!! The BSS138 seems like a good option! Do you think increasing the resistance value would reduce the power too? let's say 100K

    And also, Any advice model of the top PMOS?  capable of such a high V? since that control a JetsonNANO VBAT is 12V and the currect may pass through <= 0.5A

    like ... SI2343DS I randomly search online (SOT23-3)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to Chuitoto

    Yes, increasing the resistances will help reduce power. SI2343DS looks fine.