Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Reverse protection of Multicomp pro DC/DC converters MP-K78xx?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 338 subscribers
  • Views 2731 views
  • Users 0 members are here
  • DC/DC Converter
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Reverse protection of Multicomp pro DC/DC converters MP-K78xx?

DavidOB
DavidOB over 3 years ago

Hi,

I'm unable to find rating and description of MP-K78xx DC/DC converters in respect to reverse current/voltage protection. I have some questions:

1. What happens if another voltage source is connected to the output if this converter is not powered and used with typical application circuitry with input/output 10/22uF ceramics capacitors?

2. Same question as 1. but what if the converter is powered?

3. Same question as 1. but what if the converter input is shorted to ground?

3. What would happen if that another source voltage is higher than the converter nominal output? E.g. MP-K7803-500R3 is used for a battery powered device and USB + is connected to the output power rail while connected with a PC. If USB cable is connected, its 5V would then go into this 3.3V K7803 output.

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 3 years ago +3
    Good questions and you're right to research them. LM78xx (and LM79xx) don't like reverse current so I always provide diode protection in case there is any over voltage/current problem downstream. I've…
  • scottiebabe
    scottiebabe over 3 years ago in reply to Andrew J +2
    I saw the cross-section of one of those last night:
  • Andrew J
    Andrew J over 3 years ago in reply to shabaz +1
    Are there USB connectors that have an Earth switch in them like DC Barrel Jacks - when a USB cable is plugged in it disconnects an Earth turning an alternate power source off?
Parents
  • DavidOB
    0 DavidOB over 3 years ago

    Thanks for the responses. Shabaz, I have read that sequence about "hot swap and parallel" several times but did not realize that in fact suggests the answers!

    Seems the answer to all questions is "it would probably fail" :-) and to prevent it, a Schottky (or a P-FET for lower drop) in series with the output should do the trick. A diode across the converter from Vout to Vin is not a good option as that would make a short from the external source to ground via this diode in case of my first Q3 situation (my bad for two threes, sorry).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • DavidOB
    0 DavidOB over 3 years ago

    Thanks for the responses. Shabaz, I have read that sequence about "hot swap and parallel" several times but did not realize that in fact suggests the answers!

    Seems the answer to all questions is "it would probably fail" :-) and to prevent it, a Schottky (or a P-FET for lower drop) in series with the output should do the trick. A diode across the converter from Vout to Vin is not a good option as that would make a short from the external source to ground via this diode in case of my first Q3 situation (my bad for two threes, sorry).