Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Best way to disconnect a SOIC-8 pin?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Subscribers 337 subscribers
  • Views 7855 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Best way to disconnect a SOIC-8 pin?

Andrew J
Andrew J over 3 years ago

I've accidentally connected a pin to GND and it should have been left unconnected.  It's pin 5 of an 8-pin SOIC so reasonably accessible but what would be the best way to actually disconnect it without stressing other pins?  Note that the track that connects it to GND is very short and actually under the IC so isn't accessible.  I don't really want to de-solder the chip so all I can think of is to try and wick up the solder from that pad and then gently bend the pin up.  I've found that trying to wick it up is quite difficult because there's always some that remains under the pin.

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago +6
    Go big! lol
  • baldengineer
    baldengineer over 3 years ago +4 verified
    I would heat up the pin, lift it, and then wick any solder left making a connection. In fact, you may find adding some solder first helps to make lifting it easier.
  • michaelkellett
    michaelkellett over 3 years ago +3
    I would cut the pin, I do have a nice pair of rather expensive micro cutters for this purpose. Works well on SOIC, less good on 0.5mm pitch pins. You can (with care) use a scalpel with a nice new blade…
Parents
  • shabaz
    0 shabaz over 3 years ago

    Hi Andrew,

    Usually the way I do that is to apply the iron onto the top of the leg of the SOIC chip (the part of the leg that is against the board), and when it's clearly molten, lever up at the same time with flat-ended tweezers. A tiny bit of solder as baldengineer says is helpful to get a bit of heat into it. And then, if there is still a bridge of solder, then the desoldering wick will get rid of it. This works 100% of the time, no broken legs or ripped pads, provided it's properly melted : )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to shabaz

    EDIT: actually, exactly as baldengineer mentions, sorry just read it!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 3 years ago in reply to shabaz

    EDIT: actually, exactly as baldengineer mentions, sorry just read it!