Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Trying to understand NFC ASK Modulation
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 19 replies
  • Subscribers 337 subscribers
  • Views 4483 views
  • Users 0 members are here
  • raspberry pico
  • nfc
  • nfc-a
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Trying to understand NFC ASK Modulation

BigG
BigG over 3 years ago

According to my Google search, NFC uses ASK modulation to transmit data:

https://www.rfwireless-world.com/Tutorials/NFC-Near-Field-Communication-tutorial.html

https://www.rfwireless-world.com/Tutorials/NFC-Modulation-and-NFC-Coding.html

Which I have interpreted as the following where the "Mixing Circuit" includes the NFC tuned antenna and two picoFarad capacitors... but what else is needed.

image

As a non electronics engineer I am trying to work out a minimum circuit required.

Then my lofty intentions is to use a Raspberry Pi Pico to generate my clock signal using PIO and as there is also a Manchester Encoding PIO example, I will attempt to use that too.

So could this work, I wonder?

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 3 years ago +3
    I'm far from being an expert, but this is my understanding of the basic principles in case it helps (this is 20 years out of date, but the basic stuff won't have changed too much). I think I'm duplicating…
  • michaelkellett
    michaelkellett over 3 years ago +2
    This will be harder than you think ! A long time ago (2006) I did work designing antennae for MIFARE (same thing, more or less) and it's quite tricky. NXP still are fairly active in this field and…
  • scottiebabe
    scottiebabe over 3 years ago +2
    It is possible for sure, but its not really a project I would recommend taking on without an oscilloscope. So if your looking for an excuse to purchase an MXO4 scope, id say go for it ;) I am Rx/Tx…
Parents
  • scottiebabe
    0 scottiebabe over 3 years ago

    It is possible for sure, but its not really a project I would recommend taking on without an oscilloscope.

    So if your looking for an excuse to purchase an MXO4 scope, id say go for it ;) 

    I am Rx/Tx USB-PD with the pio on a PI pico right now which is differential Manchester, so that could provide some inspiration  

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to scottiebabe

    Agree, unfortunately this is a project that's very unlikely to work, because there's several hurdles here; not just the hardware design and building of the receiver, but also the decoding complexity, it won't be a nice friendly stream of usable data all the time either, there will be noise to deal with so it needs some signal processing as well (can be partially in hardware and partially in software). It's all a major project, not a weekend thing. 

    If the Pico can be replaced with a PC and sound card, then that could make life easier to better understand the challenge and implement on the PC first perhaps, rather than coding for the Pico initially. But the signal would need to be mixed down to see it (e.g. with any SDR project hardware).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 3 years ago in reply to scottiebabe

    Agree, unfortunately this is a project that's very unlikely to work, because there's several hurdles here; not just the hardware design and building of the receiver, but also the decoding complexity, it won't be a nice friendly stream of usable data all the time either, there will be noise to deal with so it needs some signal processing as well (can be partially in hardware and partially in software). It's all a major project, not a weekend thing. 

    If the Pico can be replaced with a PC and sound card, then that could make life easier to better understand the challenge and implement on the PC first perhaps, rather than coding for the Pico initially. But the signal would need to be mixed down to see it (e.g. with any SDR project hardware).