• Products and Partners
    Products and Partners
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
Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum I have a small audio amplifier project I am working on.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 337 subscribers
  • Views 6822 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

I have a small audio amplifier project I am working on.

rcayot
rcayot over 3 years ago

  The power amplifier requires 12v ac *2 which I am providing via a 24v CT transformer.  I also have a preamplifier board which requires 12vDC for power.  I was wondering if I could tap each 12 feed for the power amp, and run each through a diode followed by a capacitor, would that rectify the source enough to be considered 12VDC?  If so, what value of cap do I need?

Roger

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +4
    It depends, but since a preamplifier might not consume much current, around 2200uF could be fine. However, the output won't be at precisely 12V, it will be a bit higher (as you'll see with a multimeter…
  • michaelkellett
    michaelkellett over 3 years ago in reply to rcayot +3
    The power supply voltage won't affect the gain of the power amplifier. There are some suggestions about changing the pre-amp to have a gain of 1 here: https://theartofsound.net/forum/showthread.php…
  • shabaz
    shabaz over 3 years ago in reply to rcayot +2
    Hi, You mention it is a 24V CT transformer, and that you wish to rectify it to 12V DC, so it can be wired as shown: If you actually have access to the amplifier circuit and can identify a 12V DC…
Parents
  • shabaz
    shabaz over 3 years ago

    It depends, but since a preamplifier might not consume much current, around 2200uF could be fine. However, the output won't be at precisely 12V, it will be a bit higher (as you'll see with a multimeter if you then measure it). This shouldn't be an issue for a preamplifier, but you may get better quality if supplied with the voltage it requires, with less ripple too. For that you could then also attach a voltage regulator like L4940D2T12-TR . Its circuit is in its datasheet. It is a surface-mount part but it's large and easy to attach to wires. A better option would be to get a small piece of copper-clad board, and just use a knife to score out some traces. This type of style basically, although it won't be intricate with the voltage regulator mentioned, it will be far easier.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    It depends, but since a preamplifier might not consume much current, around 2200uF could be fine. However, the output won't be at precisely 12V, it will be a bit higher (as you'll see with a multimeter if you then measure it). This shouldn't be an issue for a preamplifier, but you may get better quality if supplied with the voltage it requires, with less ripple too. For that you could then also attach a voltage regulator like L4940D2T12-TR . Its circuit is in its datasheet. It is a surface-mount part but it's large and easy to attach to wires. A better option would be to get a small piece of copper-clad board, and just use a knife to score out some traces. This type of style basically, although it won't be intricate with the voltage regulator mentioned, it will be far easier.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rcayot
    rcayot over 3 years ago in reply to shabaz

    I was scratching some stuff out, and I thought that half wave rectification would yield only 6v if fed 12ac.  With two diodes, it could be full wave, but still only 6v with some ripple.  The idea of a voltage regulator is good, but I am trying to develop more understanding of electronics, the point of the project.  The pre-amp is a cheap $12 dual tube basically a 'buffer' preamp. the preamp can be fed with a typical wall wort of 12v, suggested 1A capable.  IS there a way I can use the out of phase 2^12v outputs to rectify to 12v DC?

    I will try some stuff, thanks for your feedback, I will try to update on the project.

    Roger

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to rcayot

    Hi,

    You mention it is a 24V CT transformer, and that you wish to rectify it to 12V DC, so it can be wired as shown:

    image

    If you actually have access to the amplifier circuit and can identify a 12V DC rail, i.e. after rectification and filtering (through visual inspection and using a multimeter to check) then you could wire that to the pre-amp, and then you don't need the circuit above. If you have access to the 12V rail in the amplifier circuit, then there's no need for any diodes, and no need to try to connect the +12V and -12V rails with diodes (if that is what you were suggesting), because that won't work with DC rails that will be inside the amplifier. Besides, usually the preamplifier will use a very small amount of current*, so it doesn't matter if one rail has a slightly higher load than the other.

    If you wish to do the rectification yourself using the circuit shown above (and even if you'd used supply rails inside the amplifier circuit) then it won't be 12V, it will be slightly higher as mentioned, plus it will have some ripple. It may not be an issue for the preamplifier (it depends how good it is), but if it is an issue, then you will need a voltage regulator as mentioned earlier. You could try it without, and if the sound contains hum, then you'll likely at least need the voltage regulator, and probably careful audio wiring.

    * In your case, since you now mention it is a tube preamp, it may actually consume more current, you mention 1A which is probably 10 times more than a non-tube pre-amp, so you'll need to ensure the transformer can provide enough power for both the preamp and the amplifier.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rcayot
    rcayot over 3 years ago in reply to shabaz

    Thank you Shabaz, you are always so helpful to everyone.

    Roger