Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Upcycling a broken weather station: how to drive LCD segments from 3v3 logic?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 337 subscribers
  • Views 2974 views
  • Users 0 members are here
  • lcd
  • i2c
  • lowpower
  • spi
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Upcycling a broken weather station: how to drive LCD segments from 3v3 logic?

obones
obones over 3 years ago

I have here a Lacrosse Techonlogy / StarMeteo WD-4103F weather station that had misbehaving user buttons.
I thus opened it in order to fix them which I believe I did well. Before putting it back together, I wanted to test it and because the battery older is not on the PCB, I decided to power it from my benchtop power supply. And that's when a bug occurred in my mind which somehow thought that two C batteries would be 6V.

The LCD was a lot darker that usual, but it seemed to work for a bit. Nothing smoked but by the time I figured my error, I believe damage was done to the "brains" of that board.
Now, when I power it with regular batteries (or 3V) it starts up, but seems to deadlock after a while as can be seen on that video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I contacted the manufacturer support center but, unsurprisingly, they did not even reply to me.

Considering that the outside sensor can be read just well with an RTL-SDR and rtl_433, I have the project of changing the brains of the device, using the MAX32666FTHR board that I have sitting on my desk. It's a very low power device which is really appropriate in such a battery powered project, and because it supports BLE, I figured it could talk to one of the ESP32s that I already have around the house. This would make for this:

ESP32 gathers weather forecast from Internet and stores it, MAX32666 connects whenever it sees fit and displays it on the WD-4103F LCD.

I started my thought process by studying the main PCB which looks like this:

image

The row of pads at the center is what "touches" the LCD interface and so I would have to control it this way.

Having been allowed to use an X-Ray imager as an exceptional favor, I was able to see through the resin patch and this leads to this photo montage where I colored each track:

image

What's very interesting is that some LCD pads are connected together, and each have a test pad exposed onto which I could solder a connection wire.

My issue, and the object of my question, is how can I connect the LCD segments to the MAX32666?
I understand that LCDs require specific high voltage to operate but are there specialized low power chips that do this? And ideally a SPI or I2C solution because the dev board definitely does not have enough IO pins available for all LCD segments that need to be driven.

Many thanks in advance for any suggestion here.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +2
    I think you are unlikely to succeed here. The LCD display has at least 190 segments so you would need a driver chip with at least 28 pins (14 * 14 = 196). The MAX won't ever do this directly. It will…
  • dougw
    dougw over 3 years ago +1
    Have you checked the voltages on the card? Maybe some power supply component has sacrificed itself and replacing it will bring everything back to life.
  • shabaz
    shabaz over 3 years ago +1
    Hi, This is going to be very difficult. There are enough LCD segments on the display, that it won't be 'statically-driven' and will instead have multiplexed signals, using non-binary voltages, i.e. there…
Parents
  • michaelkellett
    0 michaelkellett over 3 years ago

    I think you are unlikely to succeed here. The LCD display has at least 190 segments so you would need a driver chip with at least 28 pins (14 * 14 = 196). The MAX won't ever do this directly.

    It will almost certainly be much cheaper to buy a little graphics display with a serial interface. It will also save you a huge amount of effort in trying to work out how the existing LCD is connected.

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • obones
    0 obones over 3 years ago in reply to michaelkellett

    Finding a new display that fits in that enclosure and is easily addressable while being cheap is something that I'm having a hard time doing.
    I mean, it's a 9cm x 9cm square area when most displays are 16:9 / 16:10 aspect ratio.
    The ED050SC epaper display seems to be roughly the correct size with a somewhat acceptable price (~20€) but a quick search could not lead to any documentation on how to drive it easily.
    Would you, by chance, have any suggestions in that matter?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 3 years ago in reply to obones

    From a quick look at internet it's obsolete and unobtainable. I couldn't find a datasheet. If you have the datasheet and can get the display then post the datsheet here (or a link to it) and I'll take a look. I wouldn't expect too much joy here because the description I found said it had a parallel interface.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • obones
    0 obones over 3 years ago in reply to michaelkellett

    Yeah, I'm not holding my breath either, it's just that it's the one that comes up with "5 inch epaper display".
    I found a datasheet here: https://z3d9b7u8.stackpathcdn.com/pdf-down/E/D/0/ED050SC3_PrimeView.pdf

    But if there are other options in the same price range, I'd be happy to have a look at them

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 3 years ago in reply to obones

    No chance with that - it needs about 20signal connections , 3.3V and +/- 15V supplies.

    I think you will just need move on here !

    You could easily graft in a 1/4VGA colour display with a serial interface but it won't be the right size or shape.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 3 years ago in reply to obones

    No chance with that - it needs about 20signal connections , 3.3V and +/- 15V supplies.

    I think you will just need move on here !

    You could easily graft in a 1/4VGA colour display with a serial interface but it won't be the right size or shape.

    MK