Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Struggling to select the correct Analog Switch
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 337 subscribers
  • Views 2202 views
  • Users 0 members are here
  • pt100
  • analog switch
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Struggling to select the correct Analog Switch

BigG
BigG over 3 years ago

I wish to create this circuit (not a fully complete design), where I am hijacking a Pt100 sensor for my own readings while still allowing an existing system to read the values correctly. I'm thinking that if I switch fast enough, with the help of smoothing capacitors, I could just about get away with it as there will be a fair bit of sampling and averaging to get a temperature value.

To do this, I decided to use an analog switch as these typically have low on resistance values. What I cannot figure out is whether I need a device like a Vishay DG419LEDY-T1-GE4 which has a signal range of -15V to 15V or I could use a SPDT analog switch with a lower voltage. I think I am correct in thinking that the max voltage of Vin is the max voltage allowed through the COM-NC pin etc.

I just wanted confirmation.

image

Of course, if there is an easier way to do this, I love to hear your views as I have a habit of over complication.

Thanks

Colin

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +3
    What is the existing system ? It may get very upset by the switching, or if are really lucky, you might not need switching at all. I have systems that measure using thermistors where one side if the…
  • BigG
    BigG over 3 years ago in reply to michaelkellett +1
    I was hoping not to switch but could not see how it would work without upsetting the system - I'm also working the principle that more resistance is better than lowering the overall resistance. With the…
  • scottiebabe
    scottiebabe over 3 years ago +1
    Step 1, solve the puzzle Step 2, win the prize Step 3, start probing around :)
Parents
  • michaelkellett
    0 michaelkellett over 3 years ago

    What is the existing system ?

    It may get very upset by the switching, or if are really lucky, you might not need switching at all.

    I have systems that measure using thermistors where one side if the the thermistor is grounded and the other connected to a resistor and the micro's adc port.

    When it's time to take the temperature the micro drives the other end of the resitor to 3.3V and measures the voltage across the thermistor. The duty cycle is very low.  A second measuring system could share the thermistor byt detecting when the owner had done a measurement and doing the second measurement in the dead time. So if you know the opwner system well you might not need any high spec switches.

    The switch you suggest has a series resitsance of about 20R and a  typical change of resistance of about 0.1R per degree C. The owner system would have to be recalibrated because this is a large resistance (40R) compared with the Pt100 sensor.  The Pt100 will change by about 0.3R per dgree C so the switch is comparable - this will probably stop the owner system from working at all.

    You can get switches with lower resistance but they won't handle so many volts.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 3 years ago

    What is the existing system ?

    It may get very upset by the switching, or if are really lucky, you might not need switching at all.

    I have systems that measure using thermistors where one side if the the thermistor is grounded and the other connected to a resistor and the micro's adc port.

    When it's time to take the temperature the micro drives the other end of the resitor to 3.3V and measures the voltage across the thermistor. The duty cycle is very low.  A second measuring system could share the thermistor byt detecting when the owner had done a measurement and doing the second measurement in the dead time. So if you know the opwner system well you might not need any high spec switches.

    The switch you suggest has a series resitsance of about 20R and a  typical change of resistance of about 0.1R per degree C. The owner system would have to be recalibrated because this is a large resistance (40R) compared with the Pt100 sensor.  The Pt100 will change by about 0.3R per dgree C so the switch is comparable - this will probably stop the owner system from working at all.

    You can get switches with lower resistance but they won't handle so many volts.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • BigG
    0 BigG over 3 years ago in reply to michaelkellett

    I was hoping not to switch but could not see how it would work without upsetting the system - I'm also working the principle that more resistance is better than lowering the overall resistance. With the switching scenario I thought that maybe using decoupling or smoothing capacitors could be used to handle millisecond switch time.

    The Pt100 is wired into a control panel, which is locked. The Pt100 is simply used to trigger a warning light to indicate a motor is hot to touch. That's all you get so I want to add in my little monitoring system to capture temperature over time etc. I'm not sure of the voltage used, but as it's out of my control I have assumed for now that it is 12V as the distance between pt100 and control panel is +10metres or so - my wireless device will be much closer to the pt100 sensor. On the control panel you can recalibrate by changing the temperature threshold value to trigger the warning light. I have no other way to accessing the measuring point so need to use same sensor.

    As you have already highlighted a different switch would be better as it has lower resistance values.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 3 years ago in reply to michaelkellett

    I would be curious, however, to learn what a non switching "piggy-pack" circuit would look like if the source voltage from the control panel is much higher than my mcu can handle etc.

    Just wanted to add that the reason I like analog switches is the really fast switching time, so you have no dead time. Then I'm assuming my ADC on my MCU can measure a value in milliseconds, I can take a reading, switch back to allow the control panel to do its thing and with help of capacitors not worry too much about the voltage ripple, and then I repeat a second later to collect a decent sample (thinking 5 readings would do it) and then can wait say 30 seconds etc.