Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum LT8361 voltage doubler won't start under load .....HELP Please!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 337 subscribers
  • Views 2166 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

LT8361 voltage doubler won't start under load .....HELP Please!

davebullockmbe
davebullockmbe over 3 years ago

Hi,

Hi experts,

I need some SMPSU expert help using an LT8361 as a voltage doubler please.

Hi, I have been using the LT8361 as a +90V power supply stepping up from 12V for several years. (schematic attached below).
My application has a load of less than 10mA and with this design the power supply will start up with or without load every time. 
I now have the need to generate 120V and as the LT8361 doesn't support this voltage, (100V max) the obvious solution is to use it as a voltage doubler.
I spotted that this had been published as a -150V supply in an Analog application. (so surely it was tried and tested here) 
https://ez.analog.com/power/f/q-a/112621/searching-for-an-inverting-converter-solution/336141

  
So I generated a similar design but for +120V (attached below)
The design works fine and the regulation is very good as I only need a few milliamps at 120V.
The problem is that whilst my original +90V LT8361 design will start up when (anywhere between +7V and +12V) is applied IMMEDIATELY. 
The Voltage doubling circuit will only start when the 12V supply is slowly ramped up from zero under load.
ie. applying 12V immediately the LT8361 doesn't start.  (even with a load as low as 3mA).
(it starts every time with no load BTW!)

I initially thought that the IC was detecting too high a starting current and was going into overload shutdown.
I increased the Slow Start capacitor to 0.22uF but this made no difference.
I have tried reducing the value of C5/C6 (both output caps) down to 0.1uF each and the LT8361 still will NOT start under load which seems to suggest it isn't 'inrush' current into the output capacitors?
I tried taking the voltage feedback point from the junction of C5/C6 instead of the Vout in case it was taking too long for the FBX input to see sufficient voltage thus going into a LVO scenario.
I reduced the 1M to 510K to keep the voltage division correct. As expected the Vout regulation was poorer but the LT8361 still refused to start under load!
I also tried increasing the value of C7 in case output capacitor C6 wasn't charging fast enough at switch on thus creating a UVLO situation.
Again this made NO difference.

I have two of these boards assembled and both exhibit the same problem.
I need some help from a more experienced SMPSU expert...PLEASE

Thanks in anticipation
Dave
Dave 
imageimage

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +3
    It can be done: I think a transformer would be a much better solution than the cap and diode charge pump. Before you make this check that you are happy with the currents in the 8361 switch. You…
  • davebullockmbe
    davebullockmbe over 3 years ago in reply to michaelkellett +3
    Hi Michael, You are a genius :-) Your R3 in that position has cured my issue thankyou! I had tried series resistors in both D1 and D2's cathodes to no avail, I never thought of trying it in series…
  • michaelkellett
    michaelkellett over 3 years ago +2
    Have you tried to simulate your circuit in LTSpice. If not then I very strongly siggest that you do - it will give a great deal more insight as to why it isn't working - or maybe show you that is should…
Parents
  • michaelkellett
    0 michaelkellett over 3 years ago

    Have you tried to simulate your circuit in LTSpice.

    If not then I very strongly siggest that you do - it will give a great deal more insight  as to why it isn't working - or maybe show you that is should work.

    BTW - quick guess is that there a current spikes when the capacitor charge pump (your doubler) tries to work and the solution will be resistors in series with (some of) the caps.

    The simulator will help you sort this.

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 3 years ago

    Have you tried to simulate your circuit in LTSpice.

    If not then I very strongly siggest that you do - it will give a great deal more insight  as to why it isn't working - or maybe show you that is should work.

    BTW - quick guess is that there a current spikes when the capacitor charge pump (your doubler) tries to work and the solution will be resistors in series with (some of) the caps.

    The simulator will help you sort this.

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • davebullockmbe
    0 davebullockmbe over 3 years ago in reply to michaelkellett

    HI Michael,

    Thanks for your input.
    Yes I had LTspiced the doubler circuit when I first decided to build the design and it worked in the simulation.
    However, I have just looked back at my LTspice model and what I didn't do was add an output load...dooooh!

    Whilst I felt you may be correct about the current spikes in the o/p caps, I would have expected that reducing their value from 3u3F down to 0.1uF would have cured the problem but it doesn't.
    Also why does the NON doubling circuit work with a 3u3F surely it's the same as regards current spikes?
    I have just removed C7 and D1 and changed the connection for R1 to the junction of C5/C6 such that it's now a NON doubling configuration.
    This now starts up under any load condition.
    So it is an issue with the additional D1/C7/C6 that is stopping the IC from starting.

    I will add an o/p load to my LTspice simulation later this afternoon and see if this still works or stops it dead!
    Watch this space......

    Thanks
    Daveimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • davebullockmbe
    0 davebullockmbe over 3 years ago in reply to davebullockmbe

    Hi Michael,

    Well it looks like should have simulated it with a load ..silly me :-(
    No matter what parameters I change, add resistors in series with the diodes, change the values of C2/C3 or C4 nothing coaxes it to fire all the way up to full output.
    I am stumped.
    Incidentally I just loaded up my NON doubling LTSpice simulation with various loads from none right up to 25mA and the LT8361 drove the output to full programmed voltage every time.
    I just can't understand why the addition of the 'doubling' components causes it to fail to ramp up, just idling at a low voltage instead.
    Next step is to LTsimulate the -150V example in the LT8361 datasheet and see if that actually works, or was just an untested pipe dream?

    I wonder if anyone has ever got a doubler to work with an LT8361........

    Thanks
    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 3 years ago in reply to davebullockmbe

    The chip works by comparing the instantaneous inductor current to the feedback voltage to turn off the inductor current, so feedback waveform and timing are very important.

    Things to try....(simulate)

    If you do like one of your attempts with the feedback coming from the capacitor junction and reduce the upper cap, or increase the lower cap, timing should look more and more like the original design - from the the chip's perspective.

    Placing a very small cap across one or other of the feedback resistors would change the feedback waveform, either speeding up or slowing down the response, depending on which resistor had the cap. The upper resistor might need a resistor and a cap to keep the feedback voltage within limits.