Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Deciding on a DMM, USB logic analyser, and power profiler.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 336 subscribers
  • Views 4200 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Deciding on a DMM, USB logic analyser, and power profiler.

Hari-Seldon
Hari-Seldon over 3 years ago

Would love your advice on both logic analyzers, DMM, and a power profiler.

I've got a, let's call it semi-serious electronics habit and I'm doing some design using an ESP32C3 and a DWM1000 (UWB chip) communicating over I2C.  I've also got some sensor packages using SPI.  Debugging is a nightmare without a logic analyzer and I'm looking for an appropriate device in a "serious hobbyist" budget (ideally under £600) and without a month-long wait!

I'd also like a good handheld DMM with auto ranging, temperature, and a stable kickstand/probes!  Is there a particular one you like?

Finally, would love your input on a way of measuring power consumption of the device.  I'm looking at the Nordic Power Profiler Kit II, would you have another suggestion or is that a good one?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago in reply to fmilburn +2
    This is the circuit I'm using. It measures high side current through R100 and drives the same current throught R104, R105 and R106. It was extracted from a bigger design so apologies for the odd net…
  • michaelkellett
    michaelkellett over 3 years ago +1
    I have two logic analysers which I recomend: This one https://thedebugstore.com/products/zeroplus-lap-c-logic-cube-analyser-uk and this one: https://thedebugstore.com/products/zeroplus-lap-c-pro…
  • javagoza
    javagoza over 3 years ago in reply to charlieo21 +1
    If you only need the Logic Analyzer I think the Digital Discovery is a better option Analog Discovery 2. https://www.newark.com/digilent/410-321/pc-based-oscilloscope-30mhz-10msps/dp/40AH1640…
Parents
  • michaelkellett
    0 michaelkellett over 3 years ago

    I have two logic analysers which I recomend:

    This one

    https://thedebugstore.com/products/zeroplus-lap-c-logic-cube-analyser-uk

    and this one:

    https://thedebugstore.com/products/zeroplus-lap-c-pro-logic-protocol-analyser-uk?variant=40764571812029

    I've found them to be way better than any scope based logic analyser.

    For power measuring I've used a Joulescope but don't much like it - I've taken to making my own (1 op-amp - a P channel MOSFET and some Rs and using with a low noise scope.

    Might be your best bet is to go for a Fluke that's in your price range - they last forever and are portable - just checked and the nice ones are too pricey.

    SO my advice would go for a cheap handheld and save up or buy a secondhand bench top DMM.

    The Siglent SDM3065X almost gets into yur budget but I haven't used one and I'd be a bit reluctant to spend that much on a  Chinese brand DMM.

    The Keithley DMM6500 is great but expensive.

    If you want to use your DMM to measure power you will need one with selectable DC time contants and ideally fast (20kHz+) sampling. Or use a scope.

    If you want the ciruit of my current measuring amplifier let me know and I'll post it here.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fmilburn
    0 fmilburn over 3 years ago in reply to michaelkellett

    Hi Michael,

    I’m curious what you use for current measurement 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 3 years ago in reply to fmilburn

    This is the circuit I'm using. It measures high side current through R100 and drives the same current throught R104, R105 and R106.

    It was extracted from a bigger design so apologies for the odd net names.

    With the values shown you get 10mV per mA

    The OPA192 has a very low offset and rail to rail IO. It needs at least 5V to work. V5F is the supply for the op amp and could be increased if you needed a higher supply voltage to the DUT. V5F should be at least 0.5V above SW_3V3_PWR.

    C100 sets the rise time of the amp to about 22us, you can speed it up (or slow it down) by changing C100.

    You can look at dynamic currents with a scope across R106 aor measure average current with a DMM so long as it has a long enough integration time.

    I built my first version of this on stripboard and it worked fine.

    Q100 is a tiny PMF170XP - if you increase the supply and run at high currents it will fry - but larger parts will work.

    Its not a good design for battery power testing because it doubles the current drain of the DUT.

    MKimage

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fmilburn
    0 fmilburn over 3 years ago in reply to michaelkellett

    Thanks, I am going to try and set aside some time to model it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fmilburn
    0 fmilburn over 3 years ago in reply to michaelkellett

    Thanks, I am going to try and set aside some time to model it