Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How to interpret MAX11203 AD-converter self calibration bitvalue?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 300 subscribers
  • Views 2040 views
  • Users 0 members are here
  • ad converter
  • MAX11203
  • self calibration
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How to interpret MAX11203 AD-converter self calibration bitvalue?

Engztrom
Engztrom over 2 years ago

Hi,

What is the exact relationship between the self calibration gain bitvalue and the actual scaling it does?
E.g.what bitvalue would be measured with a saturated input (maximum voltage measured) and
the self calibration gain set to, say, 0xBFFFFF and the self calibration offset set to 0x000000?
The datasheet is very vague about that. This is all it says:
:
"SCGC: Self-Calibration Gain Register

The self-calibration gain register is a 24-bit read/write register. The data written/read to/from this register is clocked
in/out MSB first. This register holds the self-calibration gain calibration value. The format is always in two’s complement
binary format. A write to the self-calibration register is allowed. The written value remains valid until it is either rewritten
or until an on-demand self-calibration operation is performed, which overwrites the user-supplied value. Any attempt
to write to this register during an active calibration operation is ignored.
The self-calibration gain value is used to scale the self-calibration offset corrected conversion result before the system
offset and gain calibration values have been applied, provided the NOSCG bit in the CTRL3 register is set to 0. The
self-calibration gain value scales the self-calibration offset corrected conversion result by up to 2x or can correct a gain
error of approximately -50%. The gain is corrected to within 2 LSB."

And it also mention SCGC=0xBFD345 and SCOC=0x00007E as an example of values you can get when the self calibration is carried out.

Thanks for any help!

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 2 years ago +1
    I had a look at the data sheet yesterday and it didn't make too much sense to me either ! I think your best bet is to get the part connected up with an adjustable DC input and some means of tweeking…
  • Engztrom
    Engztrom over 2 years ago in reply to shabaz +1 verified
    It is important because (whatever the datasheet says) it seems to be necessary to have some kind of calibration values set. In theory (as we interpret the very fuzzy datasheet) it should work fine skipping…
  • shabaz
    shabaz over 2 years ago in reply to Engztrom +1 verified
    Hi, Regarding " But what exactly does these written down bitvalues represent? " That's my point - why does it matter? _If_ you deem that you have to do calibration anyway (whether it is self calibration…
Parents
  • michaelkellett
    0 michaelkellett over 2 years ago

    I had a look at the data sheet yesterday and it didn't make too much sense to me either !

    I think your best bet is to get the part connected up with an adjustable DC input and some means of tweeking the registers and reading the ADC  - then have  a play with it to see what it does,

    The thing that confused me about the desctiption was the refence to the register values being 2s compliment - which implies signed and then the example gain settings are negative. My guess is that the offset is 2s compliment but that the gain is unsigned - but you'll need to test it.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Engztrom
    0 Engztrom over 2 years ago in reply to michaelkellett

    Yes, the datasheets are very crude, confusing and (possibly) erroneous!
    In order to implement self- or system calibration we would have to tweak the hardware so ratiometric connection is not used during calibration (that is Plan B...)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Engztrom
    0 Engztrom over 2 years ago in reply to michaelkellett

    Yes, the datasheets are very crude, confusing and (possibly) erroneous!
    In order to implement self- or system calibration we would have to tweak the hardware so ratiometric connection is not used during calibration (that is Plan B...)