Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum config TIMER1 on pic24fj128GA202 for 1s. (SOLVED)
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 336 subscribers
  • Views 4669 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

config TIMER1 on pic24fj128GA202 for 1s. (SOLVED)

hazard
hazard over 3 years ago

I hello. I'm trying , config the timer1 from pic24fj128ga, but without success. anyone there can´try to help me, please.

I already have config the configuration bit. I have the REFO with 16MHz.

image

// CONFIG4
#pragma config DSWDTPS = DSWDTPS1F      // Deep Sleep Watchdog Timer Postscale Select bits (1:68719476736 (25.7 Days))
#pragma config DSWDTOSC = LPRC          // DSWDT Reference Clock Select (DSWDT uses LPRC as reference clock)
#pragma config DSBOREN = OFF            // Deep Sleep BOR Enable bit (DSBOR Disabled)
#pragma config DSWDTEN = OFF            // Deep Sleep Watchdog Timer Enable (DSWDT Disabled)
#pragma config DSSWEN = OFF             // DSEN Bit Enable (Deep Sleep operation is always disabled)
#pragma config PLLDIV = PLL4X           // USB 96 MHz PLL Prescaler Select bits (4x PLL selected)
#pragma config I2C1SEL = DISABLE        // Alternate I2C1 enable bit (I2C1 uses SCL1 and SDA1 pins)
#pragma config IOL1WAY = OFF            // PPS IOLOCK Set Only Once Enable bit (The IOLOCK bit can be set and cleared using the unlock sequence)

// CONFIG3
#pragma config WPFP = WPFP0             // Write Protection Flash Page Segment Boundary (Page 0 (0x00))
#pragma config SOSCSEL = OFF            // SOSC Selection bits (Digital (SCLKI) mode)
#pragma config WDTWIN = PS25_0          // Window Mode Watchdog Timer Window Width Select (Watch Dog Timer Window Width is 25 percent)
#pragma config PLLSS = PLL_FRC          // PLL Secondary Selection Configuration bit (PLL is fed by the on-chip Fast RC (FRC) oscillator)
#pragma config BOREN = OFF              // Brown-out Reset Enable (Brown-out Reset Disabled)
#pragma config WPDIS = WPDIS            // Segment Write Protection Disable (Disabled)
#pragma config WPCFG = WPCFGDIS         // Write Protect Configuration Page Select (Disabled)
#pragma config WPEND = WPSTARTMEM       // Segment Write Protection End Page Select (Write Protect from page 0 to WPFP)

// CONFIG2
#pragma config POSCMD = NONE            // Primary Oscillator Select (Primary Oscillator Disabled)
#pragma config WDTCLK = LPRC            // WDT Clock Source Select bits (WDT uses LPRC)
#pragma config OSCIOFCN = OFF           // OSCO Pin Configuration (OSCO/CLKO/RA3 functions as CLKO (FOSC/2))
#pragma config FCKSM = CSDCMD           // Clock Switching and Fail-Safe Clock Monitor Configuration bits (Clock switching and Fail-Safe Clock Monitor are disabled)
#pragma config FNOSC = FRCPLL           // Initial Oscillator Select (Fast RC Oscillator with PLL module (FRCPLL))
#pragma config ALTCMPI = CxINC_RB       // Alternate Comparator Input bit (C1INC is on RB13, C2INC is on RB9 and C3INC is on RA0)
#pragma config WDTCMX = WDTCLK          // WDT Clock Source Select bits (WDT clock source is determined by the WDTCLK Configuration bits)
#pragma config IESO = OFF               // Internal External Switchover (Disabled)

// CONFIG1
#pragma config WDTPS = PS32768          // Watchdog Timer Postscaler Select (1:32,768)
#pragma config FWPSA = PR128            // WDT Prescaler Ratio Select (1:128)
#pragma config WINDIS = OFF             // Windowed WDT Disable (Standard Watchdog Timer)
#pragma config FWDTEN = OFF             // Watchdog Timer Enable (WDT disabled in hardware; SWDTEN bit disabled)
#pragma config ICS = PGx1               // Emulator Pin Placement Select bits (Emulator functions are shared with PGEC1/PGED1)
#pragma config LPCFG = OFF              // Low power regulator control (Disabled - regardless of RETEN)
#pragma config GWRP = OFF               // General Segment Write Protect (Write to program memory allowed)
#pragma config GCP = OFF                // General Segment Code Protect (Code protection is disabled)
#pragma config JTAGEN = ON              // JTAG Port Enable (Enabled)

// #pragma config statements should precede project file includes.
// Use project enums instead of #define for ON and OFF.

#include <xc.h>

the timer.c its config:


#include <stdio.h>
#include <stdlib.h>
#include <stdbool.h>
#include <xc.h>

#include "Timer1.h"

uint16_t timer_delay_ms_UI16 = 0;
uint16_t timer_heartbeat_ms_UI16 = 250;
 
/* Example code for Timer1 ISR*/
void __attribute__((__interrupt__, __no_auto_psv__)) _T1Interrupt(void)
{
    /* Interrupt Service Routine code goes here */
//    if(timer_delay_ms_UI16>0)
//    {
//        timer_delay_ms_UI16--;
//    }
//    if(timer_heartbeat_ms_UI16>0)
//    {
//        timer_heartbeat_ms_UI16--;
//    }
    
    timer_delay_ms_UI16=1;
    IFS0bits.T1IF = 0; //Reset Timer1 interrupt flag and Return from ISR

}

void my_delay_ms(uint16_t time_to_my_delay_UI16)
{
    timer_delay_ms_UI16 = time_to_my_delay_UI16;
    while(timer_delay_ms_UI16>0);  
}     

 void Init_TIMER(void)
{
    /* The following code example will enable Timer1 interrupts, load the Timer1
    Period register and start Timer1.
     *
    When a Timer1 period match interrupt occurs, the interrupt service
    routine must clear the Timer1 interrupt status flag in software.
    */
    TMR1 = 0x00;//Clear contents of the timer register
    T1CON = 0x00;//Stops the Timer1 and reset control reg.
    TMR1 = 0x00;//Clear contents of the timer register
    
    //Set Timer 1 period register
    //Fosc = 32 KHz
    //Tosc= 1/32k=31.25us
    //Tcy(s) = TOSC * 2 =  62.5us
    //Timer1 period = Tcy * Prescaler * PR1
    //1000ms = (62.5us) * 256 * PR1
    //PR1 = 1000ms / (31.25us) * 256
    PR1 = 32E-6; //config para 1s a on e 1s a off
    
    //Setup Timer1 interrupt for level 1 priority
    IPC0bits.T1IP2=0;//(This example assigns level 1 priority)
    IPC0bits.T1IP1=0;
    IPC0bits.T1IP0=1;
    
    //config Timer1 interrupt
    IFS0bits.T1IF = 0;//Clear the Timer1 interrupt status flag
    IEC0bits.T1IE = 1;//Enable Timer1 interrupts
    
    //Select the timer prescaler ratio using the TCKPS<1:0> bits.
    T1CONbits.TCKPS1=0;//00=1:1
    T1CONbits.TCKPS0=0;//11=1:256
    
    //Set the Clock and Gating modes using the TCS, TECS<1:0> and TGATE bits.
    T1CONbits.TCS=0;//the Timer is clocked from the internal system clock (FOSC/2).
    
    //Set or clear the TSYNC bit to configure synchronous or asynchronous operation.
    T1CONbits.TGATE=0;//Gated time accumulation is disabled
    //T1CONbits.TSYNC=0;//When TCS=0 This bit is ignored.
    T1CONbits.TON = 1; //Start Timer1

   
}

the main code is:

bool teste(void);
bool estado_led=true;

int main(void)
{
    Init_PIC();
    GPIO_config();
    Init_TIMER();
    
    
    
    
    
    while(1)
    {
        //LATBbits.LATB14 = 1;
                
        //LATBbits.LATB14 = 0;
      
        
        //handles
//        estado_led=teste();
//        
//        if(estado_led == true)
//        {
//           
//            //turn on output0=RB14
//            LATBbits.LATB14 = 1;
//            //timer_delay_ms_UI16 = 1;
//            //estado_led = false;
//        }
//        if(estado_led == false)
//        {
//           _LATB14=0;//turn off output0=RB14
//            //timer_delay_ms_UI16 = 0;
//        }
            
        //return 1;
        if(timer_delay_ms_UI16==0)
        {
            LATBbits.LATB14 = 0;
            timer_delay_ms_UI16=1000;
        }
        else
        {
            _LATB14=1;
            
        }
    }
    
    
    
    
    
    
    
    
    
    
    return 0;
}
//func
bool teste(void)
{
    //for read pin uso PORTx
    if(PORTAbits.RA2)//se a porta estiver a 1 executa o conteudo do if
    {
        //estado_led = true;
        //turn on output0=RB14
        //LATBbits.LATB14=1;
        return true;
    }
    else
    {
        //estado_led = false;
        //for write pin uso LATx
        //_LATB14=0;//turn off output0=RB14
        return false;
    }
}

If some one else can help I Will appreciate the time and the help. thanks you much

GPIO/PIC (FOSC, ...) config:

#include <xc.h>
#include <stdio.h>
#include <stdlib.h>
#include <p24FJ128GA202.h>
#include "pic.h"

void Init_PIC(void)
{
    //**IOLOCK: I/O Lock Enable bit(2)**//
    //__builtin_write_OSCCONL(OSCCON & 0xbf);//unlock sequence start
    //OSCCONbits.IOLOCK=1;//1 = I/O lock is active
    //__builtin_write_OSCCONL(OSCCON | 0x40);//unlock sequence end
    ///////control bits register///////
    //while(OSCCONbits.LOCK!=1){};//pag5 ds39700  
                                
                               /*####################################*/
                               /*OSCCON: OSCILLATOR CONTROL REGISTER*/
                               /*##################################*/

//  __builtin_write_OSCCONL(OSCCON & 0xbf);//unlock sequence start
//  //**NOSC<2:0>: New Oscillator Selection bits**//disable on config_bit.c
//  OSCCONbits.NOSC2=1;//111 = Fast RC Oscillator with Postscaler (FRCDIV)
//  OSCCONbits.NOSC1=1;//no need config, is config by default in config_bit.c FNOSCX
//  OSCCONbits.NOSC0=1;//apos um reset um power one etc o mcu arranca com o osc pre definido no COSC<2:0>
//  __builtin_write_OSCCONL(OSCCON | 0x40);//unlock sequence end
   
        //**CLKLOCK: Clock Selection Lock Enable bit**//
    //OSCCONbits.CLKLOCK=1//If FSCM is Enabled(FCKSM1=1)/CLKLOCK=1-Clock and PLL selections are locked
    //If FSCM is Disabled(FCKSM1=0):Clock and PLL selections are never locked and may be modified by setting the OSWEN bit.
   
    //**POSCEN: Primary Oscillator Sleep Enable bit(4)**//
    OSCCONbits.POSCEN=0;//0 = Primary Oscillator is disabled during Sleep mode
    OSCCONbits.SOSCEN=0;//0 = Disable Secondary Oscillator
    //OSWEN: Oscillator Switch Enable bit
    OSCCONbits.OSWEN=0;//0 = Oscillator switch is complete

    __builtin_write_OSCCONL(OSCCON | 0x40);//unlock sequence end
    
                            /*###############################*/
                            /*CLKDIV: CLOCK DIVIDER REGISTER*/
                            /*#############################*/
    //RCDIV<2:0>: FRC Postscaler Select bits
    CLKDIVbits.RCDIV2=1;//111 = 31.25 kHz (divide-by-256)
    CLKDIVbits.RCDIV1=1;//000 = 8 MHz (divide-by-1)
    CLKDIVbits.RCDIV0=1;
    //DOZE<2:0>: CPU Peripheral Clock Ratio Select bits
    //CLKDIVbits.DOZE2=0;//111=CPU peripheral clock ratio is set to 1:128
    //CLKDIVbits.DOZE1=0;//not need config DOZEN bit is clear
    //CLKDIVbits.DOZE0=0;
    //Doze Mode Enable bit
    //CLKDIVbits.DOZEN=0;//0=CPU peripheral clock ratio is set to 1:1
    //PLLEN: PLL Enable bit
    //CLKDIVbits.PLLEN=0;//0 = PLL is disabled
   
    /*Reference Clock Output Control Register (REFOCON)*/
    REFOCONLbits.ROEN=1;//enable the module
    REFOCONLbits.ROOUT=1;//makes the clock signal available on the REFO pin
    REFOCONHbits.RODIV=0;//No Divide
   
   
   
                                       /*########################*/
                                       /*SR: ALU STATUS REGISTER*/
                                       /*######################*/
    //**DC: ALU Half Carry/Borrow bit**//
    SRbits.DC=1;//1 = A carry out from the 4th low-order bit (for byte-sized data) or 8th low-order bit (for word-sized data) of the result occurred
   
    //**IPL<2:0>: CPU Interrupt Priority Level Status bits**//
    SRbits.IPL2=1;//100 = CPU Interrupt Priority Level is 4 (12)
    SRbits.IPL1=0;
    SRbits.IPL0=0;
    //**N: ALU Negative bit**//
    SRbits.N=1;//1 = Result was negative
    //**OV: ALU Overflow bit**//
    SRbits.OV=1;//1 = Overflow occurred for signed (2?s complement) arithmetic in this arithmetic operation
   
   
                                       /*##################################*/
                                       /*CORCON: CPU CORE CONTROL REGISTER*/
                                       /*################################*/
    /*IPL3: CPU Interrupt Priority Level Status bit*/
    /*CORCONbits.IPL3=0;//CPU Interrupt Priority Level is 7 or less*/


}

void GPIO_config(void)
{
    /*TRISX config:PORTx Data Direction Control register (1=INPUT or 0=OUTPUT)*/
    /*PORTx: I/O Port register*/ //for read
    /*LATx: PORTx Data Latch register*/ //for write
    /*ODCx: PORTx Open-Drain Control register*/ //for external VCC
        
    
    /*RA2-digital input0 pin 9 */
    ANSAbits.ANSA2=0;//digital
    TRISAbits.TRISA2=1;//input
    Nop();
    
    /*RA3-digital input1 pin10 */
    ANSAbits.ANSA3=0;//digital
    TRISAbits.TRISA3=1;//input
    Nop();
    
    /*RB12-analog input0 remap pins pin 23 */
    ANSBbits.ANSB12=1;//analog
    TRISBbits.TRISB12=1;//input
    Nop();
    
    /*RB13-analog input1 remap pins pin 24 */
    ANSBbits.ANSB13=1;//analog
    TRISBbits.TRISB13=1;//input
    Nop();

    /*RB14-digital output0 remap pins pin 25 */
    ANSBbits.ANSB14=0;//digital
    TRISBbits.TRISB14=0;//output
    Nop();
    
    /*RB15-digital (open-drain) output1 remap pins pin 26 */
    ANSBbits.ANSB15=0;//digital
    TRISBbits.TRISB15=0;//output
    //ODCBbits.ODB15=1;//open-drain
    Nop();
    
    /*Pullup resistor config*///pag171
    CNPU2bits.CN30PUE=1;//enable pullup resistor on pin RA2 (digita input0)
    CNPU2bits.CN29PUE=1;//enable pullup resistor on pin RA3 (digita input1)
            
            
    //TRISAbits.TRISA0=1;//input RA0
    //TRISAbits.TRISA1=1;//input RA1
    //TRISAbits.TRISA2=1;//input RA2
    //TRISAbits.TRISA3=1;//input RA3
    //TRISBbits.
            
    LATAbits.LATA0=0;//low
    LATAbits.LATA1=0;//low
    LATAbits.LATA2=0;//low
    LATAbits.LATA3=0;//low
}

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago in reply to hazard +3
    AndrewJ also gives good advice setting the IPL, I copied some of your code into a blank project and ran it on the simulator /* * File: newmainXC16.c * Author: Scottie * * Created on April 1,…
  • Jan Cumps
    Jan Cumps over 3 years ago +2
    Have you seen MicroE's PIC Timer Configurator? https://www.mikroe.com/blog/timer-calculator-1-50-now-supports-dspic-pic24-and-pic32 It can give you a headstart to get a grip on all the registers
  • Andrew J
    Andrew J over 3 years ago +2
    There's a lot going on here: I would cut this right down to the bare minimum and see what happens. It's not necessary to set bits in registers individually and it *may* make it clearer if you set the register…
Parents
  • Jan Cumps
    Jan Cumps over 3 years ago

    Have you seen MicroE's PIC Timer Configurator?

    https://www.mikroe.com/blog/timer-calculator-1-50-now-supports-dspic-pic24-and-pic32

    It can give you a headstart to get a grip on all the registers

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • hazard
    hazard over 3 years ago in reply to Jan Cumps
    Jan Cumps said:
    It can give you a headstart to get a grip on all the registers

    thanks for the tip.

    I already have re check all register, but I don´t find the problem.

    I think ISR it's never been call.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to hazard

    In your post, you don't say what you want to do, or what your problem is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hazard
    hazard over 3 years ago in reply to Jan Cumps

    I wanna config the timer1 from pic24fj128GA202, the problem is the ISR not been call.

    I wanna togle a led state.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to hazard

    why this: "_LATB14=1;" and not "LATBbits.LATB14 = 1;" as you do when you set it off?  Again, I don't know if this is a problem or not - I assume it compiles - but I come back to my comment below.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andrew J
    Andrew J over 3 years ago in reply to hazard

    why this: "_LATB14=1;" and not "LATBbits.LATB14 = 1;" as you do when you set it off?  Again, I don't know if this is a problem or not - I assume it compiles - but I come back to my comment below.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • hazard
    hazard over 3 years ago in reply to Andrew J

    it's the same,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to Andrew J

    Also, where are you registering the ISR as the routine for Timer 1 - in Timer1.h?  This chip uses vector tables so the entry for Timer1 must be set to the address of the actual ISR.  Here's a Microchip example to help you: https://microchipdeveloper.com/projects:16bit-interrupts

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hazard
    hazard over 3 years ago in reply to Andrew J

    my code in timer.h

    #include <xc.h> // include processor files - each processor file is guarded.  
    #include <stdint.h>        /* Includes uint16_t definition                    */
    #include <stdbool.h>       /* Includes true/false definition                  */
    #include <stdio.h>
    #include <stdlib.h>

    extern uint16_t timer_delay_ms_UI16;
    extern uint16_t timer_heartbeat_ms_UI16;



    void my_delay_ms(uint16_t time_to_my_delay_UI16);
    void Init_TIMER(void);


    I think it's not need do prototype of ISR in time.h

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hazard
    hazard over 3 years ago in reply to Andrew J

    I tryng re-config de pic_config.c

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to hazard

    You misunderstood: it's not defining the prototype it's registering the ISR routine into the Vector table for Timer1 interrupt so that the PIC knows what address to call when the interrupt occurs.  Is that what the function definition itself does perhaps by calling it _T1Interrupt(void)?  Sorry, I'm not that familiar with this PIC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hazard
    hazard over 3 years ago in reply to Andrew J

    sorry maybe it's that my problem, . but i'm not  sure what you talk about.