Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How to know wire polarity in an open circuit without any electrical power?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 335 subscribers
  • Views 11578 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How to know wire polarity in an open circuit without any electrical power?

z234
z234 over 3 years ago

Dear friends, thank you for all your kind help.

How to know wire polarity in an open circuit without any electrical power? E.g. you have a dashcam with 2 wires with same color insulation. How do you know which is positive and which is negative?

If you plug wires wrongly into the battery, a short circuit may happen and damage the dashcam.

How to test for wire polarity in this open circuit then?

Thank you very much 

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +4
    You measure *continuity* using the continuity/ohms setting on your multimeter to determine which of your two same coloured wires go to positive or negative. Alternatively, apply power to one side of…
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to z234 +1
    z234 said: How do u see the ohms which is positive or negative by testing continuity? Does the numbers of ohms determine POS or neg ? Ohms can only be positive value. The range is from 0 to infinity…
Parents
  • Gough Lui
    0 Gough Lui over 3 years ago

    You measure *continuity* using the continuity/ohms setting on your multimeter to determine which of your two same coloured wires go to positive or negative.

    Alternatively, apply power to one side of the wire while the load is disconnected, using the multimeter in volts to determine polarity.

    The wire may be the same colour but also may have a subtle stripe down one side. This can indicate negative, but this is not universal.

    Otherwise, ask the manufacturer, or disassemble the device and test for continuity of the wire to a polarised component (e.g. the negative of an electrolytic capacitor on the input).

    - Gough

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • z234
    0 z234 over 3 years ago in reply to Gough Lui

    Dearest Gough,

    I have followed ur advice n did a partial power on , without closing the circuit. I was able to detect polarity using a digital multimeter. Tq very much.

    How do u see the ohms which is positive or negative by testing continuity? Does the numbers of ohms determine POS or neg ? Tq very much

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to z234
    z234 said:
    How do u see the ohms which is positive or negative by testing continuity? Does the numbers of ohms determine POS or neg ?

    Ohms can only be positive value. The range is from 0 to infinity.

    Gough suggested to measure, with a continuity meter, which wire goes to the + point of the circuit. And which wire to the - point. You would put one probe on a known + or - point. Then touch one wire with the other probe. The one that shows continuity is connected to that point. The other wire is then the oposite one.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robogary
    0 robogary over 3 years ago in reply to z234

    When the meter is used to test continuity, it applies a small positive voltage to the red lead of the meter. Hopefully the small voltage avoids causing damage in case the actual polarity is reversed. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • z234
    0 z234 over 3 years ago in reply to robogary

    Thank u very much for ur kind help.

    To recap, The multimeter does produce a very small positive voltage so as to check for the polarity but it is so small a voltage it may not damage the Component in case it really is of reverse polarity ya?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • z234
    0 z234 over 3 years ago in reply to robogary

    Thank u very much for ur kind help.

    To recap, The multimeter does produce a very small positive voltage so as to check for the polarity but it is so small a voltage it may not damage the Component in case it really is of reverse polarity ya?