Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How to know wire polarity in an open circuit without any electrical power?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 335 subscribers
  • Views 11535 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How to know wire polarity in an open circuit without any electrical power?

z234
z234 over 3 years ago

Dear friends, thank you for all your kind help.

How to know wire polarity in an open circuit without any electrical power? E.g. you have a dashcam with 2 wires with same color insulation. How do you know which is positive and which is negative?

If you plug wires wrongly into the battery, a short circuit may happen and damage the dashcam.

How to test for wire polarity in this open circuit then?

Thank you very much 

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +4
    You measure *continuity* using the continuity/ohms setting on your multimeter to determine which of your two same coloured wires go to positive or negative. Alternatively, apply power to one side of…
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to z234 +1
    z234 said: How do u see the ohms which is positive or negative by testing continuity? Does the numbers of ohms determine POS or neg ? Ohms can only be positive value. The range is from 0 to infinity…
  • Gough Lui
    0 Gough Lui over 3 years ago

    You measure *continuity* using the continuity/ohms setting on your multimeter to determine which of your two same coloured wires go to positive or negative.

    Alternatively, apply power to one side of the wire while the load is disconnected, using the multimeter in volts to determine polarity.

    The wire may be the same colour but also may have a subtle stripe down one side. This can indicate negative, but this is not universal.

    Otherwise, ask the manufacturer, or disassemble the device and test for continuity of the wire to a polarised component (e.g. the negative of an electrolytic capacitor on the input).

    - Gough

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • z234
    0 z234 over 3 years ago in reply to Gough Lui

    Thank u so much 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • z234
    0 z234 over 3 years ago in reply to Gough Lui

    Dearest Gough,

    I have followed ur advice n did a partial power on , without closing the circuit. I was able to detect polarity using a digital multimeter. Tq very much.

    How do u see the ohms which is positive or negative by testing continuity? Does the numbers of ohms determine POS or neg ? Tq very much

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to z234
    z234 said:
    How do u see the ohms which is positive or negative by testing continuity? Does the numbers of ohms determine POS or neg ?

    Ohms can only be positive value. The range is from 0 to infinity.

    Gough suggested to measure, with a continuity meter, which wire goes to the + point of the circuit. And which wire to the - point. You would put one probe on a known + or - point. Then touch one wire with the other probe. The one that shows continuity is connected to that point. The other wire is then the oposite one.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robogary
    0 robogary over 3 years ago in reply to z234

    When the meter is used to test continuity, it applies a small positive voltage to the red lead of the meter. Hopefully the small voltage avoids causing damage in case the actual polarity is reversed. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • z234
    0 z234 over 3 years ago in reply to robogary

    Thank u very much for ur kind help.

    To recap, The multimeter does produce a very small positive voltage so as to check for the polarity but it is so small a voltage it may not damage the Component in case it really is of reverse polarity ya?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 3 years ago

    image

    I have followed these post and chimed in to confirm my understanding without breaking out the meter.

    Using the ohm scale on the VOM, is it not reasonable to determine polarity by measuring each dash camera lead to ground in order to determine polarity. I assuming the -ve connection is tied to gnd. Using the ground plane of the dash camera as the -ve polarity not acceptable?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to colporteur

    It is an assumption. The designers may have taken an other decision.


    Just like saying that when measuring resistance or continuity, the red lead will send positive voltage. The only mode where a meter will send out positive voltage, guaranteed, is diode mode. For resistance and continuity, there are meters that send the positive via the common connector.

    Not all advices in this post's comments are true at all times.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 3 years ago in reply to Jan Cumps

    I agree it is an assumption but what do you do when you don't know what to do an assumption is the start.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to colporteur

    If it's a cheap device that's easy to replace, I'd go with the assumption.

    If it puts a dent in your budget, or is hard / impossible to replace, I would not.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>