Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum MC1377P video circuit drops to almost 0 when terminated with 75 ohm. Any ideas?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 337 subscribers
  • Views 1650 views
  • Users 0 members are here
  • mc1377p
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

MC1377P video circuit drops to almost 0 when terminated with 75 ohm. Any ideas?

baldengineer
baldengineer over 5 years ago

A project I've been working on for several months, or years depending on how you count, is build a Mini Apple IIe. (Originally it was a portable, now its just a mini.) The key to the project is the MEGA-II ASIC from the Apple IIgs. It contains all of the support logic found in old Apple II computers. (Approximately 80 7400-series chips!).

 

Since no one has ever used the MEGA-II in this way, I decided to build a couple of prototype boards to test three key sections: 6502, MEGA-II, and VGC. Turns out, we have the 65c02 and MEGA-II to be seemingly working. It even attempts to boot the Apple IIe ROM. (And then it appears to panic.)

 

So, I moved our attention to the video board. There are two basic sections on the board: the digital side and the analog side. The digital side consists of the VGC (video graphics controller) ASIC and three 4-bit DACs for RGB. Long story short, the MEGA-II generates the classic Apple II video bitstream, the VGC+DAC section converts it to analog R,G,B.

 

The analog part of the video circuit is based on an MC1377 RGB-to-NTSC encoder. That is the part of the circuit giving me trouble. In this iteration of the project, I just copied the circuit from the Apple IIgs. (My final project won't have composite.) The problem is that when I attach a video receiver or terminate the MC1377's output with 75-ohms, its output drops from 2.6 Vpp to 300 mVpp. A bit too small.

 

Here's the circuit:

image

The Full KiCad file is available here.

 

Here's the comparison of output:

image

In both cases I am, effectively, probing at J18's signal. On the right, I terminate that node with a 75 ohm resistor. (Same behavior with an actual composite receiver.)

 

A bunch more waveforms and link to MC1377P datasheet here: https://www.baldengineer.com/mc1377-measurements-on-mini-apple-iie-prototype-video-board.html .

 

Any ideas why the output is clamping so hard?

  • Sign in to reply
  • Cancel
Parents
  • jc2048
    jc2048 over 5 years ago

    shabaz just beat me to it. These were my thoughts for what they're worth:

     

    Is R54-2 unconnected?

     

    When you terminate and the signal at J18 collapses, what does the chip output do? Is it still pushing out 2V pk/pk or does it collapse in proportion?

     

    The datasheet suggests a lower value for the load resistor R9 when using a coupling capacitor. Not sure it would make as much difference as you're seeing, but might be worth looking at.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jc2048
    jc2048 over 5 years ago

    shabaz just beat me to it. These were my thoughts for what they're worth:

     

    Is R54-2 unconnected?

     

    When you terminate and the signal at J18 collapses, what does the chip output do? Is it still pushing out 2V pk/pk or does it collapse in proportion?

     

    The datasheet suggests a lower value for the load resistor R9 when using a coupling capacitor. Not sure it would make as much difference as you're seeing, but might be worth looking at.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • baldengineer
    baldengineer over 5 years ago in reply to jc2048

    Thanks Jon for looking it over. Yeah R54-2 is unconnected. It goes to a header pin in my design and it goes to the RGB connector in Apple's design. I think its just a copy of the composite signal for external monitors. I tried terminating that one too. If both R54-2 and J17 went to 75 ohms, the output was in the 10s of millivolts.

     

    For the record, when terminated, the output of the chip dropped as well. After futzing with the passives after that point, it definitely looked like the amplifier was clamping for some reason.  (see below for the solution, R9 was unnconnected.)