Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How it this analog front end circuit working?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 334 subscribers
  • Views 5854 views
  • Users 0 members are here
  • analog
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How it this analog front end circuit working?

Sudeep AJ
Sudeep AJ over 3 years ago

image

This circuit has been taken from a "DIY Oscilloscope" project. This circuit is changing the input wave swing to 0V to 3.3V. The circled voltage source is Vsys/2, which is the voltage at which the zero level of the input wave will be shifted to. Vsys is 3.3V here. 

The output is as follows:

image

I wanted to know how is this working and can I use it for my project?

The original circuit with Raspberry PI PICO is as follows.

image

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago +5
    U1 is set up as inverting opamp with gain of -R2/R1 = -0.1 and biased to the voltage on the positiv input 1.65 V (= 3.3V/2) because of the AC coupling cap C1. So the input sin wave with 14.1 V peak to…
  • scottiebabe
    scottiebabe over 3 years ago +4
    Its not the best circuit ever but its definitely worth putting on a breadboard and experimenting with it. With these magnitude of resistors in the feedback path you may find you need a tiny compensation…
  • phoenixcomm
    phoenixcomm over 3 years ago +3
    Sudeep AJ Ok, here we go. I hate to do this but, did you figure out what bandwidth you need? I noticed that you limit your voltage to 3.3v which by the way is a FLOATER in TTL. I personally think you are…
Parents
  • phoenixcomm
    phoenixcomm over 3 years ago

     Sudeep AJ  Ok, here we go. I hate to do this but, did you figure out what bandwidth you need? I noticed that you limit your voltage to 3.3v which by the way is a FLOATER in TTL. I personally think you are going to have a toy when you're done.image Save the sweat, money, and time and pick up a good used scope. You can pick one up like my old Tektronix 475A for about 150 bucks plus shipping. I have inserted the first

    a paragraph from the manual.  image

    Please note that I can see 1ns/div which I do use when I have noise transits from things like Switches, Keyboards, and Relays. In other words any contactor. 

    If you go through this exercise remember that the front end is ANALOG and therefore near RF frequencies, and EVERYTHING MUST BE SHIELDED. Also, my probes (Tektronix) have a built-in compensator as well as a 10:1 divider, and they're good to 500 MHz. 

    Please enjoy the project just keep some of my wisdom in your mind. ~~ CAH

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • phoenixcomm
    phoenixcomm over 3 years ago

     Sudeep AJ  Ok, here we go. I hate to do this but, did you figure out what bandwidth you need? I noticed that you limit your voltage to 3.3v which by the way is a FLOATER in TTL. I personally think you are going to have a toy when you're done.image Save the sweat, money, and time and pick up a good used scope. You can pick one up like my old Tektronix 475A for about 150 bucks plus shipping. I have inserted the first

    a paragraph from the manual.  image

    Please note that I can see 1ns/div which I do use when I have noise transits from things like Switches, Keyboards, and Relays. In other words any contactor. 

    If you go through this exercise remember that the front end is ANALOG and therefore near RF frequencies, and EVERYTHING MUST BE SHIELDED. Also, my probes (Tektronix) have a built-in compensator as well as a 10:1 divider, and they're good to 500 MHz. 

    Please enjoy the project just keep some of my wisdom in your mind. ~~ CAH

    • Cancel
    • Vote Up +3 Vote Down