Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum SMD Transistors
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 323 subscribers
  • Views 2309 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

SMD Transistors

Shourov001
Shourov001 over 2 years ago

Hello, I am making a digital logic project that requires SMD NPN transistors there are a lot of transistors but which transistor should I choose?BC847, BC817,2N3904, SS8550, SS8050 Please help me to choose one among them.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago in reply to Shourov001 +3
    Really hope you're going to simulate it before using up so many transistors! This isn't a beginners level project, expect to troubleshoot a lot unless you're really going to put effort into simulating…
  • robogary
    robogary over 2 years ago +2
    All the comments in this post to you are completely valid and insightful. Recommend you start with the basics - what is your logic voltage, what is the load (needing to drive) in mA or amps, and how…
  • JWx
    JWx over 2 years ago in reply to Shourov001 +2
    posting schematics would be useful... SS8050 have maximum collector current of 1.5A - will they be used to drive some load? Or to implement some logic functions? Are you building this adder with only transistors…
  • ggabe
    ggabe over 2 years ago

    Transistors are selected for speed, transfer parameters (hFE, etc.) voltage, and current requirements. What are the conditions your digital logic is working under?

    Just for completeness, listing a few additional selection criteria, primary used in non-digital circuits: noise, heat transfer, high frequency impedance parameters, capacitance, reverse voltage breakdown, leakage current. Many charted over various other conditions, like temperature.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago

    You will have to look at the datasheets and decide which device has the features you want for your application. If we don't know the application, we cannot help you select.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago

    SS8550 is a PNP. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • bidrohini
    bidrohini over 2 years ago

    The choice depends on your requirement. To be more specific, the input voltage, current etc. and the desired output of your project. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 2 years ago

    All the comments in this post  to you are completely valid and insightful.

    Recommend you start with the basics - what is your logic voltage, what is the load (needing to drive) in mA or amps, and how fast does it need to switch ? If your logic is asynchronous, timing may not be critical, but if your logic is clocked, the transistor needs to be faster than the clock.    

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Shourov001
    Shourov001 over 2 years ago in reply to ggabe

    I am planning to make 8-bit adder with those transistors! after reading all the datasheet I decided to buy ss8050. Should this transistor work for this application?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Shourov001
    Shourov001 over 2 years ago in reply to dougw

    I am planning to make 8-bit adder with those transistors! after reading all the datasheet I decided to buy ss8050. Should this transistor work for this application?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Shourov001
    Shourov001 over 2 years ago in reply to robogary

    As I am a beginner in this field I don't know much but I am planning to make 8-bit adder with those transistors! after reading all the datasheet I decided to buy ss8050. Should this transistor work for this application?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to Shourov001

    posting schematics would be useful... SS8050 have maximum collector current of 1.5A - will they be used to drive some load? Or to implement some logic functions? Are you building this adder with only transistors or some ICs also?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to Shourov001

    Really hope you're going to simulate it before using up so many transistors! This isn't a beginners level project, expect to troubleshoot a lot unless you're really going to put effort into simulating, modular design, test features in your board, and so on. Also, at least test a single adder or two first. 

    By the way there's a good chance of getting bad transistors if you're buying from unknown sources (I have no idea), and since you're a beginner, you might not know that,  therefore consider how you're going to either eliminate them, or how you will isolate faults and replace them (i.e. you'll need spares too..). 

    Also, it's unlikely to perform like a modern digital circuit if you're solely constructing from NPN transistors. Again, lots of opportunities to trip up if you're a beginner.

    • Cancel
    • Vote Up +3 Vote Down