Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum The best transistor replacement
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 335 subscribers
  • Views 6644 views
  • Users 0 members are here
  • Replacement transistor grundig ts1000
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

The best transistor replacement

b139b
b139b over 3 years ago

Hello everyone. Hope you all are doing well Thumbsup
I need some smart input from you... I am looking for some replacement transistors for my old tape recorder. The recorder sounds like a thunderstorm, so I think one transistor is bad. Since those transistors (BC330C, BC237B, BC238B) not are available anymore, I am looking for replacements.

In this case, since the design already is given, is "typical hfe" the parameter witch is most important to match with the original transistor? - To keep the same amplification steps. 


All maximum-voltages must of course to be the same or higher to the original.

I have some BC550C with hfe=420-800. Is it correct to think that the typical hfe for the BC550C is in the middle of this values =610 ? Too much amplification in my case?
Any input is appreciated Blush
Christian

image

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 3 years ago +3
    b139b said: The recorder sounds like a thunderstorm, so I think one transistor is bad Have you already replaced the electrolytic capacitors? They are far more likely to have gone bad.
  • Gough Lui
    Gough Lui over 3 years ago in reply to baldengineer +3
    That and potentiometers ... *crackle crackle - Gough
  • shabaz
    shabaz over 3 years ago +2
    Hi, The BC550 is likely fine for all of these NPN transistors, since the actual transistor gain doesn't matter usually (because the circuit will control the actual gain). The BC550 is a very decent substitute…
Parents
  • b139b
    b139b over 3 years ago

    Thank you all for your replies! Great community! 

    The Thunderstorm is heat depended...came when I thought the player was fixed after the backlid was on. I have changed all electrolytes and C2. With a oscilloscope/RTA I can see that the signal is ok at the left side of C2 but the noise is present at the right. I have tried to find the faulty component by knocking on the components, potmeters too. Cool them with freezespray... heat with a heatingun but no component changed clearly.

    Thanks for the link to BC237B Blush

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • b139b
    b139b over 3 years ago

    Thank you all for your replies! Great community! 

    The Thunderstorm is heat depended...came when I thought the player was fixed after the backlid was on. I have changed all electrolytes and C2. With a oscilloscope/RTA I can see that the signal is ok at the left side of C2 but the noise is present at the right. I have tried to find the faulty component by knocking on the components, potmeters too. Cool them with freezespray... heat with a heatingun but no component changed clearly.

    Thanks for the link to BC237B Blush

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • b139b
    b139b over 3 years ago in reply to b139b

    Here is my setup. The 50Hz comes from the charger. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ggabe
    ggabe over 3 years ago in reply to b139b

    Right side of C2 goes with the wire somewhere up high - could the noise come from there?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • b139b
    b139b over 3 years ago in reply to ggabe

    Goes to the Auto level part. I think they rectify the signals an use this to set the recording level automatically. image

    Could be, cause the other channel has made a "bump" (... oh, my English Rolling eyes) onces or twice. But very seldom. Could be something else too. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ggabe
    ggabe over 3 years ago in reply to b139b

    Is the issue happening with or without auto leveleing, or in both cases? T6/T8 seems serving the leveling/regular path. I would look at replacing C25/C26, perhaps before doing it just to put a known good cap in parallel to see if it reduces the noise. Are the voltages across R77 and R78 equal?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to b139b

    Also, you could temporarily bypass the autolevel to see what happens, by lifting the two capacitors C2 and C6, and bridge across with a single capacitor, if you suspect auto-level.

    If you don't already have a 'scope (not sure the Phonic product you have there will replace it unfortunately) then it would be worth picking up a low-priced one, since there are some reasonable options at $200 and under.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • b139b
    b139b over 3 years ago in reply to ggabe

    Thank you for your reply! C25/C26 are you new. I have not checked it, but since the thunder is only in the right channel, the voltage would not be equal at R77/R78. I am on holyday until next week, so I check when I am home again 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • b139b
    b139b over 3 years ago in reply to shabaz

    Thanks. I have a scope, and the phonic can be a scope too. I have switched the recorder to manual.