Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Cooling salt water with minimal cost.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 334 subscribers
  • Views 2268 views
  • Users 0 members are here
  • help
  • water
  • temperature
  • cooling
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Cooling salt water with minimal cost.

Bigmacpie
Bigmacpie over 3 years ago

So, I’m curious if it’s possible to cool a large body of salt water using pipes with cooler flowing water. How would one make an efficient simplistic system to do this. I have read that copper pipes with cold flowing water through them wold cool the water but with salt water corrosion would be a big issue. Also what would be the easiest way to pump the cold water through the pipes and recirculate it back around through a cooling mechanism? 

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +4
    A lot of your problems in this area have been solved by people making "keel cooling" systems for boats. The applications are different but many of the components used might be suitable for your purpose…
  • bobthemallett
    bobthemallett over 3 years ago +2
    There's lots of data available on dealing with salt water corrosion but almost anything will add to the cost, such as using A4 (Marine) grade Stainless Steel. Using a heat-exchanger to increase the effective…
  • beacon_dave
    beacon_dave over 3 years ago in reply to Bigmacpie +1
    In the construction of the Hoover Dam, around 600miles of 1" diameter steel pipe was used for the mass concrete cooling process. Before that, Fulgence Bienvenüe used similar cooling techniques to freeze…
Parents
  • bobthemallett
    0 bobthemallett over 3 years ago

    There's lots of data available on dealing with salt water corrosion but almost anything will add to the cost, such as using A4 (Marine) grade Stainless Steel. Using a heat-exchanger to increase the effective surface area and minimise the effects of any corrosion or other build-up such as salt coating the system. Plastic pipes may be resistant to corrosion but all the plastics used to make pipes are pretty goo thermal insulators so will tend to make the system very inefficient with regards to heat transfer which may or may not be an issue. A thin layer of paint, plenty of salt-resistant / marine grade paints are available, will allow you to use more convenient metal tubing. You also need to remember to consider the problems of deposition of calcium salts from the "cool" water. If you use a three-part system i.e. with a closed-loop between two tanks (one the salt water, one with the cooling mechanism) then that could be filled with de-ionised water (known as "distilled" but it hasn't been for decades!) then, depending on the rate of heat flow you need, you could just use a standard pond-pump or similar. Bob

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bobthemallett
    0 bobthemallett over 3 years ago

    There's lots of data available on dealing with salt water corrosion but almost anything will add to the cost, such as using A4 (Marine) grade Stainless Steel. Using a heat-exchanger to increase the effective surface area and minimise the effects of any corrosion or other build-up such as salt coating the system. Plastic pipes may be resistant to corrosion but all the plastics used to make pipes are pretty goo thermal insulators so will tend to make the system very inefficient with regards to heat transfer which may or may not be an issue. A thin layer of paint, plenty of salt-resistant / marine grade paints are available, will allow you to use more convenient metal tubing. You also need to remember to consider the problems of deposition of calcium salts from the "cool" water. If you use a three-part system i.e. with a closed-loop between two tanks (one the salt water, one with the cooling mechanism) then that could be filled with de-ionised water (known as "distilled" but it hasn't been for decades!) then, depending on the rate of heat flow you need, you could just use a standard pond-pump or similar. Bob

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Bigmacpie
    0 Bigmacpie over 3 years ago in reply to bobthemallett

    I’m not familiar at all with this type of stuff. You said a 3 part system, is there any related information on how to build this. The  area is really large ( 100 miles by 4 miles) that will be needed for cooling, so it would have to be very economical to build and operate, if it is possible to do at all.

    Thank you for responding and the info you have already provided. 
    Erich 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anniel747
    0 anniel747 over 3 years ago in reply to Bigmacpie

    Geothermal is cheap and easy.