Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Cooling salt water with minimal cost.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 334 subscribers
  • Views 2271 views
  • Users 0 members are here
  • help
  • water
  • temperature
  • cooling
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Cooling salt water with minimal cost.

Bigmacpie
Bigmacpie over 3 years ago

So, I’m curious if it’s possible to cool a large body of salt water using pipes with cooler flowing water. How would one make an efficient simplistic system to do this. I have read that copper pipes with cold flowing water through them wold cool the water but with salt water corrosion would be a big issue. Also what would be the easiest way to pump the cold water through the pipes and recirculate it back around through a cooling mechanism? 

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +4
    A lot of your problems in this area have been solved by people making "keel cooling" systems for boats. The applications are different but many of the components used might be suitable for your purpose…
  • bobthemallett
    bobthemallett over 3 years ago +2
    There's lots of data available on dealing with salt water corrosion but almost anything will add to the cost, such as using A4 (Marine) grade Stainless Steel. Using a heat-exchanger to increase the effective…
  • beacon_dave
    beacon_dave over 3 years ago in reply to Bigmacpie +1
    In the construction of the Hoover Dam, around 600miles of 1" diameter steel pipe was used for the mass concrete cooling process. Before that, Fulgence Bienvenüe used similar cooling techniques to freeze…
Parents
  • beacon_dave
    0 beacon_dave over 3 years ago

    Perhaps take a look at some of the mass concrete cooling setups and calculations.

    It is going to depend on how large a volume and how much cooling is required.

    You may be able to use plastic pipes to avoid salt water corrosion.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Bigmacpie
    0 Bigmacpie over 3 years ago in reply to beacon_dave

    Suppose I needed to cool a length of approx 100 miles by 4 miles in shallow waters of 25 feet depth, would it be feasible to build something like that to cool down the water? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anniel747
    0 anniel747 over 3 years ago in reply to Bigmacpie

    What kind of insulation you have on top of that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 3 years ago in reply to Bigmacpie

    In the construction of the Hoover Dam, around 600miles of 1" diameter steel pipe was used for the mass concrete cooling process.

    Before that, Fulgence Bienvenüe used similar cooling techniques to freeze the ground to stabilise it for tunnelling in the construction of the Paris Metro. I recall a similar ground freezing technique was used more recently for the Boston 'Big Dig' construction.

    Some places use arrays of passive thermosyphon cooling piles to create permafrost conditions in ground to stabilise it without the need for cooling plants, but it requires sufficient temperature differentials for the syphon to work..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • beacon_dave
    0 beacon_dave over 3 years ago in reply to Bigmacpie

    In the construction of the Hoover Dam, around 600miles of 1" diameter steel pipe was used for the mass concrete cooling process.

    Before that, Fulgence Bienvenüe used similar cooling techniques to freeze the ground to stabilise it for tunnelling in the construction of the Paris Metro. I recall a similar ground freezing technique was used more recently for the Boston 'Big Dig' construction.

    Some places use arrays of passive thermosyphon cooling piles to create permafrost conditions in ground to stabilise it without the need for cooling plants, but it requires sufficient temperature differentials for the syphon to work..