Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Inline Key Switch or Tamper Resistant control for mains devices?!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 58 replies
  • Answers 2 answers
  • Subscribers 334 subscribers
  • Views 9286 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Inline Key Switch or Tamper Resistant control for mains devices?!

shabaz
shabaz over 3 years ago

Hi,

For one reason or another (elderly relative), I'm looking for a way to prevent operation of a mains appliance (about 6A at 230V AC) unless, say, a key of some sort is inserted, to prevent them from using the appliance themselves. It doesn't need to be a high-security solution, it could simply be a plastic key for instance, that could be pushed in and rotated, to enable the appliance.

I don't wish to cut holes in the appliance, and really do want to do this inline with the mains wire. 

Is there any existing product that could do this? If not, is there any suggestion that I could fit into a small plastic enclosure myself? I don't have access to a 3D printer, so it ideally needs to be a solution that I could make using conventional tools (electric drill, saw, etc). 

One way I can think of, is to find some sort of enclosure where a rocker switch could be fitted recessed, and then have a small padlock such that it prevents the switch from operating. But it probably requires a custom box : ( Another way could be to have a Bluetooth controlled relay. I could design this, but I'd rather find an off-the-shelf solution. 

I'm sure I can't be the only one wanting to do such a thing, but I'm having no luck googling for this. 

Anyone come across anything that could help?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +6
    It arrived today, I'd say it is a 7/10 product.. it will certainly fit many plugs, but the build quality looks very average. The hinge looks fragile, although perhaps that's deceptive. I don't know. …
  • charlieo21
    charlieo21 over 3 years ago in reply to anniel747 +5 suggested
    Definitely the simplest and cheapest option, we have those in the lab, it works perfect to avoid someone use an equipment without authorization. Another option are those smart plugs that you can control…
  • beacon_dave
    beacon_dave over 3 years ago +5 suggested
    A long shackle padlock combined with a Lego Brick sized block with a hole in it (placed between the pins) could probably fit over a 13A plug top preventing it from being plugged into a socket. I don…
Parents
  • robogary
    0 robogary over 3 years ago

    image

    https://www.lotomaster.eu/product/plug-lockout-large/

    to prevent an appliance from being powered, pull the plug and lock it out. 

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • robogary
    0 robogary over 3 years ago

    image

    https://www.lotomaster.eu/product/plug-lockout-large/

    to prevent an appliance from being powered, pull the plug and lock it out. 

    • Cancel
    • Vote Up +4 Vote Down