Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Inline Key Switch or Tamper Resistant control for mains devices?!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 58 replies
  • Answers 2 answers
  • Subscribers 334 subscribers
  • Views 9327 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Inline Key Switch or Tamper Resistant control for mains devices?!

shabaz
shabaz over 3 years ago

Hi,

For one reason or another (elderly relative), I'm looking for a way to prevent operation of a mains appliance (about 6A at 230V AC) unless, say, a key of some sort is inserted, to prevent them from using the appliance themselves. It doesn't need to be a high-security solution, it could simply be a plastic key for instance, that could be pushed in and rotated, to enable the appliance.

I don't wish to cut holes in the appliance, and really do want to do this inline with the mains wire. 

Is there any existing product that could do this? If not, is there any suggestion that I could fit into a small plastic enclosure myself? I don't have access to a 3D printer, so it ideally needs to be a solution that I could make using conventional tools (electric drill, saw, etc). 

One way I can think of, is to find some sort of enclosure where a rocker switch could be fitted recessed, and then have a small padlock such that it prevents the switch from operating. But it probably requires a custom box : ( Another way could be to have a Bluetooth controlled relay. I could design this, but I'd rather find an off-the-shelf solution. 

I'm sure I can't be the only one wanting to do such a thing, but I'm having no luck googling for this. 

Anyone come across anything that could help?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +6
    It arrived today, I'd say it is a 7/10 product.. it will certainly fit many plugs, but the build quality looks very average. The hinge looks fragile, although perhaps that's deceptive. I don't know. …
  • charlieo21
    charlieo21 over 3 years ago in reply to anniel747 +5 suggested
    Definitely the simplest and cheapest option, we have those in the lab, it works perfect to avoid someone use an equipment without authorization. Another option are those smart plugs that you can control…
  • beacon_dave
    beacon_dave over 3 years ago +5 suggested
    A long shackle padlock combined with a Lego Brick sized block with a hole in it (placed between the pins) could probably fit over a 13A plug top preventing it from being plugged into a socket. I don…
Parents
  • Fred27
    0 Fred27 over 3 years ago

    If you do end up wanting a 3D printed solution then let me know. I'd be happy to print something and send it to you.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to Fred27

    Hi Fred,

    Oh that's awesome, thank you for the support! 

    I've ordered the Martindale product that anniel747  found, and will give it a shot! If it's no good then I think we should design a 3D solution since it could help many people! : )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to shabaz

    If any of the plug pins are slightly out of line with each other, then the grip will be significant with a moulded approach. Depends on how much shrinkage Polydoh has. Might be able to wiggle it a bit before it fully hardens to give it just a little freedom around the pins and to allow for the BS pin spacing tolerance.

    In the past I've used 2-part resin body/wood filler paste for creating parts for prototypes. It's about the only free-form material I've ever had success/enjoyed working with. Not too messy/runny, sets quickly, can be cut/sanded and smells great.   

    I have however seen some very nice small-scale work done with fine-grade concrete mixes which I could be tempted to give a go. It can take on a whole new look if you use the right aggregates and sand/polish it up after and apply sealing lacquers. I think combined with flexible filament in a 3D printer to create release moulds, then it could be interesting.

    A non-moulded 13A plug will often have a bit of movement in its pins so may release easier than a moulded one.

    Dipping the pins in melted wax before moulding might also work. Depends on the working temperature of the Polydoh vs the melting point of the wax though Slight smile

    One advantage of Lego is that you can always claim that you are 'just playing with Lego' Slight smile

    It will be interesting to see what you can come up with.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to beacon_dave
    beacon_dave said:
    The one doubt I have depends on the padlock used and how much of a gap the shackle leaves when it is unlocked.

    If this turns out to be a problem, then the width of the slot could be increased to the thickness of the padlock. This would allow a padlock with even zero clearance between shackle tip and the body to be used.

    It also makes it easier to use as you can drop the body of the padlock through the slot, with the shackle at right angles to trap the cable and locate the hole in one go. Then twist the padlock body through 90 degrees to align with the tip of the shackle and lock.

    It will increase the rotational play once locked but if that is a problem then you could drill additional holes to make detents and offset the slot. The hole on the opposite side may need more clearance to allow the slight tilt angle of the padlock when passing the tip of the shackle through the hole but in most cases probably not.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to shabaz
    shabaz said:
    I'll see if I have a plate.

    Cheapest source for that type of plates, is a set of plastic kitchen cutting boards. Either in  a 1£ shop, or at a flea market, you'll find enough material for years.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to beacon_dave

    Can omit the outside edges of the slot if you want. Easier to cut manually and can use a wider range of padlock thicknesses. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anniel747
    anniel747 over 2 years ago in reply to beacon_dave
    This reply was deleted.
    • Cancel
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to anniel747

    Yes, that part can be removed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to beacon_dave

    I gave it a try today, with a slight variation that makes it quicker to construct:

    image

    I used 3mm plastic, and this seems to be sufficient for preventing a plug from functioning, however the spec should be examined really. Perhaps 4 mm plastic would be better.

    I have not made the holes for the padlock yet, because Amazon let me down with their delivery. However I'm confident that part will work fine once I've made the holes for it!

    image

    For the holes, they were spaced 22.2 mm from their centres, with the earth pin having a 9 mm hole, and the other two were 8 mm diameter.

    The plate was 100 x 60 mm, but I think 110 x 70 mm could be better (impact the switch on the socket more!). The two plastic strips were 10 mm wide.

    I really like this design, and the flat plate impacts the on-off switch on mains sockets too, making it even harder to switch on.

    I'm going to suggest this as a product for a family member (who has the right machinery!) to construct and sell, if they are interested (and obviously you should get some sort of a royalty beacon_dave although I hope they sell it at ultra-low-cost). Even if it just sells in the few dozens or hundreds, it's still a great problem-solver for those who need it. I've no idea if the family member would be interested in productizing this, but if they do, then it's a nice option for users, to either self-construct as an open-source design, or simply buy it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to shabaz

    Looks good.

    Might have to be careful of the plastic thickness as if too thin then it may flex too much and allow the pins to be released, or if it is too brittle then it may be too easy to snap. Originally I was thinking around 6mm as a starting point but would take some experimentation.. 

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to beacon_dave

    Good idea, it may be worth just moving to 6mm and then it should be near indestructible. I used whatever I had at hand which was perspex, and reckon (but would need to test) that when installed that would be hard to snap (without tools) because if they try to push it away from the earth pin end, the earth pin digs against the hole and so the leverage is very little. As for the other end, the leverage is low because the plug cable/moulding won't flex so close to the plug. That leaves the padlock area, which might be fragile, but will find out soon when I try it. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to shabaz

    Perhaps need to hand it to a 5-year old for some 'destructive testing' Slight smile

    6mm is a common thickness for ply / MDF if anyone was thinking about trying it using offcuts of wood instead of plastic.

    (French-polished Mahogany for the connoisseur...)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to shabaz

    Perhaps need to hand it to a 5-year old for some 'destructive testing' Slight smile

    6mm is a common thickness for ply / MDF if anyone was thinking about trying it using offcuts of wood instead of plastic.

    (French-polished Mahogany for the connoisseur...)