Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How to control the HV converter with analog voltage signal?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 28 replies
  • Subscribers 334 subscribers
  • Views 5305 views
  • Users 0 members are here
  • power_electronics
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How to control the HV converter with analog voltage signal?

Dykan
Dykan over 3 years ago

The HV converter require 24V power supply and some analog voltage signals. I connect two 0~10V voltage signals to the pin of HV converter, 10HVA24-N1. However what I get from the output of HVA is 0V. Is there any thing wrong with my wiring?

image

image

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 3 years ago in reply to Dykan +3
    Pin 12 is the current monitor output. It will output a voltage that's proportional to the HV current being supplied by the module. Hopefully there's enough resistance in series with the output that you…
  • michaelkellett
    michaelkellett over 3 years ago in reply to Dykan +2
    So it looks as if your power supply thinks it is working. How is you divider working - (diagram) - its a strange co-incidence that 100uA into 0.63M would give excatly 63V. Your power supply max output…
  • dang74
    dang74 over 3 years ago +1
    Interesting device. Reading through the app note that is available on the manufacturer's website I noticed that pin 11 can be driven by TTL. The app note suggests that the level on pin 11 must be at least…
Parents
  • shabaz
    0 shabaz over 3 years ago

    As dang74 says. it may be related to pin 11. A couple of resistors could help provide the right input to that pin. The resistors below will provide about +4V to the enable pin, which is within its supported range. You should be checking with a multimeter.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 3 years ago

    As dang74 says. it may be related to pin 11. A couple of resistors could help provide the right input to that pin. The resistors below will provide about +4V to the enable pin, which is within its supported range. You should be checking with a multimeter.