Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum I don't understand python venv
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 4 answers
  • Subscribers 335 subscribers
  • Views 12488 views
  • Users 0 members are here
  • raspberry pi 5
  • the environment is externally managed
  • raspberry pi 5 bookworm
  • python packages
  • pip install
  • venv
  • python3
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

I don't understand python venv

cstanton
cstanton over 2 years ago

This is going to be a growing pain for a lot of people that pick up the Raspberry Pi 5 with Bookworm, too.

A lot of guides and instructions say to do:

pip install <package>

Or

apt-get install python3-<package>

The 'problem' from a usability perspective now, is that when you try to do:

pip install <package>

It complains at you with "this environment is externally managed" and to use a venv, and I don't understand them. It doesn't direct you on how to use a venv either.

I understand why we're doing it this way, so that we do not have a clash between operating system repository packages and the python pip installed packages.

Can someone explain to me how to use pip with a venv with an example package? I'm trying to find guides online and of course everyone has an opinion on how to do it three different ways but they also don't explain what exactly venv is doing or how to use it after installing the package with pip.

  • Sign in to reply
  • Cancel

Top Replies

  • JWx
    JWx over 2 years ago +5 suggested
    Python suffers from multitude of interpreter and library versions - which can lead to the situation that one library cannot co-exist with another, because they - for example - are dependent on another…
  • shabaz
    shabaz over 2 years ago +4 suggested
    I watched a training video on it a while back. It suggested the following: (1) First off, check you've got 'virtualenv' installed. That's easy to do by typing which virtualenv (2) If you don't have…
  • michaelkellett
    michaelkellett over 2 years ago in reply to cstanton +3 suggested
    There's a comprehensive, but not perfect, description here. https://realpython.com/python-virtual-environments-a-primer/ which may help. MK
Parents
  • JWx
    0 JWx over 2 years ago

    Python suffers from multitude of interpreter and library versions - which can lead to the situation that one library cannot co-exist with another, because they - for example - are dependent on another library, but in different versions.

    To overcome this - as I understand - virtual environments were created, to have local execution sandbox with all the required libraries

    To create one:

    #python3 -m venv /root/test-venv

    optionally - install required package first:

    #apt install python3.10-venv

    To activate it:

    #source /root/test-venv/bin/activate

    and then pip is local copy and packages should be installed inside this venv (to not interfere with other versions)

    (test-venv) root@e14-panda:~# which pip
    /root/test-venv/bin/pip
    /root/test-venv/bin/pip
    (test-venv) root@e14-panda:~# pip list
    Package    Version
    ---------- -------
    pip        22.0.2
    setuptools 59.6.0

    Install something

    (test-venv) root@e14-panda:~# pip install pandas
    Collecting pandas
      Downloading pandas-2.1.1-cp310-cp310-manylinux_2_17_x86_64.manylinux2014_x86_64.whl (12.3 MB)
         ━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━ 12.3/12.3 MB 5.1 MB/s eta 0:00:00
    Collecting tzdata>=2022.1
      Downloading tzdata-2023.3-py2.py3-none-any.whl (341 kB)
         ━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━ 341.8/341.8 KB 3.3 MB/s eta 0:00:00
    Collecting python-dateutil>=2.8.2
      Downloading python_dateutil-2.8.2-py2.py3-none-any.whl (247 kB)
         ━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━ 247.7/247.7 KB 3.8 MB/s eta 0:00:00
    Collecting numpy>=1.22.4
      Downloading numpy-1.26.1-cp310-cp310-manylinux_2_17_x86_64.manylinux2014_x86_64.whl (18.2 MB)
         ━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━ 18.2/18.2 MB 5.1 MB/s eta 0:00:00
    Collecting pytz>=2020.1
      Downloading pytz-2023.3.post1-py2.py3-none-any.whl (502 kB)
         ━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━━ 502.5/502.5 KB 5.2 MB/s eta 0:00:00
    Collecting six>=1.5
      Downloading six-1.16.0-py2.py3-none-any.whl (11 kB)
    Installing collected packages: pytz, tzdata, six, numpy, python-dateutil, pandas
    Successfully installed numpy-1.26.1 pandas-2.1.1 python-dateutil-2.8.2 pytz-2023.3.post1 six-1.16.0 tzdata-2023.3

    List again:

    (test-venv) root@e14-panda:~# pip list
    Package         Version
    --------------- ------------
    numpy           1.26.1
    pandas          2.1.1
    pip             22.0.2
    python-dateutil 2.8.2
    pytz            2023.3.post1
    setuptools      59.6.0
    six             1.16.0
    tzdata          2023.3

    Deactivate venv:

    (test-venv) root@e14-panda:~# deactivate

    Try pip again:

    root@e14-panda:~# pip list
    Command 'pip' not found, but can be installed with:
    apt install python3-pip

    There is even no pip command installed outside of venv

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • cstanton
    0 cstanton over 2 years ago in reply to JWx

    Hi JWx,

    JWx said:

    and then pip is local copy and packages should be installed inside this venv (to not interfere with other versions)

    Does this then mean there're effectively 'duplicates' of all packages?

    And I wonder what the priority order is, that it goes "hey version pip-package0.1 is in the externally managed, but version pip-package 0.5 is in the venv" presumably it uses the venv, but if it doesn't exist in the venv, does that mean you have to then install it?

    JWx said:
    virtual environments don't need to even be activated after creation - simply using (by calling it with full path) python interpreter from given venv sets all the environment automatically

    I'm having trouble parsing what that sentence means and what it relates to in practice.

    Thanks for answering Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 2 years ago in reply to cstanton

    There's a comprehensive, but not perfect, description here.

    https://realpython.com/python-virtual-environments-a-primer/

    which may help.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • JWx
    0 JWx over 2 years ago in reply to cstanton

    that the problem with fast typing in foreign language Slight smile

    yes - there will be duplicates (but maybe in different versions to satisfy dependencies):

    create second one, enter it and list packages:

    root@e14-panda:~/test-venv# python3 -m venv /root/test-venv1
    root@e14-panda:~/test-venv# source /root/test-venv1/bin/activate
    (test-venv1) root@e14-panda:~/test-venv# pip list
    Package    Version
    ---------- -------
    pip        22.0.2
    setuptools 59.6.0

    install something

    (test-venv1) root@e14-panda:~/test-venv# pip install numpy
    Collecting numpy
      Using cached numpy-1.26.1-cp310-cp310-manylinux_2_17_x86_64.manylinux2014_x86_64.whl (18.2 MB)
    Installing collected packages: numpy
    Successfully installed numpy-1.26.1

    exit and try to find installations:

    root@e14-panda:~# find . -type d -name numpy
    ./test-venv1/lib/python3.10/site-packages/numpy
    ./test-venv1/lib/python3.10/site-packages/numpy/core/include/numpy
    ./test-venv/lib/python3.10/site-packages/numpy
    ./test-venv/lib/python3.10/site-packages/numpy/core/include/numpy
    ./test-venv/lib/python3.10/site-packages/pandas/compat/numpy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • feiticeir0
    0 feiticeir0 over 2 years ago in reply to cstanton

    I've stumbled on that issue yesterday... Didn't new that bookworm would be like that. 

    I only think it's a pain in the a s s because if you have a project that you want to run on startup, you need to initialize the virtual environment previously.

    It's not duplicates per say... You're creating an environment with its own packages. It's duplicating size, it is, but it's safer because you don't break any dependencies. There's a lot of packages out there that only work with specific versions..

    It's not perfect, but gets the job done. I have that "problem" already with Arch Linux. 

    If you want, you also have conda . I personally use more venv from Python - but probably because I'm already accustomed to it - but conda it's also great.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • feiticeir0
    0 feiticeir0 over 2 years ago in reply to cstanton

    I've stumbled on that issue yesterday... Didn't new that bookworm would be like that. 

    I only think it's a pain in the a s s because if you have a project that you want to run on startup, you need to initialize the virtual environment previously.

    It's not duplicates per say... You're creating an environment with its own packages. It's duplicating size, it is, but it's safer because you don't break any dependencies. There's a lot of packages out there that only work with specific versions..

    It's not perfect, but gets the job done. I have that "problem" already with Arch Linux. 

    If you want, you also have conda . I personally use more venv from Python - but probably because I'm already accustomed to it - but conda it's also great.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • JWx
    0 JWx over 2 years ago in reply to feiticeir0

    not exactly - simply use dedicated python interpreter from venv using #! directive, like this:

    #!/home/user/venv1/bin/python3

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JWx
    0 JWx over 2 years ago in reply to JWx

    like in documentation (docs.python.org/.../venv.html):

    "

    You don’t specifically need to activate a virtual environment, as you can just specify the full path to that environment’s Python interpreter when invoking Python. Furthermore, all scripts installed in the environment should be runnable without activating it.

    In order to achieve this, scripts installed into virtual environments have a “shebang” line which points to the environment’s Python interpreter, i.e. #!/<path-to-venv>/bin/python. This means that the script will run with that interpreter regardless of the value of PATH. On Windows, “shebang” line processing is supported if you have the Python Launcher for Windows installed. Thus, double-clicking an installed script in a Windows Explorer window should run it with the correct interpreter without the environment needing to be activated or on the PATH.

    When a virtual environment has been activated, the VIRTUAL_ENV environment variable is set to the path of the environment. Since explicitly activating a virtual environment is not required to use it, VIRTUAL_ENV cannot be relied upon to determine whether a virtual environment is being used.

    "