Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Trying to find a high-speed, high-power transistor to use as a switch
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 20 replies
  • Subscribers 334 subscribers
  • Views 6067 views
  • Users 0 members are here
  • mosfet
  • components
  • igbt
  • ask_an_expert
  • circuit
  • switch
  • power
  • power_electronics
  • question
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Trying to find a high-speed, high-power transistor to use as a switch

ZappaMap
ZappaMap over 3 years ago

I'm designing a high power H-bridge circuit, and I'm trying to find the best transistor for the design. The most important parameters are that it has
- 10MHz switching speed frequency

- Low on-state resistance

- Low off-state capacitance

From there, I would need it to handle high voltages and have a low gate charge. With that in mind, does anyone know of any parameter relationships I should be aware of or what products potentially match that description? Thank you!

EDIT:

Thank you all for your responses! To answer a couple questions I saw:

- I do not have a preference between MOSFETS and BJTs.

- For voltage and amperage, I don't have hard numbers for those. I'm still operating in the tradespace stage of the design right now, so I'm still figuring out what options I have. To give a ballpark range, a component that works with volts on the order of 10V or 100V and amps on the order of 10A wouldn't hurt. I am more concerned with the switching frequency, on-state resistance, and off-state capacitance.

I also learned a little more about switchmode amplifiers, and that is another avenue that I am now looking down (specifically class D and E).

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +5
    I think you'll need to quantify the current and voltage to get good advice. 10MHz is very fast for typical H bridge type applications. Do you have a preference between MOSFETs and BJTs ? As you probably…
  • dougw
    dougw over 3 years ago +3
    You might have a look at Gallium Nitride transistors.
  • scottiebabe
    scottiebabe over 3 years ago +3
    You may also consider pre-engineered GaN half-bridge modules or ultrasound pulse drivers.
  • michaelkellett
    0 michaelkellett over 3 years ago

    I think you'll need to quantify the current and voltage to get good advice. 10MHz is very fast for typical H bridge type applications.

    Do you have  a preference between MOSFETs and BJTs ?

    As you probably already know its easy to get high current and high voltage at low speeds and possible to get very high speeds at low voltages and currents - getting all three is very hard.

    What is the end game here ?

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 3 years ago

    You might have a look at Gallium Nitride transistors.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anniel747
    0 anniel747 over 3 years ago
    [deleted]
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to dougw

    They still require a 10-ish ns deadband. 1MHz is just doable for a half bridge.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rsc
    0 rsc over 3 years ago in reply to anniel747

    IGBTs are very slow.  100khz is pushing the limits.10mhz I've never heard of with an IGBT.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • scottiebabe
    0 scottiebabe over 3 years ago

    You may also consider pre-engineered GaN half-bridge modules or ultrasound pulse drivers.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    +1 shabaz over 3 years ago

    No real information of what is a high voltage and what current needs to be supported.

    You could examine RF power transistors, discrete or otherwise. Here is an example dual transistor (i.e. half a H-bridge so two would be needed for a full H-bridge) which is pretty high-power and high-voltage, with a driver built-in. https://ww1.microchip.com/downloads/en/DeviceDoc/DRF1400_%20B.pdf 

    The price is as expected...

    Discrete transistors are going to be pricey too. They will come in funny packages, and you may need "opposite-packaged" pairs, otherwise it's a bit hard to route traces for them.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • anniel747
    0 anniel747 over 3 years ago in reply to rsc
    [deleted]
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to scottiebabe

    I tested TI LMG5200. GaN half bridge + frontend in a single package. It can switch fast - 1 MHz. Still a magnitude slower than the reqs. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 3 years ago in reply to anniel747

    http://www2.arrl.org/files/file/QEX_Next_Issue/2014/May-Jun_2014/Horowitz.pdf

    But .... this is a quasi linear application of an IGBT.

    The rise and fall times (of the IGBT they used) add up to 37ns so they wouldn't work in a switching H bridge at anything like 20MHz - might scrape1MHz but they would get warm.

    But unless the OP comes back an explains better what they are looking for we are, to coin a phrase, "switching in the dark" (although he did say switching speed, but he might have meant switching frequency which is more commonly measured in Hz)

    Has anyone (here on E14) used IGBTs in a linear application.

    There is a nice Analogue Devices app note for an audio power amplifier design but you can't buy the P channel parts any more.

    I've used IGBTs in linear (high-ish) power regulators with reasonable success.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>