Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Any interest in collaborating on a parasitic inductance power supply? It could be used to power small LV projects like IoT nodes and microcontrollers...
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 332 subscribers
  • Views 4971 views
  • Users 0 members are here
  • microcontrollers
  • power-supply
  • iot
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Any interest in collaborating on a parasitic inductance power supply? It could be used to power small LV projects like IoT nodes and microcontrollers...

PPE_COOP
PPE_COOP over 2 years ago

I have been thinking about a design for this for some time. Mostly to help with another project im working on but I thought other people may be interested in the possibilities also. I have already filed a provisional, please see below. Im possibly looking for help developing the idea into a full product/utility patent. I have one utility patent already and understand the process. The problem is that I am completely self taught and could really benefit from a development partner with better engineering skills than myself. I'm not sure if this is a place to ask for this type of help and I apologize if it's not. Please see the excerpt from the application below.

Parasitic inductance power supply


FIELD OF INVENTION
[0001] The present invention relates to a system and method for providing
low-voltage power to single or multiple devices using inductive coupling, which is
facilitated through the mains power feeders of other apparatuses or equipment.
BACKGROUND
[0002] There is a frequent requirement for extracting power from mains supply to
operate low-voltage devices, such as sensors or communication equipment, which
may be independent or integrated with the mains-powered equipment. The
conventional approach involves direct connections to mains power, necessitating the
use of mains-rated power supplies, fuses and complex power electronics. This
method is often excessive for devices needing only milliampere-level current at very
low voltage. An alternative, more efficient solution is the use of parasitic inductive
coupling, which allows for the extraction of power without physically connecting to
the mains conductors. This method can efficiently power various devices, including
battery chargers, ensuring continuous power supply to low-power equipment, even
when the mains power is switched off.


SUMMARY
[0003] This invention involves a method where a coil of wire is wrapped around an
AC mains power conductor connected to power utilization or generation equipment.
Functioning similarly to a current transformer, the fluctuating magnetic flux from
the mains conductor induces an electrical potential in the coil. This induced voltage
is then modified and regulated through electronic circuitry, enabling it to power
small, low-voltage loads. This method effectively eliminates the need for direct
electrical connections to the mains conductors, offering a simpler and less intrusive
power supply solution for low-power devices.

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 2 years ago in reply to PPE_COOP +3
    Perhaps you need to read what I wrote again because you missed the most critical part. Fundamentally, wrapping a coil around an AC mains cable is pointless unless you separate the conductors. Which…
  • anniel747
    anniel747 over 2 years ago +2
    Deleted
  • beacon_dave
    beacon_dave over 2 years ago in reply to javagoza +2
    Just add electronics... TI Designs: TIDA-01385 Energy Harvesting From Current Transformer With Supercapacitor for Fault Indicator Reference Design https://www.ti.com/lit/ug/tidud59/tidud59.pdf
Parents
  • javagoza
    javagoza over 2 years ago

    I don't know if I understood your invention very well but it reminds me a lot of something I studied 40 years ago at university, instrument transformers.
    https://en.wikipedia.org/wiki/Instrument_transformer

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • javagoza
    javagoza over 2 years ago

    I don't know if I understood your invention very well but it reminds me a lot of something I studied 40 years ago at university, instrument transformers.
    https://en.wikipedia.org/wiki/Instrument_transformer

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • PPE_COOP
    PPE_COOP over 2 years ago in reply to javagoza

    Yes it is similar to that. The idea is to develop device similar to a CT where the output can be used to power items like a low power battery charger that can then be used to power something like a IoT tnode. My thought is that this could be used to lower the need for such devices to limit their transmissions or enter sleep modes. Picture a commercial rooftop air conditioning unit or a solar inverter that you would like to add some additional telemitry. Instead of just using battery powered nodes you could add this unit to one or more of the mains feeders to pull the small amount of power required for it to operate. It is now difficult to get 3.3VDC milliwatt power from a 480V mains supply without a lot of additional equipment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to javagoza

    Just add electronics...

    TI Designs: TIDA-01385
    Energy Harvesting From Current Transformer With Supercapacitor for Fault Indicator Reference Design

    https://www.ti.com/lit/ug/tidud59/tidud59.pdf

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • PPE_COOP
    PPE_COOP over 2 years ago in reply to beacon_dave

    Dam, that's mostly it. Thanks for sharing. Now I need to determine if there are any differences worth exploring...