Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Help Testing Relay
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 20 replies
  • Subscribers 329 subscribers
  • Views 4665 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Help Testing Relay

HBPhillie
HBPhillie over 2 years ago

I would like to replace what I think is a faulty relay on my jacuzzi board... but there are 4 P&B T92S7D12-12 Relays on this board... My question(s)

How do I test these .. the Jacuzzi J330 is powered by 220 VAC.  Do I need to remove them?  

I have some Engineering degrees but not much electronics experience.  I think I see that these are double pole and I might need to power the 'input' side and read the switching sides?  If this sounds like I'm not sure how to do this you're reading correctly.  I've actually already replaced the board but I want to see if I can diagnose the problem with the old one.

Thank you for any help.

Tom

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 2 years ago +2
    https://www.te.com/commerce/DocumentDelivery/DDEController?Action=srchrtrv&DocNm=1308242_T92&DocType=DS&DocLang=English You can see from the datasheet these operate from 12 Vdc across the coil. You…
  • dougw
    dougw over 2 years ago in reply to HBPhillie +2
    Try some resistance measurements before removing components (with the card disconnected from power). It may tell you a lot with a lot less work.
  • kmikemoo
    kmikemoo over 2 years ago in reply to HBPhillie +2
    Good plan. Resistance testing on the PCB is usually complicated by the snubber diodes across the coils. I default to the Goesinta/Goesouta test. If the circuit provides power to the relay but the contacts…
Parents
  • dougw
    0 dougw over 2 years ago

    https://www.te.com/commerce/DocumentDelivery/DDEController?Action=srchrtrv&DocNm=1308242_T92&DocType=DS&DocLang=English

    You can see from the datasheet these operate from 12 Vdc across the coil.

    You can measure the impedance of the coil using the pinout in the datasheet. If it is around 86 ohms, the coil should be okay.

    You can measure the contact impedance, unpowered, the datasheet indicates which contacts are open and which are closed. (Measuring about infinite and zero ohms)

    If you apply 12V across the coil, the relay should click and the contacts should change state (measuring zero and infinite)

    If the card is disconnected from the system you can probably do these tests without removing the relays from the card, It may be worth checking what is connected to the relay on the card to know for sure if they can be tested in-circuit.

    As acdc90  indicated you need to be careful not to apply reverse voltage to the coil since the snubber diode across the coil will conduct in that polarity.

    A photo might help the members provide better advice.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 2 years ago

    https://www.te.com/commerce/DocumentDelivery/DDEController?Action=srchrtrv&DocNm=1308242_T92&DocType=DS&DocLang=English

    You can see from the datasheet these operate from 12 Vdc across the coil.

    You can measure the impedance of the coil using the pinout in the datasheet. If it is around 86 ohms, the coil should be okay.

    You can measure the contact impedance, unpowered, the datasheet indicates which contacts are open and which are closed. (Measuring about infinite and zero ohms)

    If you apply 12V across the coil, the relay should click and the contacts should change state (measuring zero and infinite)

    If the card is disconnected from the system you can probably do these tests without removing the relays from the card, It may be worth checking what is connected to the relay on the card to know for sure if they can be tested in-circuit.

    As acdc90  indicated you need to be careful not to apply reverse voltage to the coil since the snubber diode across the coil will conduct in that polarity.

    A photo might help the members provide better advice.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • anniel747
    anniel747 over 2 years ago in reply to dougw
    This reply was deleted.
    • Cancel
    • Cancel
  • HBPhillie
    0 HBPhillie over 2 years ago in reply to anniel747

    Yes I believe this is correct... if I'm reading the Data Sheet correctly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer