Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Anyone have experience repairing an HP3325B synthesized generator?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 334 subscribers
  • Views 2673 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Anyone have experience repairing an HP3325B synthesized generator?

davebullockmbe
davebullockmbe over 2 years ago

Hi HP Experts,
I have just repaired my HP3325B Synthesised signal generator and found what appears to be a 3V memory backup battery in there.
It still measures 3.08V but has most likely been in there since the 1970's.
So I wondered just what it is backing up and should I replace it?
I looked at the attached schematic expecting it to be retaining vital calibration data.
I have scoured the service manual for any mention of this lithium battery's purpose and the only reference to it is a tiny section entitled RESET CIRCUITS. (I have pasted this as a window at the top of the attached schematic).

So what is the battery backing up?
The schematic shows it feeding a supply line called "+5B NV RAM SUPPLY VOLTAGE". However a closer look at the diagram shows it powering a pair of SRAM chips which are of course Volatile memory.
Does anyone know if these two memory IC's are holding vital calibration data or are they used to simply store user's operational data whilst the generator is switched on and operating.

I can't find this vital nugget of information in the service manual (well I can't spot it!) and DO NOT want to accidentally lose the calibration by foolishly disconnecting the battery without mitigation.

Please enlighten me if you know the answer.
Thanks in anticipation..........
Daveimage

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 2 years ago +3
    Looks like the data entry values as the manual refers to storing and recalling information.
  • davebullockmbe
    davebullockmbe over 2 years ago in reply to beacon_dave +2
    Lol...been there ... got the missing knuckles :-)
  • dougw
    dougw over 2 years ago +1
    I can't say what data is being retained in the SRAM, however the SRAM power looks like it is fed from the regular 5V supply when the system is powered up, and the battery only kicks in when 5V disappears…
Parents
  • electronicbiker
    0 electronicbiker over 2 years ago

    I don't know the answer either. My best guess is that it could be some sort of memory that retains the settings of all the knobs and switches during a power-down and that those values are used on the next power-up so that all the knobs and switches will be set to deliver the same values as when it was switched off. This would suggest that the knobs and switches rotate continuously and generate square waves, like the two pulse-generating wheels inside an old-fashioned mouse. The extra bits and pieces may be a hold-off system whereby the voltages applied to the delicate parts have to reach and remain at a certain voltage level and for a certain length of time before being applied to the rest of the circuit. After all, if the 5 volt peak-to-peak maximum input socket on the equipment that is being calibrated is still connected after a power-down, you wouldn't want to be suppying hundreds of volts to it during power-up. It might also do a similar job on power-down, as the voltages will be all over the place as the power fades away.

    I had difficulty viewing the circuit diagram as it is blurred in places and very blurred in others. Can you do it again with the camera on a tripod and the shutter release operated remotely? I have found a desktop music stand to be very useful when standing manuals and diagrams etc nearly upright. The dark part (bottom centre) doesn't help either. Other useful info would be an approximate date of manufacture and the part numbers of some of the other devices especially the two big ones shown end-to-end in the dark area. Also, are there any crystals, and if so what is their resonant frequency? It is just possible that there is a phase-locked-loop in there somewhere.

    Final thought - "NV RAM" could be a very early version of "EEPROM", especially if it is written to on power-down and read on power-up. If that is the case then both power-up and power-down might take slightly longer than expected.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • electronicbiker
    0 electronicbiker over 2 years ago

    I don't know the answer either. My best guess is that it could be some sort of memory that retains the settings of all the knobs and switches during a power-down and that those values are used on the next power-up so that all the knobs and switches will be set to deliver the same values as when it was switched off. This would suggest that the knobs and switches rotate continuously and generate square waves, like the two pulse-generating wheels inside an old-fashioned mouse. The extra bits and pieces may be a hold-off system whereby the voltages applied to the delicate parts have to reach and remain at a certain voltage level and for a certain length of time before being applied to the rest of the circuit. After all, if the 5 volt peak-to-peak maximum input socket on the equipment that is being calibrated is still connected after a power-down, you wouldn't want to be suppying hundreds of volts to it during power-up. It might also do a similar job on power-down, as the voltages will be all over the place as the power fades away.

    I had difficulty viewing the circuit diagram as it is blurred in places and very blurred in others. Can you do it again with the camera on a tripod and the shutter release operated remotely? I have found a desktop music stand to be very useful when standing manuals and diagrams etc nearly upright. The dark part (bottom centre) doesn't help either. Other useful info would be an approximate date of manufacture and the part numbers of some of the other devices especially the two big ones shown end-to-end in the dark area. Also, are there any crystals, and if so what is their resonant frequency? It is just possible that there is a phase-locked-loop in there somewhere.

    Final thought - "NV RAM" could be a very early version of "EEPROM", especially if it is written to on power-down and read on power-up. If that is the case then both power-up and power-down might take slightly longer than expected.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • electronicbiker
    0 electronicbiker over 2 years ago in reply to electronicbiker

    Blast! Just had another thought! Always the same, I press the Log Out button and immediately think of something else.

    The model number HP3325B might be part of the mystery. Assuming there is a HP3325A, C, D, etc, then different fixed parameters could be stored in the NV RAM for different models. In which case don't take the battery out just yet!