Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Has anyone fixed Barco projector Powersupply
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 332 subscribers
  • Views 1502 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Has anyone fixed Barco projector Powersupply

acdc90
acdc90 over 2 years ago

Hello model Roal C94 or R764833 and RHPSC94

I have repaired several of these after the TOP246 explodes and then replace IC,s on the 15v rail

Now i have 2 that start up 3 green leds then shuts down with no error message or light 

Does anyone know this fault

  • Sign in to reply
  • Cancel

Top Replies

  • Matze
    Matze over 1 year ago in reply to acdc90 +1
    Hi, thank you for your reply! Even if it is very embarrassing, it was my fault. The screw next to it was very tight, so I had to use a plier and it slipped away, breaking the diode Yeah, the theory…
Parents
  • Matze
    0 Matze over 1 year ago

    Hi acdc90,

    I just stumbled over your post and although I can't help you with your problem, perhaps you can help me?

    I'm trying to fix an R764833 LPS where one of the diodes (D301) is broken. Do you have an idea about the specs of this part? I have no clue what specifications the sparepart should have.

    Thank you in advance!

    Matze

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • acdc90
    0 acdc90 over 1 year ago in reply to Matze

    Hello, just looking at some photos there are 5 of opto coupler  HCPL-7800A used in that unit. each had 2 diodes including  D301  

    i did not have a problem with the diodes around the opto coupler/opamp which includes D301, so I did not need to investigate them,

    be warned the pin out numbers on board for ic i230 are wrong

    How does a diode inside a metal box get broken? or did you do it

    i would down load the data sheet for opto, see which pins both diodes goto, see if that makes sence, then pull another diode out and do some measurements , like with a resister and see if it is a Zenor

    what else is wrong with it. I had 6 complete modules that had 1 blown the 15v(LVPS) supply 

    I believe dust had built up across the SMPS ic and then with moisture "exploded" then zapping the output 

    so by replacing ics and 10ohm resisters on 15v rail fixed most of them 

    hope that helps 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Matze
    0 Matze over 1 year ago in reply to acdc90

    Hi,

    thank you for your reply!

    Even if it is very embarrassing, it was my fault. The screw next to it was very tight, so I had to use a plier and it slipped away, breaking the diode Face palm

    Yeah, the theory of dust and moisture sounds legit, as I found lots of both while dismantling, causing also corroded and non conduction connections to the fuses.

    The main problem is 'Error -2001, mains voltage too low'. Therefore I started looking for defects in the LPS (and made it even worse by being clumsy...)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • acdc90
    0 acdc90 over 1 year ago in reply to Matze

    does your LVPS led come on 

    if not with no mains connected to unit 

    evan with out D301

    supply external 14v to white wires between boards 

    labeled +15 and END

    if it draws more than 36ma then you have several  dead ics on that rail and dead SMPS TOP246yn

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • acdc90
    0 acdc90 over 1 year ago in reply to Matze

    does your LVPS led come on 

    if not with no mains connected to unit 

    evan with out D301

    supply external 14v to white wires between boards 

    labeled +15 and END

    if it draws more than 36ma then you have several  dead ics on that rail and dead SMPS TOP246yn

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Matze
    0 Matze over 1 year ago in reply to acdc90

    Didn't dare to give it a try before fixing the D301, but after your suggestion I'll test it