Products
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
Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum cga to vga converter uPython
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 46 replies
  • Subscribers 332 subscribers
  • Views 8467 views
  • Users 0 members are here
  • python
  • raspberry pico
  • ask_an_expert
  • microcontrollers
  • teensy
  • vga
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

cga to vga converter uPython

rlaci
rlaci over 2 years ago

Hi

im new to uPython and needing some help with fast interrupts, port handling, reading into controller, handling the big amount of data and speed

my main aim is to get it working on raspberry pico, as colors 1bit resolution is enought as its an industrial equiment with RGBHV 15.6khz input(output from the machine) need to transfer it to 31khz VGA standard output for an lcd monitor

any help welcome

thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +3
    There's a website listing monitors that support your resolution: http://15khz.wikidot.com/ I think it's far more likely that you'll be able to source a monitor if you search long enough on eBay, than…
  • beacon_dave
    beacon_dave over 2 years ago in reply to shabaz +3
    There is a PIO based implementation of a VGA driver discussed here if anyone is interested: https://www.youtube.com/watch?v=ZXMdZGQzrWg
  • michaelkellett
    michaelkellett over 2 years ago in reply to rlaci +3
    It's very, very difficult. You need to delve quite deeply into the data sheets. The things to look for are the IO toggle rate, maximum clock rate of internal RAM, and maybe some benchmarks of complete…
Parents
  • dougw
    0 dougw over 2 years ago

    Are you looking for something like this RGB to VGA adapter? They cost about $1.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to dougw

    I think they mean the old IBMPC Color Graphics Array RGBI TTL output

    https://en.wikipedia.org/wiki/Color_Graphics_Adapter#DE-9_connector_for_RGBI_monitor

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rlaci
    0 rlaci over 2 years ago in reply to beacon_dave

    RGB + Hsync Vsync. the adapter should contain 5inputs the one youl listed looks like 3 inputs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rlaci
    0 rlaci over 2 years ago in reply to beacon_dave

    sorry the other reply was for the original comment.

    i looked up your link and hsync is pretty similiar, but vsync is 63hz not 59.xxx

    the sync is ttl level

    rgb also ttl level

    mine has no intensity output and rgb signals look like low high

    possibly you are right and my machine was derived from this standard, its a cnc mill sinumerik controlled operators panel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to rlaci

    You might be able to pick up an Extron VS 304 for next to nothing. They could handle 15kHz RGBHV and scale to VGA.

    https://www.extron.com/product/dvs304

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 2 years ago in reply to rlaci

    RGBHV2VGA is a bit more expensive $7-$8

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rlaci
    0 rlaci over 2 years ago in reply to beacon_dave

    nice hint as i saw on ebay its common in usa but im from europe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to dougw

    Hi Doug,

    He needs to change pixel rate, which requires electronics. I suspect the cable in the photo is unlikely to do that, there's no power source connection in the photo (there may be power delivered through a VGA connector, but I believe it's in the direction from PC->monitor, not monitor->PC).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 2 years ago in reply to dougw

    Hi Doug,

    He needs to change pixel rate, which requires electronics. I suspect the cable in the photo is unlikely to do that, there's no power source connection in the photo (there may be power delivered through a VGA connector, but I believe it's in the direction from PC->monitor, not monitor->PC).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • rlaci
    0 rlaci over 2 years ago in reply to shabaz

    i saw that cable before and i predict its from vga to rgb not from rgb to vga

    solutions what i found as standalone products:

    - GBS2019 Xvga box but was highly delayed when i first searched it

    - getting a 15khz monitor, i got one and not working possibly the 63Hz vertical sync messes it up

    - Extron VS 304 looks documented like can work, but at the rgbhv place the resolution was not really documented i got this info here from beacon_dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to rlaci
    rlaci said:
    i saw that cable before and i predict its from vga to rgb not from rgb to vga

    It's a bidirectional cable but passive.

    AV installs often ran RGBHV over 5 coax cables whereas PC's used the 15pin Hi Density 'D' type connector with additional I2C DDC data line. Early multisync monitors used to come with the 5x BNC as default as well. These type of cables were common place to convert between the two physical formats.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rlaci
    0 rlaci over 2 years ago in reply to beacon_dave

    i saw a DVS 406 unit in europe, is it better or worse newer older equipment?

    i hope it does not mean the signal just passes throught and no processing done for the output signal :D

    • Scales composite video, S-video, component video, and optional SDI inputs with RGBHV pass-through
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to rlaci

    Similar unit, just more inputs and has the pass through functionality. Looks like it is optimised for PAL / NTSC video though but that might just be the sales pitch.

    The pass through is an input loop feature that allows you to insert the device into an existing signal path without interrupting it. The scaling happens between the inputs on the left and the outputs on the right.

    I don't think either of these boxes are much use to you if you definitely have the original CGA TTL level signals, unless you were to convert the levels first.

    The board I linked to on Amazon, looks a closer match for your needs, as it looks like it has been designed for the 1980s CGA/EGA TTL level signals. Looks like it is aimed at keeping some of the early video gaming systems alive with modern displays.