Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum POWER FOR SOLENOID VALVE
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 35 replies
  • Subscribers 331 subscribers
  • Views 6399 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

POWER FOR SOLENOID VALVE

Afiq
Afiq over 2 years ago

When 36W supply to specification 16W solenoid valve normally open, is there is effect to the solenoid valve?

  • Sign in to reply
  • Cancel

Top Replies

  • Anthocyanina
    Anthocyanina over 2 years ago in reply to Afiq +5
    your valve works with 230V AC, it will not work (to specification, if at all) with a 24V power supply
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Andrew J +4
    Maybe ordered the wrong one? There is a 24 V version:
  • michaelkellett
    michaelkellett over 2 years ago in reply to shabaz +3
    The article is a bit misleading since it refers to inrush current when it means current when the solenoid armature is extended out of the coil. It may common to describe it this way but it's not that helpful…
  • kmikemoo
    0 kmikemoo over 2 years ago in reply to shabaz

    I hadn't thought to deep about this before, but I must agree with shabaz as a solenoid has no way to create a counter electromotive force - which is what creates the current reduction in motors.  There is also no inductive reactance since it's DC.  There is probably an instant of subtransient reactance during the initial energization but since there is no frequency, it's theoretical at the speed of electrons level.

    We may experiencing one of the challenges in our field - language / terms / nomenclature.  Solenoids can be the single coil relay thing or they can be the pull-in coil / holding coil variant.  Sometimes the latter solenoids have 3 wires.  These may or may not have internal contacts to drop out the pull-in coil.  The 2-wire variant will always have contacts to disconnect the pull-in coil at the end of travel for the solenoid.  The pull-in coil is used to overcome the Law of Inertia and will definitely burn up if left energized - because it has low resistance.  Magnetism in this case is all about Amp-turns with an emphasis on the amps.  We get the high impulse to move the armature but we don't need that much energy to keep it centered in the holding coil.  The holding coil is also about amp-turns but the emphasis is on the turns; thinner wire, more turns, higher - current limiting - resistance.

    SO... solenoids can appear to have inrush - but they don't.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to michaelkellett

    Agree, hard to see how that condition could be defined as inrush, (e.g. it would be called a stalled condition for a DC motor, don't know what one would call it for an AC solenoid!). Also reminds me of an old discussion (with a blog from John Wiltrout from memory) where it was discovered that impedance could be lowered in some conditions (depending on the particular metal, and the AC frequency). Granted it's more likely to be 50/60Hz here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anniel747
    0 anniel747 over 2 years ago in reply to kmikemoo

    They do create counter EMF each time they move.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Afiq
    0 Afiq over 2 years ago in reply to anniel747

    image    This is my solenoid valve voltage rating

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Anthocyanina
    0 Anthocyanina over 2 years ago in reply to Afiq

    your valve works with 230V AC, it will not work (to specification, if at all) with a 24V power supply

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to Afiq

    And you could make yourself a science experiment to see why this is the case. Get an electromagnet (any electromagnet, could be a relay coil, or a spool of wire) and by applying different voltages, try to approximately see what difference in force you're seeing. Try half the voltage, then a quarter of the voltage, and then a tenth of the voltage. What you'll  observe will make it very clear.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Afiq
    0 Afiq over 2 years ago in reply to shabaz

    shabaz to be clear can you emphasize me the causes of solenoid valve not function when testing? Can you advise me the solution to these problems/causes?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to Afiq

    The electronic portion (assuming it is a solenoid version and not a motor) is just a coil of wire, so ordinarily that could outlast a lifetime, although the winding can get damaged. You can do a very basic, very partial test by checking with a multimeter to see if it has gone open circuit. Other than that, the item is mechanical, so there can be plenty of mechanical problems (accidentally knocked plunger, stuck plunger due to dirt, etc. 

    Since it is a gas safety valve, it's best to replace it with a new modern one. Otherwise, if it ever fails and there is damage or someone is injured, the person that repaired and re-installed it will be the one that will be imprisoned.

    Obviously that's an expensive part, but if you're just looking to experiment with a solenoid valve (and don't intend to install it in it's normally intended application) you can get plenty of small low-voltage (e.g. 24V) devices for very little cost.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Afiq
    0 Afiq over 2 years ago in reply to shabaz

    Is it possible to fix and repair the plunger that being dirty or rusting? Because when there have gone open circuit, the voltage and Amp is enough, and have supplied but the solenoid valve cant trigger to close valve. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to Afiq

    Personally I think no, it should be thrown away in a condition that no-one repairs it. I know there's a strong desire to repair and re-use, but in a critical application the $100 is not worth the risk to lives (and there would be a high risk). Everyone knows of gas explosion stories in their own towns or neighbourhoods, so it's not rare for things to go badly wrong. This would increase the risk a lot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>