Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Timeout Error when Reading Measurements from Impedance Analyzer Solartron 1260 via NI MAX using IEEE 488/GPIB
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 29 replies
  • Subscribers 333 subscribers
  • Views 5493 views
  • Users 0 members are here
  • PCIB
  • NIMax
  • impedance analyzer
  • read error
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Timeout Error when Reading Measurements from Impedance Analyzer Solartron 1260 via NI MAX using IEEE 488/GPIB

Abdul
Abdul over 2 years ago

Hi, 

 I'm working with a Solartron A1260 Impedance/Gain-Phase Analyzer and attempting to read measurements on the NI MAX interface connected through a PCI bus. The analyzer itself is functioning correctly and can receive "Write" commands, as you can see the measurements on blue screen, but when I try to "Read" these measurements using NI MAX, I encounter a timeout error, as illustrated in the attached screenshot.The only command I can read is `*IDN? `. but my goal is to "Read" that simple measurement data of impedance analyzer on NI MAX interface.

I have tried adjusting the timeout/Bytes settings and reviewing the connection, but the issue persists. It seems like the main challenge is that I'm not sure about the correct commands to read the measurement data. Here are the details of my setup:


- Device Model: Solartron 1260 Impedance/Gain-Phase Analyzer
- Connection: Interface through PCIB
- Software: NI MAX
- Issue: Timeout error EABO during GPIB read operation

- Troubleshooting Steps: Adjusted timeout settings, adjusted bytes, changed addresses, checked GPIB command syntax, changed GPIB

 I would greatly appreciate any advice on the proper GPIB commands for reading measurements from a Solartron 1260 or any troubleshooting steps that might resolve this timeout error.

Thank you in advance for your help!

image

image

image

  • Sign in to reply
  • Cancel

Top Replies

  • Abdul
    Abdul over 2 years ago +4
    Subject: Successful Update: Command Reading on NI MAX Interface Achieved! Dear Element14 Community, I have successfully configured the NI MAX interface to read commands from the impedance analyzer…
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to shabaz +3
    I read the paper. Very useful to learn / understand a working conversation for this brand. Warning to Abdul , at the end of the paper, the writer explains how one of his scripts damaged the instrument…
  • shabaz
    shabaz over 2 years ago +2
    You could also check for code for other Solartron products of that era, in case you can spot any difference. For instance, a student used a 1260A here: https://www.slideshare.net/JosephHaystead/enel301…
  • Jan Cumps
    0 Jan Cumps over 2 years ago

    What query do you send before the read attempt?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Abdul
    0 Abdul over 2 years ago in reply to Jan Cumps
    • SI? ( stands for Single measurement) but gives me an error response.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to Abdul

    SI?\n

    Have you tried that string?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Abdul
    0 Abdul over 2 years ago in reply to Jan Cumps

    Yes,  also with SI?\r and SI?\r\n. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 2 years ago in reply to Abdul

    Launch NI IO Trace, set that running then send the command and see what the trace tells you.  I presume SI? Is from the manual?  If you don’t have that, here’s a link: https://mmrc.caltech.edu/Solartron/Solertron%20manual1260.pdf.  I suspect a handshake issue.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 2 years ago

    Have you tried following the procedure in the example files in the operating manual section 6.1:

    It looks as if you need to send "OP 2,1" command before "SI" command.

    It can be a problem to get old instruments to talk happily - my solution was to make my own PC to GPIB adapter with much better diagnostics than commercial ones and I still often need to resort to connecting a logic analyser to see the bus traffic.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Abdul
    0 Abdul over 2 years ago in reply to Andrew J

    Yes, SI command  is from the manual .Thank you for your prompt response and proposed solutions. I will thoroughly analyze them and provide an update tomorrow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Abdul
    0 Abdul over 2 years ago in reply to michaelkellett

    Thank you for your prompt response and proposed solution. I will thoroughly analyze them and provide an update tomorrow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago

    You could also check for code for other Solartron products of that era, in case you can spot any difference.

    For instance, a student used a 1260A here: https://www.slideshare.net/JosephHaystead/enel301-report-joseph-haystead1132999

    The Python code is in his report:

    image

    His code uses this terminator (but looks like there may be DIP switches etc on the instrument to set it?):

    image

    And this timeout:

    image

    Then he wrote a load of commands to set up the instrument, before doing the sweep:

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Abdul
    0 Abdul over 2 years ago in reply to shabaz

    Dear Shabaz, I appreciate your assistance and thank you for providing the code; I will thoroughly review it to find a solution.Unfortunately, the link you provided isn't working for me, and I am unable to download the PDF file. Could you please upload the file directly? Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>