Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum i want to build a circuit that expands dc range
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 335 subscribers
  • Views 1666 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

i want to build a circuit that expands dc range

acdc90
acdc90 over 2 years ago

Hello

most of the time i repair stuff. so not used to designing 

the input to this circuit min=0.48v max=2.5v

i want to expand the output to min=0 max =2.5v

this is for a anilog input and power supply of 5v

if i needed to generate a negative rail i could just use dc-dc module 

as it would only be a 1 off i would just use vero board and DIL ic  

    thank for looking  

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago in reply to acdc90 +3
    Unfortunately, this still needs a lot more information. Unless you're fully open about the actual use-case, and provide as much detail as possible about what this is for, it's near-impossible to help.…
  • michaelkellett
    michaelkellett over 2 years ago +1
    There are lots of ways this could be done but none are perfect. You need to tell us what the source of the signal is and where its going. The more you explain the context the better the answer you will…
Parents
  • michaelkellett
    0 michaelkellett over 2 years ago

    There are lots of ways this could be done but none are perfect. You need to tell us what the source of the signal is and where its going.

    The more you explain the context the better the answer you will get. The information you have provided so far isn't quite enough to make any good suggestions.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • acdc90
    0 acdc90 over 2 years ago in reply to michaelkellett

    THE OUTPUT from this is going into a DAQ unit that i don,t have info for so output current would be minimal 

    this is feed into a computer program which can do automatic calibration 

    but when the calbration is used the input limits drift which will eventually crash the program 

    so i set this up using a external pot  and worked for 3 hours no problem before i shut it down 

    so i think with dual op amp ic and twin rail i should get to 0v min 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to acdc90

    Unfortunately, this still needs a lot more information. Unless you're fully open about the actual use-case, and provide as much detail as possible about what this is for, it's near-impossible to help. The original information was extremely minimal, this is currently only fractionally better.

    If you really think you need an op-amp circuit then you can plug the values into an online calculator and get a circuit: https://masteringelectronicsdesign.com/differential-amplifier-calculator-2/

    However, whether that will actually provide a real solution or not, I have no idea, because the information isn't there.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 2 years ago in reply to acdc90

    Unfortunately, this still needs a lot more information. Unless you're fully open about the actual use-case, and provide as much detail as possible about what this is for, it's near-impossible to help. The original information was extremely minimal, this is currently only fractionally better.

    If you really think you need an op-amp circuit then you can plug the values into an online calculator and get a circuit: https://masteringelectronicsdesign.com/differential-amplifier-calculator-2/

    However, whether that will actually provide a real solution or not, I have no idea, because the information isn't there.

    • Cancel
    • Vote Up +3 Vote Down