Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum trying to connect MP730424 DMM with rs232 but get Timeout error
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 333 subscribers
  • Views 2611 views
  • Users 0 members are here
  • help
  • connector
  • ask_an_expert
  • cable
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

trying to connect MP730424 DMM with rs232 but get Timeout error

JeremieWerner
JeremieWerner over 2 years ago

I am trying to remote control a DMM MP730424 from a computer with Windows 11. *IDN? gives a VI_ERROR_TMO: Timeout expired before operation completed.

the instrument port information show: baud 115200, parity None, stop bits 1, data bits 8. 

What is the expected EOL and termination character?

has anyone manage to control this device via RS232?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 2 years ago +3
    It looks like an Owon XDM2041. The same (poor) documentation is on the web if you hunt for it. This discussion on eevblog (several message in) suggests that it will talk easily via the serial port.. The…
  • shabaz
    shabaz over 2 years ago +2
    I don't have this instrument, but here are some things to try. Perhaps the transmit and receive pins need swapping. Sometimes instruments require a cable (e.g. null modem cable) to attach to the usb…
  • Gough Lui
    Gough Lui over 2 years ago +2
    Most devices will need '\n' for the EOL/termination character. If not, try '\r'. - Gough
Parents
  • michaelkellett
    0 michaelkellett over 2 years ago

    Which USB to RS232 adapter are you using - if the DMM uses true RS232 it may very well not work with a logic level adapter.

    Do you have a scope (ideally with RS232 decoding) - if so then connect it to monitor the RS232 RX and TX pins.

    Found some more info here:

    https://github.com/PetteriAimonen/owon-xdm2041-info/tree/main/mcu_board

    This would suggest that the DMM is  a logic level RS232 so it won't work (reliably) with a a true RS232 adapter on the PC.

    You can check this - disconnect the lead from the DMM and use another meter to measure the voltage on pins 2 and 3 relative to pin 5.

    If all the voltages you see are between 0 and +5V it is a logic level interface.

    If at least one of the voltages is more than 3V  -ve  it is a true RS232  interface,

    If both voltages are less than +/-0.5V is not a functional interface.

    There are some more tests that can be done with a meter to check that you have RX and TX  correctly connected to their complements on the pC lead but we'll leave that until we know if we have the right voltage levels.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 2 years ago in reply to michaelkellett
    michaelkellett said:
    This would suggest that the DMM is  a logic level RS232 so it won't work (reliably) with a a true RS232 adapter on the PC.

    Looks like there is a Sipex SP232 RS232 line driver/receiver on the circuit board.


    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 2 years ago in reply to beacon_dave

    Where did you get the picture ?

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JWx
    0 JWx over 2 years ago in reply to michaelkellett

    int the repo you have found there are also photos of PCB....
    https://raw.githubusercontent.com/PetteriAimonen/owon-xdm2041-info/main/mcu_board/mcu_board_top.jpg

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • JWx
    0 JWx over 2 years ago in reply to michaelkellett

    int the repo you have found there are also photos of PCB....
    https://raw.githubusercontent.com/PetteriAimonen/owon-xdm2041-info/main/mcu_board/mcu_board_top.jpg