Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Seeking Portable Solution for Rapidly Cooling 10 Tons of Water from 100°C to 30°C for Transport
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Subscribers 334 subscribers
  • Views 3301 views
  • Users 0 members are here
  • wastewater treatment
  • thermal
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Seeking Portable Solution for Rapidly Cooling 10 Tons of Water from 100°C to 30°C for Transport

Maral
Maral over 2 years ago

I'm working on a water treatment project where we need to transport 10 tons of water from the production site to a treatment plant. The challenge is that the water exits the production process at 100°C, and this high temperature risks damaging the pump system on our transport truck, leading to operational issues. I'm looking for a portable and efficient solution that can rapidly cool this large volume of water from 100°C down to 30°C before it enters the truck’s system. The cooling mechanism needs to be compact enough to fit within the truck's infrastructure and must be compatible with the truck and tunnel system materials to prevent rust and corrosion. Has anyone dealt with a similar challenge? What technologies, materials, or approaches would you recommend to achieve this rapid cooling? Any insights on energy requirements or practical considerations would also be greatly appreciated! Thanks in advance for your help! 

  • Sign in to reply
  • Cancel

Top Replies

  • kmikemoo
    kmikemoo over 2 years ago +4
    Maral Portable and inexpensive... two options. #1 big radiator. Source second-hand from someone that blew up their large generator engine. Not common but not unobtainable either. Challenge is this requires…
  • michaelkellett
    michaelkellett over 2 years ago +2 verified
    3GJ = 817kWh of energy. And you plan to just waste this energy - think again ! If you want more helpful offers you need to explain a LOT more. Who are you (engineer, student, etc etc), what's the…
  • michaelkellett
    michaelkellett over 2 years ago in reply to Maral +2 verified
    Great - now you have explained the problem in detail I can see that most of the suggestions made are not much help ! What is the diameter of the tank access ? From what maximum depth must the water…
Parents
  • dougw
    0 dougw over 2 years ago

    Basically you need to transfer energy from water to air, but there is also an option to dump energy into evaporation. You have 3 main options: conduction, convection and latent heat of evaporation. Convection and latent heat require maximizing the water surface exposed to air, conduction requires maximizing the water surface area exposed to the heat conductor and of course the heat conductor needs the maximum surface exposed to air. There are lots of ways to increase surface area of water and air and you will need fans to increase the amount of air extracting heat. If you can't find a pump to move the water, you might be able to use heat pipes. There are numerous heat exchanger systems that are designed to do all this stuff. If you want it to work quickly, it will need to be large.

    It would be ideal if you could harness the energy in the hot water to dive the entire cooling system using something like a Stirling engine or a Peltier device.

    Although hot water can be tough on equipment, there is lots of equipment designed to handle hot water.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 2 years ago

    Basically you need to transfer energy from water to air, but there is also an option to dump energy into evaporation. You have 3 main options: conduction, convection and latent heat of evaporation. Convection and latent heat require maximizing the water surface exposed to air, conduction requires maximizing the water surface area exposed to the heat conductor and of course the heat conductor needs the maximum surface exposed to air. There are lots of ways to increase surface area of water and air and you will need fans to increase the amount of air extracting heat. If you can't find a pump to move the water, you might be able to use heat pipes. There are numerous heat exchanger systems that are designed to do all this stuff. If you want it to work quickly, it will need to be large.

    It would be ideal if you could harness the energy in the hot water to dive the entire cooling system using something like a Stirling engine or a Peltier device.

    Although hot water can be tough on equipment, there is lots of equipment designed to handle hot water.