Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Why is D5 failing?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 22 replies
  • Subscribers 335 subscribers
  • Views 2747 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Why is D5 failing?

inavitech
inavitech over 1 year ago

image

Project I am working on. I'm not a board designer. Box integration is more my thing. This circuit is needed for providing a 13VDC output. Input power is 28VDC. When 28VDC is applied the power supply voltmeter drops to 6VDC, and it goes into current limiting mode. Current output is maxed out at 5 amps. D5 starts to look like a well done hotdog on the grill and begins to smoke. There were other parts of this circuit in the original design that are not being utilized, but as I said I'm not a board guy. I think with the removal of the unnecessary portion, the current is too high, thus R15's value is too low now. Figured maybe one of you on the forum might have the answer. So how this works is the tester utilizes 28VDC to test a battery pack. All of the other functions work properly when removing this part of the circuit from the equation. There is a test for a particular circuit in the battery that requires 13VDC to verify proper operation, so I can't ditch this portion of the tester. Maybe there is a better way to do this?

  • Sign in to reply
  • Cancel

Top Replies

  • inavitech
    inavitech over 1 year ago +4
    Well, I have it figured out. It is Q1. I looked at the spec sheet again and looked at it's installation on the prototyping board and the collector and base are swapped. So that is probably why the current…
  • dougw
    dougw over 1 year ago +3
    Was this circuit ever working, or was it just assembled and never worked? The connections for U1 don't make sense, but are not likely the problem. If the collector and emitter of Q1 are reversed, The…
  • JWx
    JWx over 1 year ago +1
    could Q1 be damaged (C-B shorted for example)?
Parents
  • acdc90
    0 acdc90 over 1 year ago

    if you supply an external  13v to the output of this how much current is required to run the rest of it ? 

    is this a commercial machine with a brand and model ?

    do you have the original circuit diagram or have you just traced this out. ?

    is there a shunt resister ( for current sence ) after Q1 ? 

    which the op amp is connected to.

    You said there are unnecessary portion, i think you need to draw more of circuit

    if this machine is for testing batteries  could this be part of a current dump to control the discharge of the battery

      

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • inavitech
    0 inavitech over 1 year ago in reply to acdc90

    The 13VDC is just a pass through in the battery pack to test a diode. If the circuit path is good the annunciator LED on the test box will be lit dim since it is receiving 50% power. Then the next step is to throw another switch that adds 24VDC from the battery to the line internal to the battery giving the output about 32VDC, so the annunciator should be on brightly. That is all it is for. Just to test a pass through circuit in the battery with a diode. The diode is there to prevent back flow of current when the battery has output on the pass through so it flows the correct direction.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • inavitech
    0 inavitech over 1 year ago in reply to acdc90

    The 13VDC is just a pass through in the battery pack to test a diode. If the circuit path is good the annunciator LED on the test box will be lit dim since it is receiving 50% power. Then the next step is to throw another switch that adds 24VDC from the battery to the line internal to the battery giving the output about 32VDC, so the annunciator should be on brightly. That is all it is for. Just to test a pass through circuit in the battery with a diode. The diode is there to prevent back flow of current when the battery has output on the pass through so it flows the correct direction.