Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Why is D5 failing?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 22 replies
  • Subscribers 335 subscribers
  • Views 2778 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Why is D5 failing?

inavitech
inavitech over 1 year ago

image

Project I am working on. I'm not a board designer. Box integration is more my thing. This circuit is needed for providing a 13VDC output. Input power is 28VDC. When 28VDC is applied the power supply voltmeter drops to 6VDC, and it goes into current limiting mode. Current output is maxed out at 5 amps. D5 starts to look like a well done hotdog on the grill and begins to smoke. There were other parts of this circuit in the original design that are not being utilized, but as I said I'm not a board guy. I think with the removal of the unnecessary portion, the current is too high, thus R15's value is too low now. Figured maybe one of you on the forum might have the answer. So how this works is the tester utilizes 28VDC to test a battery pack. All of the other functions work properly when removing this part of the circuit from the equation. There is a test for a particular circuit in the battery that requires 13VDC to verify proper operation, so I can't ditch this portion of the tester. Maybe there is a better way to do this?

  • Sign in to reply
  • Cancel

Top Replies

  • inavitech
    inavitech over 1 year ago +4
    Well, I have it figured out. It is Q1. I looked at the spec sheet again and looked at it's installation on the prototyping board and the collector and base are swapped. So that is probably why the current…
  • dougw
    dougw over 1 year ago +3
    Was this circuit ever working, or was it just assembled and never worked? The connections for U1 don't make sense, but are not likely the problem. If the collector and emitter of Q1 are reversed, The…
  • JWx
    JWx over 1 year ago +1
    could Q1 be damaged (C-B shorted for example)?
  • dang74
    0 dang74 over 1 year ago in reply to inavitech

    I will keep an open mind and assume that Q1 can be self biased... and since the base is 13.5V the emitter will be 12.1V or 2x diode drops below.  And in this scenario U1 would be only used for monitoring.  It's safer to monitor on the output of U1 than it is on the base  of the transistor directly.  So even though I thought the schematic was incorrect initially... maybe it's perfectly fine... and your problem could be due to a faulty component such as Q1, which was already suggested.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gordonmx
    0 gordonmx over 1 year ago

    Do you have a picture of the actual board?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JWx
    0 JWx over 1 year ago

    what means "When 28VDC is applied the power supply voltmeter drops to 6VDC"? Where is this voltmeter placed? In the power supply above D7? then it is even stranger because D5 souldn't be conducting at 6V, thun shouldn't get hot...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 1 year ago

    Was this circuit ever working, or was it just assembled and never worked?

    The connections for U1 don't make sense, but are not likely the problem.

    If the collector and emitter of Q1 are reversed, The emitter could breakdown and cause excessive current through the base and D5, if this high current burnt D5 to a short, you could be left with the breakdown voltage of the emitter, and high current....

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • acdc90
    0 acdc90 over 1 year ago

    if you supply an external  13v to the output of this how much current is required to run the rest of it ? 

    is this a commercial machine with a brand and model ?

    do you have the original circuit diagram or have you just traced this out. ?

    is there a shunt resister ( for current sence ) after Q1 ? 

    which the op amp is connected to.

    You said there are unnecessary portion, i think you need to draw more of circuit

    if this machine is for testing batteries  could this be part of a current dump to control the discharge of the battery

      

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JWx
    0 JWx over 1 year ago in reply to JWx

    maybe Q1 is shorted, D5 gets melted/shorted by excessive current then conducts high current causing power supply to drop voltage to 6V

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • inavitech
    0 inavitech over 1 year ago

    Well, I have it figured out. It is Q1. I looked at the spec sheet again and looked at it's installation on the prototyping board and the collector and base are swapped. So that is probably why the current draw is so high and the zener is being over heated so rapidly. Was so fixated that R15 had to be to small that I didn't think Q1 could be the cause. Always helps sometimes to have others help you look for things you didn't think of.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • md_steve
    0 md_steve over 1 year ago in reply to dang74

    Unity Buffer to Nowhere. As Art Buchwald used to say, "That sounds like a good name for a rock group."  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JWx
    0 JWx over 1 year ago in reply to dougw

    good diagnosis - Ueb of TIP122 is about 5V, which explains 6V observed...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • inavitech
    0 inavitech over 1 year ago in reply to acdc90

    The 13VDC is just a pass through in the battery pack to test a diode. If the circuit path is good the annunciator LED on the test box will be lit dim since it is receiving 50% power. Then the next step is to throw another switch that adds 24VDC from the battery to the line internal to the battery giving the output about 32VDC, so the annunciator should be on brightly. That is all it is for. Just to test a pass through circuit in the battery with a diode. The diode is there to prevent back flow of current when the battery has output on the pass through so it flows the correct direction.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>