Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum PIR Sensor ultra sensitive
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 20 replies
  • Subscribers 333 subscribers
  • Views 2894 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

PIR Sensor ultra sensitive

tonyd512
tonyd512 over 1 year ago

Hello,

New to Element 14

Needing a PIR sensor (or something more appropriate) sensitive enough to detect box elder bugs. They are about 1/4 inch long. Sensor needs to have short range maybe 3-4 ft or so.

ideally it would trigger a smart phone on a tripod aimed at the target area. These bugs crawl quite slowly mostly but do fly as well.

Need a little guidance choosing an appropriate sensor for the project. This will be indoors.

Tony D

  • Sign in to reply
  • Cancel

Top Replies

  • kmikemoo
    kmikemoo over 1 year ago +2
    While electronics would be cool, if you can't localize the point of entry based on sightings, I would go with a simpler approach. They could also be "replicating" inside. You might be able to secure…
  • shabaz
    shabaz over 1 year ago +1
    What's the actual goal? What is the use-case? By 'trigger a smart phone aimed at the target area' do you mean to trigger a smart phone camera? Or something else? If all you wish to do is to take photos…
  • shabaz
    shabaz over 1 year ago in reply to tonyd512 +1
    There are some interesting solutions described here: https://stackoverflow.com/questions/189943/how-can-i-quantify-difference-between-two-images There's a simple one mentioned there which is to just…
Parents
  • shabaz
    0 shabaz over 1 year ago

    What's the actual goal? What is the use-case? By 'trigger a smart phone aimed at the target area' do you mean to trigger a smart phone camera? Or something else?

    If all you wish to do is to take photos of them, then if they move slowly, you could simply just take a photo say every minute without sensing them, because storage is cheap. Then there would be no need for a sensor other than the camera, and you could process the photos to extract the ones that are sufficiently different, to identify the interesting photos.

    If there's some other aim in mind, then it would help to know it, to come up with an appropriate solution.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tonyd512
    0 tonyd512 over 1 year ago in reply to shabaz

    Hello,

    Goal is to figure out where these bugs are getting into the house and then plugging the holes. They can get in the tiniest cracks. They are insidious and sneaky little buggers. They leave a trail pheromones for others to follow when they find a new way in. They are to be admired really. They are testing of my tenacity and resolve. I have organic vegetarian friends who have resorted to spraying their whole house with pesticides to stop them!

    PIR would trigger phone or camera to take photo when one goes by which then identifies an area they are getting in.

    Over the past year I have diligently sealed up cracks and holes where they were getting in. We are getting 80% less getting inside than the last season but still an annoying 12-24 per day on sunny days in the winter in NW Oregon.

    I have thought about time lapse every 15-30 seconds or so, but I would have to sit there and view 5,000 pictures over a 24 hr of recording to spot any that might go by!

    I have done a fair amount of Photoshop work but I'm not familiar with how to identify "sufficiently different" photos. That may be the simplest solution if you could teach me how to do that!

    Thank you so much for your help

    Tony D

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 1 year ago in reply to tonyd512

    There are some interesting solutions described here:

    https://stackoverflow.com/questions/189943/how-can-i-quantify-difference-between-two-images

    There's a simple one mentioned there which is to just have some code to compare the jog file sizes, because any image with sufficiently different content may have a noticeably different file size. 

    To test this, you could take a photo of an example location, and then add some artificial bugs if none exist, using say photoshot, and then subjecting the images to some of the solutions mentioned at that link, to see what works best. 

    One other approach could be to try a microwave sensor. Sometimes they can detect very slight changes (including vibration of the mount). But it would require experimentation, I have no idea if it would detect a slow-moving bug. There's an example microwave detector article here:

    /technologies/embedded/b/blog/posts/experimenting-with-microwave-based-sensors-for-presence-detection#mcetoc_1h0c077bia

    PIR is unfortunately very unlikely to work, because the amount of heat energy will be tiny, and most PIR sensors need sufficient movement too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 1 year ago in reply to tonyd512

    You certainly have an interesting challenge on your hand.

    Before thinking of possible solutions I wanted to understand more about your intended sensing locality or proximity to these pesky little bugs. You mentioned that the sensor needs to have short range maybe 3-4 ft or so. How narrow focused does the sensor of choice need to be, or what sort of field of view would you require at 3-4 ft away? Are you intending to keep an eye on monitoring just the hole or crack, for example. If it's a crack, how long are the cracks?

    My thinking is that if these cracks are no more than an inch or two long then you could potentially shrink things down a bit where a sensor is merely a couple of inches away, for example.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • BigG
    0 BigG over 1 year ago in reply to tonyd512

    You certainly have an interesting challenge on your hand.

    Before thinking of possible solutions I wanted to understand more about your intended sensing locality or proximity to these pesky little bugs. You mentioned that the sensor needs to have short range maybe 3-4 ft or so. How narrow focused does the sensor of choice need to be, or what sort of field of view would you require at 3-4 ft away? Are you intending to keep an eye on monitoring just the hole or crack, for example. If it's a crack, how long are the cracks?

    My thinking is that if these cracks are no more than an inch or two long then you could potentially shrink things down a bit where a sensor is merely a couple of inches away, for example.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • tonyd512
    0 tonyd512 over 1 year ago in reply to BigG

    Good questions BigG

    I've sealed up the most obvious and straightforward  cracks and holes such as a crack around a window or gap in a door weather stripping. What I need to observe over time is areas that may lead to gaps in the ceiling over kitchen cabinets which might lead to a void between a floor and ceiling, that may lead to a crack in the roofing where they begin their entry. They will follow the longest winding path that you can't believe to get in. It's impossible to tell from the outside since they are all over the house looking for ways to get in. So if I could observe an area about 4 ft away from the camera and around 4 ft of target area that should do it. If set up my camera for about 24 hours and don't see a bug then I move the camera to a different area. Keep in mind it's down to about 15 bugs per day so if they were all getting in the same spot then it would be around 1 per 2 hours, or less if they are getting in more than one spot (very likely!)