Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum MATLAB licensing advice for SDR/general hobby?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 333 subscribers
  • Views 3083 views
  • Users 0 members are here
  • ADALM-PLUTO
  • matlab
  • sdr
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

MATLAB licensing advice for SDR/general hobby?

JWx
JWx over 1 year ago

Hello!

As a follow-up to the SDR Pluto Roadtest forum thread I have a question to the MATLAB experts: considering home licensing model, what add-ons are required/nice to have for - for example - SDR related, entry level experiments?

It seems that at least:

  • Communications Toolbox
  • DSP System Toolbox
  • Signal Processing Toolbox

are needed in addition to the main license...

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 1 year ago in reply to JWx +4
    Is it cheaper to take a single uni course just to be eligible for a student license? I believe the universities around here provide free on-line degree programs for seniors, so retirees might work something…
  • shabaz
    shabaz over 1 year ago +4
    A fun simple MATLAB script that I think uses just the Communications Toolbox: % FM I/Q WAV file generator % rev 1 - shabaz - feb 2024 % Generates a WAV file containing I and Q components of an % FM modulated…
  • anniel747
    anniel747 over 1 year ago in reply to beacon_dave +3
    Deleted
  • shabaz
    shabaz over 1 year ago

    A fun simple MATLAB script that I think uses just the Communications Toolbox:

    % FM I/Q WAV file generator
    % rev 1 - shabaz - feb 2024
    % Generates a WAV file containing I and Q components of an
    % FM modulated signal. The audio source is a mono WAV file.
    % Sample rates are 48 kHz for input and output.
    
    % input audio
    audio_fname = 'eveshort-48-mono.wav';
    % FM modulation parameters, fd = frequency deviation
    fd = 5e3; % 5 kHz
    out_bw = 2*(fd + 12e3); % 2*(freq deviation + audio bandwidth (12kHz))
    out_fs = 2*out_bw; % 180*2 = 44ksps
    % might as well make it 48ksps, for a round number!
    out_fs = 48e3;
    
    % read in the source audio
    [x,fs] = audioread(audio_fname);
    
    % create the FM modulator object
    fmmodulator = comm.FMModulator( ...
        'SampleRate',out_fs, ...
        'FrequencyDeviation',fd);
    
    % perform the FM modulation
    y = fmmodulator(x);
    
    % obtain the I/Q components
    I = real(y);
    Q = imag(y);
    
    % build the stereo WAV file containing the I and Q outputs
    IQ_stereo = [I';Q']';
    audiowrite('iq_file.wav', IQ_stereo, 48e3);

    Hopefully the comments make sense. It converts an input mono WAV audio file, into an output WAV stereo file that has FM modulated I/Q output at baseband.

    You could play the stereo output file using any media player, and you should hear distortion.

    You can then play that file using any free SDR software on your PC, to demodulate the FM and convert back to the original audio.

    I've placed the file plus the example WAV input and the generated output file (so that anyone can try it without requiring MATLAB) here: https://github.com/shabaz123/fm_iq_create

    This is the example mono input file content:

    image

    And this is the output WAV file with FM modulation, with I and Q in the stereo channels:

    image

    See that GitHub link readme, to see how to use it with free SDR++ software as an example.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 1 year ago

     JWx go there why get bent over??  OPEN SOURCE 5 packages to pick from!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to phoenixcomm

    phoenixcomm , something went wrong with the hyperlink above

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 1 year ago in reply to phoenixcomm

    the problem is for example hardware support/Matlab compatibility level - I have used Octave in the past, but there is no support for Pluto (AFAIK) and writing one could be time-consuming: I am afraid I don't have skills needed. but maybe something can be adapted...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 1 year ago in reply to Jan Cumps

     Jan Cumps Sorry about that  OPENSOURCE

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 1 year ago in reply to beacon_dave
    [deleted]
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to anniel747

    I've not seen that one either.

    I'm starting to think some of you folks must be using Element14plus edition with all those extra features.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 1 year ago in reply to phoenixcomm

    after some thinking - maybe porting of ADI toolbox can be done during reasonable time and using limited skill. After all, Octave is considered (more or less) Matlab compatible. Thanks, phoenixcomm  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 1 year ago in reply to JWx

     JWx Not a problem.. Open Source is your fiend! Microsoft and people with small minds and limited sight, are not! ~~Cris 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 1 year ago in reply to phoenixcomm
    phoenixcomm said:
    Open Source is your fiend!

    That missing R worries me !

    Actually MATLAB itself is pretty good - but expensive.

    I shall be sad when I no longer do enough paying work to justify the maintenance.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>