Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Low Temperature Deviation Issue with Hart Scientific 5615 RTD
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 338 subscribers
  • Views 757 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Low Temperature Deviation Issue with Hart Scientific 5615 RTD

metroman
metroman over 1 year ago

Hi everyone,

I'm encountering a strange behavior during an intercomparison between several calibrated RTD temperature probes. Here's the context:

  • I'm using 5 RTD sensors, one of which is a Hart Scientific 5615.
  • Each sensor is connected to its own readout instrument.
  • Measurements were performed in both an oil bath and a dry air oven to rule out medium-related effects.
  • All sensors were allowed to stabilize for over 20 minutes at each temperature point.

Observed behavior

  • From 0 °C to 121 °C, all sensors agree very closely, with negligible deviations.
  • Below 0 °C, the 5615 starts to deviate by approximately 0.2°C from the others (MPE is at +/- 0.03 °C yes extreme precision is needed).
  • Once the temperature is raised again, the 5615 returns to normal behavior.
  • The issue is repeatable, regardless of medium, measurement point, or configuration.

Hypotheses already ruled out

  • Response time: ruled out (long stabilization time).
  • Material or construction differences: all sensors are identical in build and sheath, the only difference is the model of this particular sensor, but it's calibrated by the same Lab and it shouldn't be a problem.
  • Measurement point: tested at various positions multiple times.
  • Measurement medium: tested in both oil and air, I get the same result.
  • Readout device: each sensor has its own dedicated instrument.

Possible causes under consideration

  • Incorrect application of ITS-90 or Callendar–Van Dusen coefficients in the readout?
  • Localized calibration error at low temperatures, is it possible? Could it be that the sensor is linear for "high" tempreratures and non-linear for "lower" ones?
  • Firmware or electronic behavior specific to the readout used with the 5615?
  • Interpolation or coefficient misapplication in the readout or calibration file?

Has anyone experienced a similar issue with the 5615 or other high-precision RTDs?
Any suggestions for further testing or troubleshooting would be greatly appreciated.

Thanks in advance!

  • Sign in to reply
  • Cancel
Parents
  • kmikemoo
    kmikemoo over 1 year ago

     metroman I'm no expert, but the problem is intriguing.  Is the Hart the "odd man out" or do you have 5 unique instruments?  Have you moved the sensors between instruments to isolate it to the 5615?  With the sensors being as precises as they are, maybe it's the difference of a picogram of solder somewhere in the circuit.  Are there any probe adapters or anything like that in your sensor circuit that makes that instrument different?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • metroman
    metroman over 1 year ago in reply to kmikemoo

    Thank you very much for your reply I really appreciate it!

    To clarify:

    • All five sensors are Hart Scientific RTDs, but the one showing the deviation is of a different model than the others  that’s the only notable difference. I didn't know it but when I looked I saw that it had a slightly different shape.
    • Each sensor is connected to its own dedicated readout, and they are calibrated as a pair (sensor + instrument), so swapping instruments isn’t an option without breaking traceability.
    • I’ve tested the 5615 in different environments (oil bath and air oven), and even in isolation with just one other sensor the deviation at low temperatures remains consistent.
    • There are no adapters or special connections in the setup all sensors are connected identically, I also did some tests with different connections but nothing changes.

    The deviation is about 0.2 °C below 0 °C, which is well beyond the expected tolerance. It's true that with sensors this precise, even the tiniest physical or electrical variation could potentially have an effect.
    That said, it would be extremely difficult to detect or confirm something like a microscopic solder variation in practice, especially since the setup is otherwise very clean and consistent.

    Thanks again for your input your questions helped me think it through more clearly!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • metroman
    metroman over 1 year ago in reply to kmikemoo

    Thank you very much for your reply I really appreciate it!

    To clarify:

    • All five sensors are Hart Scientific RTDs, but the one showing the deviation is of a different model than the others  that’s the only notable difference. I didn't know it but when I looked I saw that it had a slightly different shape.
    • Each sensor is connected to its own dedicated readout, and they are calibrated as a pair (sensor + instrument), so swapping instruments isn’t an option without breaking traceability.
    • I’ve tested the 5615 in different environments (oil bath and air oven), and even in isolation with just one other sensor the deviation at low temperatures remains consistent.
    • There are no adapters or special connections in the setup all sensors are connected identically, I also did some tests with different connections but nothing changes.

    The deviation is about 0.2 °C below 0 °C, which is well beyond the expected tolerance. It's true that with sensors this precise, even the tiniest physical or electrical variation could potentially have an effect.
    That said, it would be extremely difficult to detect or confirm something like a microscopic solder variation in practice, especially since the setup is otherwise very clean and consistent.

    Thanks again for your input your questions helped me think it through more clearly!