Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Power outage alarm
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 25 replies
  • Answers 1 answer
  • Subscribers 336 subscribers
  • Views 3251 views
  • Users 0 members are here
  • power outage
  • pico 2
  • outage
  • alarm
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Power outage alarm

EdgarAndre
EdgarAndre over 1 year ago

Hello, I am new to electronics and I would like to make a power outage alarm with a Raspberry Pi Pico 2 circuit that I bought as a kit. The Pico would be connected via USB and when a power outage occurs, a two-hour timer would start and after these two hours an alarm would sound. The circuit would be powered by a 9 volt battery for two hours. The alarm could sound for one minute with a bib every two seconds. If the power comes back on before two hours, I would like the timer to reset. Do you have any solutions to suggest or examples of circuits adaptable to this project? Thank you very much for your help.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 1 year ago +4
    If you're a beginner, you could just try some beginner projects, they may get you halfway there. The first project is usually a blinking LED. If you can blink an LED then you can pulse a buzzer with…
  • kmikemoo
    kmikemoo over 1 year ago in reply to shabaz +3
    shabaz I understand EdgarAndre's desire for the 2-hour wait. At the last place we rented, the squirrels would regularly trip the main feeder breaker. The outage would typically last 45 minutes to an hour…
  • kmikemoo
    kmikemoo over 1 year ago in reply to shabaz +3
    shabaz Many years ago, I put my router on a UPS. The first outage proved that my ISP had NONE of their equipment on UPS's. Nor did they have backup generators. I can only hope that they have improved.
Parents
  • EdgarAndre
    0 EdgarAndre over 1 year ago

    I just returned the freezer and refrigerator alarm I bought on Amazon because one of the sensors wasn't working. I also reread the comments from other dissatisfied buyers and there seem to be reliability issues with the thermometer's accuracy and overall build quality. However, I found a circuit that seems interesting and I'll give you the link. If you have the time, I would appreciate your feedback. Leaving a light on isn't ideal, but since I would only be using this alarm at night for severe storm warnings, it's acceptable. I will obviously use the smallest Dell bulb possible.https://www.instructables.com/Power-Outage-Alarm/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kmikemoo
    0 kmikemoo over 1 year ago in reply to EdgarAndre

    EdgarAndre I'm sorry to hear that you had to return the sensor.  It has a 4.3 of 5 rating with over 2,500 reviews.  Also remember that people are much more likely to leave a negative review than a positive one.  The system is skewed towards the negative.

    You can replicate what this was going to do with you Pico and a temperature sensor - such as the DS18B20, DHT11, DHT22 or LM35.  I'd still go with a small piezo alarm.  Since it seems like you really want to build one, pick up a LiPo battery and charger module (TP4056).  Use that to power the Pico and charge the battery.  A single 18650 battery should be sufficient.  With normal power available, the system runs off of the wall wart.  If the power goes out, it runs off of battery.  The only downside is the cable that goes into the fridge and/or freezer for the sensor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kmikemoo
    0 kmikemoo over 1 year ago in reply to EdgarAndre

    EdgarAndre I'm sorry to hear that you had to return the sensor.  It has a 4.3 of 5 rating with over 2,500 reviews.  Also remember that people are much more likely to leave a negative review than a positive one.  The system is skewed towards the negative.

    You can replicate what this was going to do with you Pico and a temperature sensor - such as the DS18B20, DHT11, DHT22 or LM35.  I'd still go with a small piezo alarm.  Since it seems like you really want to build one, pick up a LiPo battery and charger module (TP4056).  Use that to power the Pico and charge the battery.  A single 18650 battery should be sufficient.  With normal power available, the system runs off of the wall wart.  If the power goes out, it runs off of battery.  The only downside is the cable that goes into the fridge and/or freezer for the sensor.