Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Need help designing a flow sensor for marine application
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 335 subscribers
  • Views 986 views
  • Users 0 members are here
  • flow sensor
  • flow meter
  • transit-time transducer
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Need help designing a flow sensor for marine application

e14 Contributor
e14 Contributor 8 months ago

I want to develop a flow sensor for sea water hose flow rate. It will be used to provide information to be able to shut off and on a water pump. I'd say a clamp on style able to be mounted on a short piece of pipes of various diameters. Any engineers would like to help or guide me in the right direction? 

AI is helping me but I'm not an engineer. I have found out that I'll need transit-time transducers (non-intrusive) and a flow rate of 5-100 GPM. 

The transducers will be mounted in a short piece of Schedule 80PVC (about 3-4" long) and threaded on both sides for easy installation. There is a product that already exists for my needs but it is Propriatary. (Electrosea "ClearVis" sensor). Basically I'm in need to know the flow rate of sea water so when it is lower than, say 13GPM, send a signal to shut off the water pump. In the available Electrosea system it is used for it's operation and depending on the water flow rate it will introduce current so create cholrine in the sea water to prevent biologiacal fouling. Eventually I'll get there, right now just looking to design that sensor.

Any takers?

Thanks

Mario

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett 8 months ago +1
    Unless your time is of zero value you will not be able to develop a flow sensor like an existing product for less cost than just buying one. You might come up with a novel solution to your problem (but…
  • colporteur
    colporteur 8 months ago in reply to e14 Contributor +1
    https://community.element14.com/products/roadtest/rt/roadtests/583/flusso_fls110_mass_flow_sensor_evaluation_kit#pifragment-18971=4&pifragment-18972=7&pifragment-19828=11 As a community we would be remiss…
Parents
  • dougw
    0 dougw 8 months ago

    You can measure flow rate analogous to measuring electrical current by measuring the voltage drop across a resistor. Pressure corresponds to voltage and a restriction corresponds to resistance. Measuring the pressure at each end of a pipe of known "resistance" allows the flow to be calculated. flow = (Pin - Pout) / r.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor 8 months ago in reply to dougw

    I did went down this path but the water flow is too much for this solution, 4-75GPM of seawater. Also there would be way to many turns and loops in the system with verious diameter. The resistor solution fits best on a straight pipe and low flow. But thanks for making me learn a bit more about other solutions. Deifately I've seen paddle flow sensors but I want to avoid intrucion and the seawater would eventually degrade moving parts. 

    Thank you again for your input.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor 8 months ago in reply to dougw

    I did went down this path but the water flow is too much for this solution, 4-75GPM of seawater. Also there would be way to many turns and loops in the system with verious diameter. The resistor solution fits best on a straight pipe and low flow. But thanks for making me learn a bit more about other solutions. Deifately I've seen paddle flow sensors but I want to avoid intrucion and the seawater would eventually degrade moving parts. 

    Thank you again for your input.