Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Soldering iron station that suddenly does not heat anymore
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 2 answers
  • Subscribers 336 subscribers
  • Views 929 views
  • Users 0 members are here
  • soldering
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Soldering iron station that suddenly does not heat anymore

obones
obones 3 months ago

Hello,

I have a soldering "station" that has been working just fine for quite a while now and up until this morning. You can get a glimpse of it in this message:  Finally took the time to reorganize the workbench! 

But this afternoon, when I turn it on, the usual two left LEDs turn on, one for "there is power" and one for "heating up" but the iron tip and body do not get hot at all and the temperature bar does not light up to the set temperature.

What could be the reason? What should I look at in the hopes of repairing it?

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur 3 months ago +3
    20 years! That will have some burnt skin on it. Time to Christmas shop for a new one.
  • obones
    obones 3 months ago +3
    Looking around for the handle pinout, I stumbled across a picture of of it brand new: The cord has a 5 pin DIN connector but I'm not sure which pin is which. And to open then handle, I should have…
  • obones
    obones 19 hours ago +3
    Well, there was an offer that I couldn't resist on a C245 station with quite a few tips, so in exchange for a little over 100€ instead of well above 125€, I am now the happy owner of a Yihua 982DSE: …
Parents
  • obones
    0 obones 3 months ago

    Looking around for the handle pinout, I stumbled across a picture of of it brand new: 

    image

    The cord has a 5 pin DIN connector but I'm not sure which pin is which.
    And to open then handle, I should have needed a "prong" screwdriver but luckily the screw heads were accessible and moved with simple flat pliers.
    But even if I could figure out the pinout, I don't think I even could replace the heating element, it looks like it's potted:

    image

    However, and that's the good news, taking it apart and putting it back together brought it back to life!
    It's now heating up again and not lying about it either.

    This gives me more time to better document myself on current technology, especially with respect to tips.

    So far, I believe my station and the three candidates that I presented below are using "passive" tips in that the temperature sensor is inside the body, not near the extremity of the tip.

    And it seems there are newer technologies named T12 and JBC, the latter being the most recent one, and so the recommended these days.

    As I've never used any of those new techs, what could I expect from upgrading in terms of usage feeling?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • battlecoder
    0 battlecoder 3 months ago in reply to obones

    I've used a couple of stations with T12 tips and they heat up fast so the are ready to go in seconds. They are also very efficient (or at least a lot more efficient than passive tips) when it comes to supplying heat to beefier joints/components/leads.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • battlecoder
    0 battlecoder 3 months ago in reply to obones

    I've used a couple of stations with T12 tips and they heat up fast so the are ready to go in seconds. They are also very efficient (or at least a lot more efficient than passive tips) when it comes to supplying heat to beefier joints/components/leads.