Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Buck converters
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 306 subscribers
  • Views 1370 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Buck converters

Former Member
Former Member over 9 years ago

Hi experts.

 

Being new to electronics, I got this unanswered question about adjustable buck converters (dc step down converter modules) - see Buck Step Down LM2596 Power Converter Module DC 4 0 40 to 1 3 37V LED Voltmeter | eBay.

 

They are usually built around a LM2596 IC, which uses 2 resistors to adjust the output voltage.

 

On my module, the first resistor is fixed and the second one is a multi-turn potentiometer.

 

The module should be able to handle 37V / 2A, but the potentiometer is only rated 1/2 watt. So why is it that 1/2 watt is enough for this application?

 

I want to replace the multi turn potentiometer with a rotary potentiometer. Does anyone have a clue how much resistance the potentiometer should provide? I guess the higher the better?

 

Kind regards,

Klaus

  • Sign in to reply
  • Cancel
  • D_Hersey
    D_Hersey over 9 years ago

    It is unlikely very much current flows through the sense terminal, you should be fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 9 years ago

    Hi Klaus,

    The potentiometer is a control mechanism that allows a small amount of current to control the larger output. Think of it as a steering wheel on a vehicle. The steering wheel allows a weak person to turn two large vehicle wheels with only a little effort. I have used buck power converter like this in some of my power supply builds. I have used multi-turn panel mounted potentiometers to give me fine control of the output voltage. Because of the small current that flows through the control potentiomenter you do not have to worry about the wattage rating in this instance. Here is a link to what a multi-turn panel mount potentiomenter looks like. Make sure you get a Linear Potentiomenter for this application.

     

    http://www.ebay.com/itm/2pcs-NEW-WXD3-13-2W-10K-ohm-Rotary-Multiturn-Wirewound-Potentiometer-Good-/171505107581?hash=item27ee80427d:g:ThMAAMXQQQZR1RvX

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 9 years ago

    Hi Klaus,

     

    The small blue board mounted potentiometer will have a number on it. It is coded just like the small components. For example it will be a 3 digit number. The first 2 numbers are significant and the third digit is a times ten multiplier. In this way 1 0 2 becomes 1000 ohms, 1 0 3 becomes 10,000 ohms, 5 0 2 becomes 5000 ohms, and so on.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to jw0752

    It has 2 numbers printed on it.

     

    One is 123 T and the other is W 503.

     

    So I guess either the max resistance would be 12000 ohms or 50000 ohms. Guessing its 50000.

     

    R1 on my module is a 1800 ohm resistor.

     

    Using the vout formula from the LM2596S datasheet:

     

    vOut = vRef * (1 + R2/R1) where vRef is 1.2V, I get that the max output voltage would be 34.5V.

     

    That sounds reasonable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to jw0752

    I guess I'm trying to understand what part of the buck converter plays a part in limiting the current through the resistors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to Former Member

    Hi Klaus,

    The 50,000 ohms is the correct guess. The ones I have used have also all been 50,000 ohms. The LM 2596 chips does the heavy work of supplying the voltage and current to the output. All the resistor / potentiometer divider does is provide a reference voltage that tells the LM 2596 what to do. The LM2596 itself uses switching technology to send the proper duration of pulses to the output to create the output voltage. Feedback of the output voltage is compared to the reference voltage you have selected with the potentiomenter and adjustments are then made by the LM 2596 to keep things stable. If you want to learn more about switching converters check out this nice book by Recom:

     

    http://www.recom-power.com/de/americas/downloads/book-of-knowledge.html

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to jw0752

    Thank you for your fine explanation image