Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Buck converters
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 313 subscribers
  • Views 1401 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Buck converters

Former Member
Former Member over 9 years ago

Hi experts.

 

Being new to electronics, I got this unanswered question about adjustable buck converters (dc step down converter modules) - see Buck Step Down LM2596 Power Converter Module DC 4 0 40 to 1 3 37V LED Voltmeter | eBay.

 

They are usually built around a LM2596 IC, which uses 2 resistors to adjust the output voltage.

 

On my module, the first resistor is fixed and the second one is a multi-turn potentiometer.

 

The module should be able to handle 37V / 2A, but the potentiometer is only rated 1/2 watt. So why is it that 1/2 watt is enough for this application?

 

I want to replace the multi turn potentiometer with a rotary potentiometer. Does anyone have a clue how much resistance the potentiometer should provide? I guess the higher the better?

 

Kind regards,

Klaus

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    jw0752 over 9 years ago

    Hi Klaus,

    The potentiometer is a control mechanism that allows a small amount of current to control the larger output. Think of it as a steering wheel on a vehicle. The steering wheel allows a weak person to turn two large vehicle wheels with only a little effort. I have used buck power converter like this in some of my power supply builds. I have used multi-turn panel mounted potentiometers to give me fine control of the output voltage. Because of the small current that flows through the control potentiomenter you do not have to worry about the wattage rating in this instance. Here is a link to what a multi-turn panel mount potentiomenter looks like. Make sure you get a Linear Potentiomenter for this application.

     

    http://www.ebay.com/itm/2pcs-NEW-WXD3-13-2W-10K-ohm-Rotary-Multiturn-Wirewound-Potentiometer-Good-/171505107581?hash=item27ee80427d:g:ThMAAMXQQQZR1RvX

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 9 years ago

    Hi Klaus,

    The potentiometer is a control mechanism that allows a small amount of current to control the larger output. Think of it as a steering wheel on a vehicle. The steering wheel allows a weak person to turn two large vehicle wheels with only a little effort. I have used buck power converter like this in some of my power supply builds. I have used multi-turn panel mounted potentiometers to give me fine control of the output voltage. Because of the small current that flows through the control potentiomenter you do not have to worry about the wattage rating in this instance. Here is a link to what a multi-turn panel mount potentiomenter looks like. Make sure you get a Linear Potentiomenter for this application.

     

    http://www.ebay.com/itm/2pcs-NEW-WXD3-13-2W-10K-ohm-Rotary-Multiturn-Wirewound-Potentiometer-Good-/171505107581?hash=item27ee80427d:g:ThMAAMXQQQZR1RvX

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 9 years ago in reply to jw0752

    I guess I'm trying to understand what part of the buck converter plays a part in limiting the current through the resistors.