Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Multiple Linear Regulators in a Circuit
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 304 subscribers
  • Views 687 views
  • Users 0 members are here
  • linear regulators
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Multiple Linear Regulators in a Circuit

jeffrichley@gmail.com
jeffrichley@gmail.com over 9 years ago

I have a 24V power supply coming into my circuit and I need a 12V for a fan and 5V to run my logic.  I have 12V and 5V linear regulators that I can use to get the desired voltages.  Would it be better to run the 24V to both or the 24V to 12V and then take the 12V to the 5V?  My reasoning for the 24V -> 12V -> 5V is that the 5V would need to dissipate less power (7V vs 19V), but I didn't know if it is a bad idea to have one regulator pull from another.

 

I appreciate any input you have,

 

Jeff

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 9 years ago

    You'll just be dissipating extra current with the 12v regulator doing it that way so the 12v regulator will get hotter than it would if it wasn't providing power for both of the loads. Because it is such a large voltage drop and likely a high overall power load with it being 2 fans, you would be better off investing in a switching regulator board. Is there any way you could use 2 fans that run at the same voltage? that way you would only need 1 switching regulator for both loads. It just makes more sense and is less wasteful of power in the long run.

     

    Because of the expense of lost power with using a linear regulator, a switching regulator will more than pay for itself over time by reducing the amount of waste power you are having to pay for.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 9 years ago

    You'll just be dissipating extra current with the 12v regulator doing it that way so the 12v regulator will get hotter than it would if it wasn't providing power for both of the loads. Because it is such a large voltage drop and likely a high overall power load with it being 2 fans, you would be better off investing in a switching regulator board. Is there any way you could use 2 fans that run at the same voltage? that way you would only need 1 switching regulator for both loads. It just makes more sense and is less wasteful of power in the long run.

     

    Because of the expense of lost power with using a linear regulator, a switching regulator will more than pay for itself over time by reducing the amount of waste power you are having to pay for.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jeffrichley@gmail.com
    jeffrichley@gmail.com over 9 years ago in reply to Former Member

    There is just the one 12V fan.  The 5V is running my logic circuits which are fairly basic.  I'm having to take some measurements and drive the fan with a transistor.  Perhaps what I should do is just get a different power supply that actually provides 12V and then use the 5V linear regulator to step down from that?  I'm assuming that would make it a fair bit more efficient?  Or would you still go with the switching one to help be more efficient with the extra 7V?