Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Multiple Linear Regulators in a Circuit
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 339 subscribers
  • Views 930 views
  • Users 0 members are here
  • linear regulators
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Multiple Linear Regulators in a Circuit

jeffrichley@gmail.com
jeffrichley@gmail.com over 9 years ago

I have a 24V power supply coming into my circuit and I need a 12V for a fan and 5V to run my logic.  I have 12V and 5V linear regulators that I can use to get the desired voltages.  Would it be better to run the 24V to both or the 24V to 12V and then take the 12V to the 5V?  My reasoning for the 24V -> 12V -> 5V is that the 5V would need to dissipate less power (7V vs 19V), but I didn't know if it is a bad idea to have one regulator pull from another.

 

I appreciate any input you have,

 

Jeff

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago

    You'll just be dissipating extra current with the 12v regulator doing it that way so the 12v regulator will get hotter than it would if it wasn't providing power for both of the loads. Because it is such a large voltage drop and likely a high overall power load with it being 2 fans, you would be better off investing in a switching regulator board. Is there any way you could use 2 fans that run at the same voltage? that way you would only need 1 switching regulator for both loads. It just makes more sense and is less wasteful of power in the long run.

     

    Because of the expense of lost power with using a linear regulator, a switching regulator will more than pay for itself over time by reducing the amount of waste power you are having to pay for.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jeffrichley@gmail.com
    jeffrichley@gmail.com over 9 years ago in reply to e14 Contributor

    There is just the one 12V fan.  The 5V is running my logic circuits which are fairly basic.  I'm having to take some measurements and drive the fan with a transistor.  Perhaps what I should do is just get a different power supply that actually provides 12V and then use the 5V linear regulator to step down from that?  I'm assuming that would make it a fair bit more efficient?  Or would you still go with the switching one to help be more efficient with the extra 7V?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago

    If its just light electronics on the 5v rail, I'd just look at a different power source to provide 12v and use the linear regulator to step that down to 5v. Im not a fan of driving heavy loads like motors for long periods of time with linear regulators, it is possible but the more power you dissipate, the larger the heatsink has to be to stop it overheating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 9 years ago

    Jeff -

     

    Running the output of one linear regulator into the input of another linear regulator is possible for low currents, but you must consider the relatively high power dissipation of such a configuration. In most cases you would be better off with a switching regulator with two outputs: one 12V output and one 5V output. If you run the 24V supply into both the 12V and the 5V linear regulators, you must add the quiescent current of the 5V regulator to the output current of that 5V regulator and multiply the result by 19V (24V – 5V) to determine the power dissipation. Then you must determine if that much dissipation is beyond the capability of the regulator or not. Similarly, consider the power dissipation of the 12V regulator. If you run the 12V output into the 5V regulator, you must similarly consider power dissipation in the two regulators. Of course a regulator in a TO-220 package, or even a TO-66 or TO-3 package, can dissipate more power than can the same regulator in smaller packages, but it is generally easier to deal with a switching regulator, which will also give you power efficiency overall. If this is just for hobby use, you might be fine with the linear regulators, but you still need to consider the power dissipation of the regulators.

    Good luck!